Greetings,
I can see that the Depth Range for the ZED X Mini with a 2mm focal length is 0.1m to 8m.
I can’t seem to find a depth range for the 4mm focal length variant of the ZED mini.
I went through the available datasheets online. All I could find is that the depth range is 1.5m to 35m for the ZED 2 and ZED X 4mm focal length variants. But nothing on the ZED mini.
Where can I find this specification?
Hello there,
Thank you for reaching out.
Please note that the ZED mini is only available with a 2.8mm focal length.
The ZED mini (2.8 mm focal length) depth range is 0.1 - 15 m.
It can be found on the product page here: https://www.stereolabs.com/zed-mini/
The ZED X mini is available with 2.2 mm and 4 mm focal lengths.
Antoine Lassagne
Senior Developer - ZED SDK
Stereolabs Support
Hi again,
I am sorry, I made a mistake. I meant to ask only about ZED X Mini. So my initial question should be rephrased like this:
"
I can see that the Depth Range for the ZED X Mini with a 2mm focal length is 0.1m to 8m.
I can’t seem to find a depth range for the 4mm focal length variant of the ZED X mini.
I went through the available datasheets online. All I could find is that the depth range is 1.5m to 35m for the ZED 2 and ZED X 4mm focal length variants. But nothing on the ZED X mini.
Where can I find this specification?
"
Thank you,
John