ZED X drivers for TZTEK YS-X1-32G

Hello,

We are planning to use Stereolabs ZED X MINI and NANO GMSL2 cameras on a TZTEK YS-X1-32G / NVIDIA Jetson AGX Orin platform.

Current system:

L4T R36.4.3
Kernel: 5.15.148-tegra
SoC: NVIDIA Jetson AGX Orin / tegra234
Board compatible: nvidia,p3737-0000+p3701-0004
GMSL topology: 4x MAX9296, up to 8 camera ports

The current BSP uses an IMX185 camera stack:

tztek_camera_driver
tztek_max9296
max9296_class
nv_imx185

Could you please advise:

  1. Is there a ready-to-use driver/BSP for ZED X + TZTEK YS-X1-32G + L4T R36.4.3?

  2. Can you provide compatible versions of:

    • sl_zedx.ko

    • sl_max9296.ko

    • DTB/DTBO for MAX9296/ZED X

    • ZEDX_Daemon

    • ISP file for AR0234

  3. If no ready package is available, could you provide recommendations for adaptation, or source code/DKMS to build the drivers for kernel 5.15.148-tegra?

Thank you.

Hi @dbarinov
Welcome to the StereoLabs community.

Unfortunately, we only provide a driver for the GEACX2-64G model.

You can contact TZTEK to ask for a compatible driver for the YS-X1-32G model.

You can write to support@stereolabs.com to ask to sign the required NDA to be invited to the repository of the source code of the ZED X Driver and use the provided information to develop a custom driver.

Hi!

Thank you for your reply.

I will try both: TZTEK and stereolabs support approaches.

Also I will respond here about final resolution.