Zed X daemon I2C driver error

Hi,

I ran into an error with the zed_x_daemon on my ZED Box 8GB. I don’t have any clue of how it happened, but since this morning all my tests came up to the same results, which are “camera not detected” or “failed to connect to zed x daemon”.

I tried to troubleshoot by running a ZED_Diagnostic --dmesg, and this is the content of the logs file :

Created: Mon Jul 29 2024

###########################################
############ DMESG [ZEDX] LOG #############
###########################################

[   12.475165] zedx 9-0018: Driver Version : v0.6.4
[   12.475172] zedx 9-0018: Probing v4l2 sensor.
[   12.475356] zedx 9-0018: tegracam sensor driver:video0_v2.0.6
[   12.798456] zedx 9-0018: zedx_links_check: -1 link(s) detected
[   12.798458] zedx 9-0018: zedx_links_check: fail while reading the GMSL links state
[   12.808816] zedx: probe of 9-0018 failed with error -1
[   12.816677] zedx 9-0010: Driver Version : v0.6.4
[   12.816680] zedx 9-0010: Probing v4l2 sensor.
[   12.816949] zedx 9-0010: tegracam sensor driver:video1_v2.0.6
[   12.935176] zedx 9-0010: zedx_links_check: -1 link(s) detected
[   12.935178] zedx 9-0010: zedx_links_check: fail while reading the GMSL links state
[   12.946142] zedx: probe of 9-0010 failed with error -1
[   12.951754] zedx 10-0018: Driver Version : v0.6.4
[   12.951756] zedx 10-0018: Probing v4l2 sensor.
[   12.962439] zedx 10-0018: tegracam sensor driver:video2_v2.0.6
[   18.612923] zedx 10-0018: zedx_links_check: 1 link(s) detected
[   21.225625] zedx 10-0018: Single ZED-X camera detect success
[   22.093113] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 10-0018 bound
[   22.108074] zedx 10-0018: Detected ZED-X sensor
[   22.112681] zedx 10-0010: Driver Version : v0.6.4
[   22.112691] zedx 10-0010: Probing v4l2 sensor.
[   22.112944] zedx 10-0010: tegracam sensor driver:video3_v2.0.6
[   22.220864] zedx 10-0010: zedx_links_check: 1 link(s) detected
[   23.097007] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 10-0010 bound
[   23.097857] zedx 10-0010: Detected ZED-X sensor
[   23.101603] zedx 10-0010: zedx_open: Accessing the camera
[   23.103941] zedx 10-0018: zedx_open: Accessing the camera

###########################################
############ DMESG [DTS] LOG #############
###########################################

[    0.002357] DTS File Name: /builds/sl/jetson-gmsl-kernel/src/kernel/kernel-5.10/arch/arm64/boot/dts/../../../../../../hardware/nvidia/platform/t23x/p3768/kernel-dts/tegra234-p3767-0001-p3509-a02.dts
[    2.212317] tegra-pmc c360000.pmc: scratch reg offset dts data not present

###########################################
############ DTB list original  ###########
###########################################

/boot/dtb/kernel_tegra234-p3767-0001-p3509-a02.dtb

###########################################
############ DTB list SLabs     ###########
###########################################

/boot/stereolabs/tegra194-p2888-0001-p2822-0000.dtb
/boot/stereolabs/tegra194-p3668-0000-p3509-0000.dtb
/boot/stereolabs/tegra194-p3668-0001-p3509-0000.dtb
/boot/stereolabs/tegra234-p3701-0000-p3737-0000.dtb
/boot/stereolabs/tegra234-p3701-0004-p3737-0000.dtb
/boot/stereolabs/tegra234-p3767-0000-p3509-a02.dtb
/boot/stereolabs/tegra234-p3767-0000-p3768-0000-a0.dtb
/boot/stereolabs/tegra234-p3767-0001-p3509-a02.dtb
/boot/stereolabs/tegra234-p3767-0001-p3768-0000-a0.dtb
/boot/stereolabs/tegra234-p3767-0003-p3509-a02.dtb
/boot/stereolabs/tegra234-p3767-0003-p3768-0000-a0.dtb
/boot/stereolabs/tegra234-p3767-0004-p3509-a02.dtb
/boot/stereolabs/tegra234-p3767-0004-p3768-0000-a0.dtb

/boot/stereolabs/utils:
extlinux.py
fio.py
__pycache__

###########################################
############ EXTlinux file      ###########
###########################################

TIMEOUT 30
DEFAULT Stereolabs

MENU TITLE L4T boot options

LABEL primary
      MENU LABEL primary kernel
      LINUX /boot/Image
      FDT /boot/dtb/kernel_tegra234-p3767-0001-p3509-a02.dtb
      INITRD /boot/initrd
      APPEND ${cbootargs} root=PARTUUID=d74135a3-ccbe-49cc-83e5-3691772f7e0a rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 console=ttyAMA0,115200 firmware_class.path=/etc/firmware fbcon=map:0 net.ifnames=0 

# When testing a custom kernel, it is recommended that you create a backup of
# the original kernel and add a new entry to this file so that the device can
# fallback to the original kernel. To do this:
#
# 1, Make a backup of the original kernel
#      sudo cp /boot/Image /boot/Image.backup
#
# 2, Copy your custom kernel into /boot/Image
#
# 3, Uncomment below menu setting lines for the original kernel
#
# 4, Reboot

# LABEL backup
#    MENU LABEL backup kernel
#    LINUX /boot/Image.backup
#    FDT /boot/dtb/kernel_tegra234-p3767-0001-p3509-a02.dtb
#    INITRD /boot/initrd
#    APPEND ${cbootargs}


LABEL Stereolabs
	MENU LABEL Stereolabs kernel
	LINUX /boot/Image
	FDT /boot/stereolabs/tegra234-p3767-0001-p3509-a02.dtb
	INITRD /boot/initrd
	APPEND ${cbootargs} root=PARTUUID=d74135a3-ccbe-49cc-83e5-3691772f7e0a rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 console=ttyAMA0,115200 firmware_class.path=/etc/firmware fbcon=map:0 net.ifnames=0

####################################
############ Driver list ###########
####################################

/usr/lib/modules/5.10.104-tegra/kernel/drivers/stereolabs/max9296/sl_max9296.ko==> exists
/usr/lib/modules/5.10.104-tegra/kernel/drivers/stereolabs/zedx/sl_zedx.ko ==> exists

################################################
############ ZEDX Daemon Status LS #############
################################################

● zed_x_daemon.service - ZED-X Daemon service
     Loaded: loaded (/etc/systemd/system/zed_x_daemon.service; enabled; vendor preset: enabled)
     Active: active (running) since Mon 2024-07-29 13:50:19 UTC; 1min 58s ago
   Main PID: 2138 (ZEDX_Daemon)
      Tasks: 5 (limit: 8481)
     Memory: 6.5M
     CGroup: /system.slice/zed_x_daemon.service
             └─2138 /usr/sbin/ZEDX_Daemon

Jul 29 13:50:19 GTW-ONX2-D1REMSVZ systemd[1]: Started ZED-X Daemon service.
Jul 29 13:50:19 GTW-ONX2-D1REMSVZ ZEDX_Daemon[2138]: [ "Mon Jul 29 13:50:19 2024" ]  ** Start ZED-X Daemon
Jul 29 13:50:19 GTW-ONX2-D1REMSVZ ZEDX_Daemon[2138]: Tegra release :  9
Jul 29 13:50:19 GTW-ONX2-D1REMSVZ ZEDX_Daemon[2138]: [ "Mon Jul 29 13:50:19 2024" ]  ** Searching for Preload file  "/etc/systemd/system/zed_x_daemon.preload"  :  false
Jul 29 13:50:19 GTW-ONX2-D1REMSVZ ZEDX_Daemon[2138]: [ "Mon Jul 29 13:50:19 2024" ]   Process  "insmod  /usr/lib/modules/5.10.104-tegra/kernel/drivers/stereolabs/max9296/sl_max9296.ko" outputs  "insmod: ERROR: could not insert module /usr/lib/modules/5.10.104-tegra/kernel/drivers/stereolabs/max9296/sl_max9296.ko: File exists\n"
Jul 29 13:50:19 GTW-ONX2-D1REMSVZ ZEDX_Daemon[2138]: [ "Mon Jul 29 13:50:19 2024" ]   Process  "rmmod sl_zedx" outputs  "rmmod: ERROR: Module sl_zedx is in use\n"
Jul 29 13:50:24 GTW-ONX2-D1REMSVZ ZEDX_Daemon[2138]: [ "Mon Jul 29 13:50:24 2024" ]   Process  "insmod  /usr/lib/modules/5.10.104-tegra/kernel/drivers/stereolabs/zedx/sl_zedx.ko" outputs  "insmod: ERROR: could not insert module /usr/lib/modules/5.10.104-tegra/kernel/drivers/stereolabs/zedx/sl_zedx.ko: File exists\n"
Jul 29 13:50:24 GTW-ONX2-D1REMSVZ ZEDX_Daemon[2138]: ** ZED-X Driver loaded
Jul 29 13:50:24 GTW-ONX2-D1REMSVZ ZEDX_Daemon[2138]: [ "Mon Jul 29 13:50:24 2024" ]  ** Searching for Postload file  "/etc/systemd/system/zed_x_daemon.postload"  :  false
Jul 29 13:50:24 GTW-ONX2-D1REMSVZ ZEDX_Daemon[2138]: [ "Mon Jul 29 13:50:24 2024" ]  ** Created Endpoint  "tcp://127.0.0.1:20026"

################################################
############ I2C Trace  [-l]       #############
################################################

i2c-3	i2c       	3190000.i2c                     	I2C adapter
i2c-10	i2c       	i2c-2-mux (chan_id 1)           	I2C adapter
i2c-1	i2c       	c240000.i2c                     	I2C adapter
i2c-8	i2c       	31e0000.i2c                     	I2C adapter
i2c-6	i2c       	31c0000.i2c                     	I2C adapter
i2c-4	i2c       	Tegra BPMP I2C adapter          	I2C adapter
i2c-2	i2c       	3180000.i2c                     	I2C adapter
i2c-0	i2c       	3160000.i2c                     	I2C adapter
i2c-9	i2c       	i2c-2-mux (chan_id 0)           	I2C adapter
i2c-7	i2c       	c250000.i2c                     	I2C adapter
i2c-5	i2c       	31b0000.i2c                     	I2C adapter

################################################
############ I2C Trace /dev/i2C-30 #############
################################################

Error: Could not open file `/dev/i2c-30' or `/dev/i2c/30': No such file or directory

################################################
############ I2C Trace /dev/i2C-31 #############
################################################

Error: Could not open file `/dev/i2c-31' or `/dev/i2c/31': No such file or directory

################################################
############ I2C Trace /dev/i2C-32 #############
################################################

Error: Could not open file `/dev/i2c-32' or `/dev/i2c/32': No such file or directory

################################################
############ I2C Trace /dev/i2C-33 #############
################################################

Error: Could not open file `/dev/i2c-33' or `/dev/i2c/33': No such file or directory
#########################

It seems like i2c 30 to 33 don’t exist and that the modules sl_max9296.ko and sl_zedx fail to be inserted into the kernel. I tried to restart the services, to reboot the ZED Box many times, but nothing works.

Do you have an idea or any suggestion to try? Should I reinstall my ZED Box?
Thanks

Hi @wisteca
did you upgrade the OS of the ZED Box?
Can you try to install the latest version v1.0.5 of the driver?

Hi @Myzhar,

As you suggested, I installed the last version of the driver by following the documentation. It seems to have worked fine and I switched from the v0.6.4 to the v1.0.5. This is the diagnostic :

Created: Tue Jul 30 2024

###########################################
############ DMESG [ZEDX] LOG #############
###########################################

[   13.265340] sl_max9296 9-0048: sl_max9296_parse_serializer_node: DTS loaded for zedx
[   13.431935] sl_max9296 10-0048: sl_max9296_parse_serializer_node: DTS loaded for zedx
[   13.603712] zedx 9-0062: Driver Version : v1.0.5
[   13.603719] zedx 9-0062: Probing v4l2 sensor.
[   13.603723] zedx 9-0062: Driver Version : v1.0.5
[   13.604676] zedx 9-0062: ser_write_reg:i2c write failed: dev. 0x62, reg. 0x10, val. 0x21
[   13.617686] zedx 9-0062: ser_write_table: try 4
[   13.640650] zedx 9-0062: ser_write_reg:i2c write failed: dev. 0x62, reg. 0x10, val. 0x21
[   13.661857] zedx 9-0062: ser_write_table: try 3
[   13.689690] zedx 9-0062: ser_write_reg:i2c write failed: dev. 0x62, reg. 0x10, val. 0x21
[   13.726510] zedx 9-0062: ser_write_table: try 2
[   13.750142] zedx 9-0062: ser_write_reg:i2c write failed: dev. 0x62, reg. 0x311, val. 0x41
[   13.750178] zedx 9-0062: Single ZED-X detect error
[   13.750180] zedx 9-0062: zedx_probe: serializer initialization failed
[   13.750246] zedx: probe of 9-0062 failed with error -1
[   13.750296] zedx 9-0018: Driver Version : v1.0.5
[   13.750298] zedx 9-0018: Probing v4l2 sensor.
[   13.750302] zedx 9-0018: zedx_probe: ar0234 initialization failed
[   13.750335] zedx 9-0010: Driver Version : v1.0.5
[   13.750336] zedx 9-0010: Probing v4l2 sensor.
[   13.750339] zedx 9-0010: zedx_probe: ar0234 initialization failed
[   13.750362] zedx 10-0062: Driver Version : v1.0.5
[   13.750363] zedx 10-0062: Probing v4l2 sensor.
[   13.750365] zedx 10-0062: Driver Version : v1.0.5
[   13.865145] zedx 10-0062: ZED-X serializer detect success
[   13.865247] zedx 10-0018: Driver Version : v1.0.5
[   13.865250] zedx 10-0018: Probing v4l2 sensor.
[   13.865654] zedx 10-0018: tegracam sensor driver:video2_v2.0.6
[   13.961928] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 10-0018 bound
[   13.962962] zedx 10-0018: Detected ZED-X sensor
[   13.963111] zedx 10-0010: Driver Version : v1.0.5
[   13.963113] zedx 10-0010: Probing v4l2 sensor.
[   13.963246] zedx 10-0010: tegracam sensor driver:video3_v2.0.6
[   14.053884] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 10-0010 bound
[   14.054637] zedx 10-0010: Detected ZED-X sensor
[   14.058529] zedx 10-0018: zedx_open: Accessing the camera
[   14.058782] zedx 10-0010: zedx_open: Accessing the camera
[   18.948845] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 10-0010 unbind
[   18.949129] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 10-0018 unbind
[   18.949250] zedx 10-0062: ZED-X serializer successfully removed
[   19.013155] sl_max9296 9-0048: sl_max9296_parse_serializer_node: DTS loaded for zedx
[   19.139731] sl_max9296 10-0048: sl_max9296_parse_serializer_node: DTS loaded for zedx
[   19.283701] zedx 9-0062: Driver Version : v1.0.5
[   19.283707] zedx 9-0062: Probing v4l2 sensor.
[   19.283711] zedx 9-0062: Driver Version : v1.0.5
[   19.284176] zedx 9-0062: ser_write_reg:i2c write failed: dev. 0x62, reg. 0x10, val. 0x21
[   19.292727] zedx 9-0062: ser_write_table: try 4
[   19.313354] zedx 9-0062: ser_write_reg:i2c write failed: dev. 0x62, reg. 0x10, val. 0x21
[   19.321995] zedx 9-0062: ser_write_table: try 3
[   19.337800] zedx 9-0062: ser_write_reg:i2c write failed: dev. 0x62, reg. 0x10, val. 0x21
[   19.346172] zedx 9-0062: ser_write_table: try 2
[   19.361818] zedx 9-0062: ser_write_reg:i2c write failed: dev. 0x62, reg. 0x311, val. 0x41
[   19.370254] zedx 9-0062: Single ZED-X detect error
[   19.370256] zedx 9-0062: zedx_probe: serializer initialization failed
[   19.376974] zedx: probe of 9-0062 failed with error -1
[   19.382323] zedx 9-0018: Driver Version : v1.0.5
[   19.382325] zedx 9-0018: Probing v4l2 sensor.
[   19.382330] zedx 9-0018: zedx_probe: ar0234 initialization failed
[   19.388613] zedx 9-0010: Driver Version : v1.0.5
[   19.388614] zedx 9-0010: Probing v4l2 sensor.
[   19.388617] zedx 9-0010: zedx_probe: ar0234 initialization failed
[   19.394914] zedx 10-0062: Driver Version : v1.0.5
[   19.394916] zedx 10-0062: Probing v4l2 sensor.
[   19.394919] zedx 10-0062: Driver Version : v1.0.5
[   19.505481] zedx 10-0062: ZED-X serializer detect success
[   19.505626] zedx 10-0018: Driver Version : v1.0.5
[   19.505629] zedx 10-0018: Probing v4l2 sensor.
[   19.505803] zedx 10-0018: tegracam sensor driver:video2_v2.0.6
[   19.601635] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 10-0018 bound
[   19.602413] zedx 10-0018: Detected ZED-X sensor
[   19.602512] zedx 10-0010: Driver Version : v1.0.5
[   19.602516] zedx 10-0010: Probing v4l2 sensor.
[   19.602690] zedx 10-0010: tegracam sensor driver:video3_v2.0.6
[   19.605521] zedx 10-0018: zedx_open: Accessing the camera
[   19.693636] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 10-0010 bound
[   19.694170] zedx 10-0010: Detected ZED-X sensor
[   19.697891] zedx 10-0010: zedx_open: Accessing the camera
[  339.737149] Modules linked in: fuse(E) sl_zedx(E) xt_conntrack(E) xt_MASQUERADE(E) nf_conntrack_netlink(E) nfnetlink(E) iptable_nat(E) nf_nat(E) nf_conntrack(E) nf_defrag_ipv6(E) nf_defrag_ipv4(E) libcrc32c(E) sl_max9296(E) xt_addrtype(E) iptable_filter(E) br_netfilter(E) nvidia_modeset(OE) lzo_rle(E) lzo_compress(E) zram(E) overlay(E) ramoops(E) reed_solomon(E) bnep(E) loop(E) iwlmvm(E) hid_logitech_hidpp(E) input_leds(E) mac80211(E) snd_soc_tegra186_asrc(E) snd_soc_tegra186_dspk(E) snd_soc_tegra210_ope(E) snd_soc_tegra210_iqc(E) snd_soc_tegra186_arad(E) snd_soc_tegra210_mvc(E) snd_soc_tegra210_afc(E) snd_soc_tegra210_adx(E) snd_soc_tegra210_dmic(E) snd_soc_tegra210_amx(E) snd_soc_tegra210_admaif(E) snd_soc_tegra210_i2s(E) snd_soc_tegra_pcm(E) snd_soc_tegra210_mixer(E) snd_soc_tegra210_sfc(E) aes_ce_blk(E) crypto_simd(E) cryptd(E) aes_ce_cipher(E) ghash_ce(E) sha2_ce(E) sha256_arm64(E) sha1_ce(E) btusb(E) btrtl(E) btbcm(E) btintel(E) hid_logitech_dj(E) snd_soc_spdif_tx(E)
[  345.771351] zedx 10-0010: zedx_open: Accessing the camera
[  345.771436] zedx 10-0018: zedx_open: Accessing the camera

###########################################
############ DMESG [DTS] LOG #############
###########################################

[    0.002354] DTS File Name: /builds/sl/jetson-gmsl-kernel/src/kernel/kernel-5.10/arch/arm64/boot/dts/../../../../../../hardware/nvidia/platform/t23x/p3768/kernel-dts/tegra234-p3767-0001-p3509-a02.dts
[    2.217783] tegra-pmc c360000.pmc: scratch reg offset dts data not present
[   13.265046] sl_max9296 9-0048: sl_max9296_parse_dt: Number of declared cameras with this dts 1
[   13.431631] sl_max9296 10-0048: sl_max9296_parse_dt: Number of declared cameras with this dts 1
[   19.012913] sl_max9296 9-0048: sl_max9296_parse_dt: Number of declared cameras with this dts 1
[   19.139495] sl_max9296 10-0048: sl_max9296_parse_dt: Number of declared cameras with this dts 1

###########################################
############ DTB list original  ###########
###########################################

/boot/dtb/kernel_tegra234-p3767-0001-p3509-a02.dtb

###########################################
############ DTB list SLabs     ###########
###########################################

/boot/stereolabs/tegra194-p2888-0001-p2822-0000.dtb
/boot/stereolabs/tegra194-p3668-0000-p3509-0000.dtb
/boot/stereolabs/tegra194-p3668-0001-p3509-0000.dtb
/boot/stereolabs/tegra234-p3701-0000-p3737-0000.dtb
/boot/stereolabs/tegra234-p3701-0004-p3737-0000.dtb
/boot/stereolabs/tegra234-p3767-0000-p3509-a02.dtb
/boot/stereolabs/tegra234-p3767-0000-p3768-0000-a0.dtb
/boot/stereolabs/tegra234-p3767-0001-p3509-a02.dtb
/boot/stereolabs/tegra234-p3767-0001-p3768-0000-a0.dtb
/boot/stereolabs/tegra234-p3767-0003-p3509-a02.dtb
/boot/stereolabs/tegra234-p3767-0003-p3768-0000-a0.dtb
/boot/stereolabs/tegra234-p3767-0004-p3509-a02.dtb
/boot/stereolabs/tegra234-p3767-0004-p3768-0000-a0.dtb

/boot/stereolabs/utils:
extlinux.py
fio.py
__pycache__

###########################################
############ EXTlinux file      ###########
###########################################

TIMEOUT 30
DEFAULT Stereolabs

MENU TITLE L4T boot options

LABEL primary
      MENU LABEL primary kernel
      LINUX /boot/Image
      FDT /boot/dtb/kernel_tegra234-p3767-0001-p3509-a02.dtb
      INITRD /boot/initrd
      APPEND ${cbootargs} root=PARTUUID=d74135a3-ccbe-49cc-83e5-3691772f7e0a rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 console=ttyAMA0,115200 firmware_class.path=/etc/firmware fbcon=map:0 net.ifnames=0 

# When testing a custom kernel, it is recommended that you create a backup of
# the original kernel and add a new entry to this file so that the device can
# fallback to the original kernel. To do this:
#
# 1, Make a backup of the original kernel
#      sudo cp /boot/Image /boot/Image.backup
#
# 2, Copy your custom kernel into /boot/Image
#
# 3, Uncomment below menu setting lines for the original kernel
#
# 4, Reboot

# LABEL backup
#    MENU LABEL backup kernel
#    LINUX /boot/Image.backup
#    FDT /boot/dtb/kernel_tegra234-p3767-0001-p3509-a02.dtb
#    INITRD /boot/initrd
#    APPEND ${cbootargs}


LABEL Stereolabs
	MENU LABEL Stereolabs kernel
	LINUX /boot/Image
	FDT /boot/stereolabs/tegra234-p3767-0001-p3509-a02.dtb
	INITRD /boot/initrd
	APPEND ${cbootargs} root=PARTUUID=d74135a3-ccbe-49cc-83e5-3691772f7e0a rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 console=ttyAMA0,115200 firmware_class.path=/etc/firmware fbcon=map:0 net.ifnames=0

####################################
############ Driver list ###########
####################################

/usr/lib/modules/5.10.104-tegra/kernel/drivers/stereolabs/max9296/sl_max9296.ko==> exists
/usr/lib/modules/5.10.104-tegra/kernel/drivers/stereolabs/zedx/sl_zedx.ko ==> exists

################################################
############ ZEDX Daemon Status LS #############
################################################

● zed_x_daemon.service - ZED-X Daemon service
     Loaded: loaded (/etc/systemd/system/zed_x_daemon.service; enabled; vendor preset: enabled)
     Active: active (running) since Tue 2024-07-30 07:01:02 UTC; 5min ago
   Main PID: 1876 (ZEDX_Daemon)
      Tasks: 5 (limit: 8481)
     Memory: 9.9M
     CGroup: /system.slice/zed_x_daemon.service
             └─1876 /usr/sbin/ZEDX_Daemon

Jul 30 07:01:02 GTW-ONX2-D1REMSVZ systemd[1]: Started ZED-X Daemon service.
Jul 30 07:01:02 GTW-ONX2-D1REMSVZ ZEDX_Daemon[1876]: [ "Tue Jul 30 07:01:02 2024" ]  ** Start ZED-X Daemon
Jul 30 07:01:02 GTW-ONX2-D1REMSVZ ZEDX_Daemon[1876]: Tegra release :  9
Jul 30 07:01:02 GTW-ONX2-D1REMSVZ ZEDX_Daemon[1876]: [ "Tue Jul 30 07:01:02 2024" ]  ** Searching for Preload file  "/etc/systemd/system/zed_x_daemon.preload"  :  false
Jul 30 07:01:03 GTW-ONX2-D1REMSVZ ZEDX_Daemon[1876]: ** ZED-X Driver loaded
Jul 30 07:01:03 GTW-ONX2-D1REMSVZ ZEDX_Daemon[1876]: [ "Tue Jul 30 07:01:03 2024" ]  ** Searching for Postload file  "/etc/systemd/system/zed_x_daemon.postload"  :  false
Jul 30 07:01:03 GTW-ONX2-D1REMSVZ ZEDX_Daemon[1876]: [ "Tue Jul 30 07:01:03 2024" ]  ** Created Endpoint  "tcp://127.0.0.1:20026"

################################################
############ I2C Trace  [-l]       #############
################################################

i2c-3	i2c       	3190000.i2c                     	I2C adapter
i2c-10	i2c       	i2c-2-mux (chan_id 1)           	I2C adapter
i2c-1	i2c       	c240000.i2c                     	I2C adapter
i2c-8	i2c       	31e0000.i2c                     	I2C adapter
i2c-6	i2c       	31c0000.i2c                     	I2C adapter
i2c-4	i2c       	Tegra BPMP I2C adapter          	I2C adapter
i2c-2	i2c       	3180000.i2c                     	I2C adapter
i2c-0	i2c       	3160000.i2c                     	I2C adapter
i2c-9	i2c       	i2c-2-mux (chan_id 0)           	I2C adapter
i2c-7	i2c       	c250000.i2c                     	I2C adapter
i2c-5	i2c       	31b0000.i2c                     	I2C adapter

################################################
############ I2C Trace /dev/i2C-30 #############
################################################

Error: Could not open file `/dev/i2c-30' or `/dev/i2c/30': No such file or directory

################################################
############ I2C Trace /dev/i2C-31 #############
################################################

Error: Could not open file `/dev/i2c-31' or `/dev/i2c/31': No such file or directory

################################################
############ I2C Trace /dev/i2C-32 #############
################################################

Error: Could not open file `/dev/i2c-32' or `/dev/i2c/32': No such file or directory

################################################
############ I2C Trace /dev/i2C-33 #############
################################################

Error: Could not open file `/dev/i2c-33' or `/dev/i2c/33': No such file or directory
#########################

The insmod errors disappear and I don’t have the “Failed to connect to Zed X daemon” message anymore, which is great. I can access the camera.
Even though everything seem to work as expected, I see that there are still some I2C related errors, is it a normal behavior using the ZED X or is there still something wrong ?

Thanks

This is expected. I cannot explain why because it’s something related to how the driver works, but you can ignore those lines as long as your cameras work correctly.