Hello I am setting up the zed x camera on a jetson xavier NX using a carrier board from connect tech and the GMSL2 interface card from the stereolabs website.
nvidia@Xavier:~/jetsonUtilities$ python3 jetsonInfo.py
NVIDIA Jetson-AGX
L4T 35.4.1 [ JetPack UNKNOWN ]
Ubuntu 20.04.6 LTS
Kernel Version: 5.10.120-tegra
CUDA 11.4.315
CUDA Architecture: NONE
OpenCV version: 4.5.4
OpenCV Cuda: NO
CUDNN: 8.6.0.166
TensorRT: 8.5.2.2
Vision Works: NOT_INSTALLED
VPI: 2.3.9
Vulcan: 1.3.204
I installed the ZED_SDK_Tegra_L4T35.4_v4.0.7.zstd.run file for the SDK and installed stereolabs-zedx_0.6.1-MAX96712-L4T35.4.1_arm64.deb for the zed X drivers following that and rebooted. However when running any of the examples I get zed camera not found.
nvidia@Xavier:/usr/local/zed/samples/tutorials/tutorial 1 - hello ZED/cpp$ ./ZED_Tutorial_1
Error CAMERA NOT DETECTED, exit program.
I am getting these errors during the startup of the zed x daemon:
nvidia@Xavier:~/jetsonUtilities$ systemctl status zed_x_daemon.service
● zed_x_daemon.service - ZED-X Daemon service
Loaded: loaded (/etc/systemd/system/zed_x_daemon.service; enabled; vendor preset: enabled)
Active: active (running) since Thu 2023-09-28 18:31:30 EDT; 1h 41min ago
Main PID: 1443 (ZEDX_Daemon)
Tasks: 3 (limit: 37110)
Memory: 18.4M
CGroup: /system.slice/zed_x_daemon.service
└─1443 /usr/sbin/ZEDX_Daemon
Sep 28 18:31:30 Xavier systemd[1]: Started ZED-X Daemon service.
Sep 28 18:31:31 Xavier ZEDX_Daemon[1443]: [ "Thu Sep 28 18:31:31 2023" ] ** Start ZED-X Daemon
Sep 28 18:31:31 Xavier ZEDX_Daemon[1443]: [ "Thu Sep 28 18:31:31 2023" ] ** Searching for Preload file "/etc/systemd/system/zed_x_daemon.preload" : false
Sep 28 18:31:31 Xavier ZEDX_Daemon[1443]: [ "Thu Sep 28 18:31:31 2023" ] Process "rmmod sl_zedx" outputs "rmmod: ERROR: Module sl_zedx is not currently loaded\n"
Sep 28 18:31:31 Xavier ZEDX_Daemon[1443]: ** ZED-X Driver loaded
Sep 28 18:31:31 Xavier ZEDX_Daemon[1443]: [ "Thu Sep 28 18:31:31 2023" ] ** Searching for Postload file "/etc/systemd/system/zed_x_daemon.postload" : false
Sep 28 18:31:31 Xavier ZEDX_Daemon[1443]: [ "Thu Sep 28 18:31:31 2023" ] ** Created Endpoint "tcp://127.0.0.1:20026"
The preload and postload files its looking for don’t exist and im not sure how I can force the system to load the sl_zedx module.
nvidia@Xavier:~/jetsonUtilities$ sudo modprobe sl_zedx
[sudo] password for nvidia:
modprobe: FATAL: Module sl_zedx not found in directory /lib/modules/5.10.120-tegra
The ZED_Diagnostic command does not produce any meaningful output.
nvidia@Xavier:~/jetsonUtilities$ sudo ZED_Diagnostic --dmesg
- Running Log Kernel Trace Diagnostic : OK
I am not booting from NVME, my system is running directly from the emmc
nvidia@Xavier:~/jetsonUtilities$ df -h
Filesystem Size Used Avail Use% Mounted on
/dev/mmcblk0p1 28G 19G 7.2G 73% /
none 16G 0 16G 0% /dev
tmpfs 16G 0 16G 0% /dev/shm
tmpfs 3.1G 27M 3.1G 1% /run
tmpfs 5.0M 4.0K 5.0M 1% /run/lock
tmpfs 16G 0 16G 0% /sys/fs/cgroup
tmpfs 3.1G 20K 3.1G 1% /run/user/124
tmpfs 3.1G 8.0K 3.1G 1% /run/user/1000
I do have an nvme drive physically connected, however it is not mounted as a drive in the operating system.
Is there any other tool that can produce logs to debug the connection? Are all the correct versions installed? Is there a way to force the driver to load?
Any help would be appreciated.