Hey,
I just want to validate something using the streaming feature.
a ZED connected to a Jetson streaming to the host PC (windows11).
From the host, I can interact with ZED as if it were directly connected to the host via USB. All features and commands are available, even the ROI option where I can load a png image (sl.Mat.read - sl.set_region_of_interest).