ZED SDK v3.8.2
Download it here.
Bug Fixes
- Fixed Python installation script on Windows, the pyzed whl package URL was incorrectly generated
- Fixed incorrect reporting of ZED Diagnostic tool ‘person reid association’ optimized model status
- Fixed performance regression within the object detection module.
- Fixed object detection module random crash that could happen after a long runtime.
- Fixed incorrect error code returned in case of camera disconnection.
- Fixed a memory leak occurring during SVO recording.
- Fixed
RetrieveImageregression with a custom resolution as parameters. - Fixed CUDA error when using HD2K resolution in body tracking sample.
- Fixed CUDA error occurring when using the combo parameters
enable_right_side_measure+SENSING_MODE::FILLon Jetson. - Fixed random image freeze that can occur after a long runtime.
- Fixed CUDA installation process on Ubuntu Desktop
Known issue
- Maxwell and Kepler GPUs (compute capabilities 35, 50, and 52) are not supported using CUDA 11.X, only with CUDA 10.2
- Windows installers are not signed due to certificate expiry, this should be resolved for the next releases