ZED SDK support for L4T36.5

I have downloaded the ZED SDK for JetPack 6.1 and 6.2 (L4T 36.4) 5.2 (Jetson Orin, CUDA 12.6) for the Jetson Orin Nano. However the I have the Jetpack 6.2(L4T36.5) installed on the Jetson.
Will the downloaded ZED SDK work on it?

Hi @moneeshmohan
As already said in other posts, Jetpack 6.2.2 (L4T36.5) will be supported with the next patch version of the ZED SDK and ZED X Driver that will be released as soon as they complete the Quality tests.

Saw a new release this morning, but no mention of L4T36.5. This jetpack version includes a fix for hardware decoding in chrome here: AV1 encoder disables hardware decoding in Chrome on forceKeyFrame / PLI - Jetson Orin NX - NVIDIA Developer Forums

Any plans to get this in still?

The ZED X Driver for L4T 36.5 is not yet ready, so the ZED SDK patch v5.2.1 does not yet support this version.

The ZED SDK Download page now says that version 5.4 supports L4T 36.5. Is that true? If so, can you also provide an updated zedbox_all_usb_flash script? I tried creating one myself but there appears to be no match for zedbox_rootfs_365.tar on your website.