Hi, I am using 3 Zedx with Jetson Orin AGX, and trying to stream via local network by the Sample.
Hardware:
Zed X *3 with Jetson Orin AGX, PC with RTX 3090.
Platform:
Sender: Jetson Orin AGX JP5.1.2 with a container runing ZED SDK 4.1
Reciever: PC Ubuntu 22.04 with a container runing ZED SDK 4.1
Problems:
I set the sender Depth Mode as NEURAL_PLUS , but the reciever get the init parameter from stream as PERFORMANCE. The point cloud is also PERFORMANCE mode.
sender.py as follows:
import pyzed.sl as sl
init=sl.InitParameters()
init.camera_resolution=sl.RESOLUTION.HD1080
init.camera_fps=30
init.coordinate_units=sl.UNIT.METER
init.depth_maximum_distance=20
# init.depth_mode=sl.DEPTH_MODE.ULTRA
init.depth_mode=sl.DEPTH_MODE.NEURAL_PLUS
zed_list=[]
name_list=[]
cameras=sl.Camera.get_device_list()
for idx,cam in enumerate(cameras):
init.set_from_serial_number(cam.serial_number)
zed_list.append(sl.Camera())
name_list.append(cam.serial_number)
status=zed_list[idx].open(init)
zed_list[idx].set_camera_settings(sl.VIDEO_SETTINGS.EXPOSURE,-1)
zed_list[idx].set_camera_settings(sl.VIDEO_SETTINGS.WHITEBALANCE_AUTO,1)
if status != sl.ERROR_CODE.SUCCESS:
print(repr(status))
zed_list[idx].close()
stream=sl.StreamingParameters()
stream.codec=sl.STREAMING_CODEC.H264
stream.bitrate=8000
stream.port=30000
for zed in zed_list:
err=zed.enable_streaming(stream)
stream.port+=2
while True:
for zed in zed_list:
zed.grab()
pass
here is the senders logs:
[2024-07-15 05:19:22 UTC][ZED][INFO] Logging level INFO
[2024-07-15 05:19:23 UTC][ZED][INFO] [Init] Depth mode: NEURAL PLUS
[2024-07-15 05:19:26 UTC][ZED][INFO] [Init] Camera FW version: 2001
[2024-07-15 05:19:26 UTC][ZED][INFO] [Init] Video mode: HD1080@30
[2024-07-15 05:19:26 UTC][ZED][INFO] [Init] Serial Number: S/N 47253491
[2024-07-15 05:19:29 UTC][ZED][INFO] Logging level INFO
[2024-07-15 05:19:29 UTC][ZED][INFO] [Init] Depth mode: NEURAL PLUS
[2024-07-15 05:19:32 UTC][ZED][INFO] [Init] Camera FW version: 2001
[2024-07-15 05:19:32 UTC][ZED][INFO] [Init] Video mode: HD1080@30
[2024-07-15 05:19:32 UTC][ZED][INFO] [Init] Serial Number: S/N 45705924
[2024-07-15 05:19:33 UTC][ZED][INFO] Logging level INFO
[2024-07-15 05:19:33 UTC][ZED][INFO] [Init] Depth mode: NEURAL PLUS
[2024-07-15 05:19:37 UTC][ZED][INFO] [Init] Camera FW version: 2001
[2024-07-15 05:19:37 UTC][ZED][INFO] [Init] Video mode: HD1080@30
[2024-07-15 05:19:37 UTC][ZED][INFO] [Init] Serial Number: S/N 42570003
[2024-07-15 05:19:38 UTC][ZED][INFO] [Init] Notice: The streaming is using STREAM version 2, enabled by default starting from SDK version 4.1. To revert to the original stream version, set the environment variable "ZED_SDK_STREAM_VERSION" to 1
Opening in BLOCKING MODE
NvMMLiteOpen : Block : BlockType = 4
===== NvVideo: NVENC =====
NvMMLiteBlockCreate : Block : BlockType = 4
H264: Profile = 77, Level = 50
[2024-07-15 05:19:38 UTC][ZED][INFO] [Init] Notice: The streaming is using STREAM version 2, enabled by default starting from SDK version 4.1. To revert to the original stream version, set the environment variable "ZED_SDK_STREAM_VERSION" to 1
NVMEDIA: Need to set EMC bandwidth : 2872000
Opening in BLOCKING MODE
NvMMLiteOpen : Block : BlockType = 4
===== NvVideo: NVENC =====
NvMMLiteBlockCreate : Block : BlockType = 4
H264: Profile = 77, Level = 50
[2024-07-15 05:19:38 UTC][ZED][INFO] [Init] Notice: The streaming is using STREAM version 2, enabled by default starting from SDK version 4.1. To revert to the original stream version, set the environment variable "ZED_SDK_STREAM_VERSION" to 1
NVMEDIA: Need to set EMC bandwidth : 2872000
Opening in BLOCKING MODE
NvMMLiteOpen : Block : BlockType = 4
===== NvVideo: NVENC =====
NvMMLiteBlockCreate : Block : BlockType = 4
H264: Profile = 77, Level = 50
NVMEDIA: Need to set EMC bandwidth : 2872000
NvVideo: bBlitMode is set to TRUE
NvVideo: bBlitMode is set to TRUE
NvVideo: bBlitMode is set to TRUE
[Streaming] Streaming is now running....
[Streaming] Streaming is now running....
[Streaming] Streaming is now running....
[ZED][Streaming] Adding Receiver with IP: 192.168.10.134
[ZED][Streaming] Adding Receiver with IP: 192.168.10.242
[ZED][Streaming] Removing Receiver with IP: 192.168.10.242
[ZED][Streaming] Adding Receiver with IP: 192.168.10.242
[ZED][Streaming] Adding Receiver with IP: 192.168.10.242
[ZED][Streaming] Adding Receiver with IP: 192.168.10.242
[ZED][Streaming] Removing Receiver with IP: 192.168.10.242
[ZED][Streaming] Removing Receiver with IP: 192.168.10.242
[ZED][Streaming] Removing Receiver with IP: 192.168.10.242
[ZED][Streaming] Adding Receiver with IP: 192.168.10.134
[ZED][Streaming] Adding Receiver with IP: 192.168.10.134
[ZED][Streaming] Adding Receiver with IP: 192.168.10.134
the reciever.py:
class Cameras:
def __init__(self,ip_list:list,port_list:list) -> None:
# ip_list: camera ip list
# port_list: camera port list
self._zed_list=[]
for ip,port in zip(ip_list,port_list):
init=sl.InitParameters()
init.set_from_stream(ip,port)
zed=sl.Camera()
err=zed.open(init)
if err != sl.ERROR_CODE.SUCCESS:
exit(1)
self._zed_list.append(zed)
def get_img(self,get_pcd=False,get_depth=False):
img_list=[]
pcd_list=[]
dep_list=[]
serial_number_list=[]
img=sl.Mat()
pcd=sl.Mat()
depth=sl.Mat()
for zed in self._zed_list:
if zed.grab() == sl.ERROR_CODE.SUCCESS:
zed.retrieve_image(img,sl.VIEW.LEFT)
img_ocv=img.get_data()
img_list.append(img_ocv.copy())
serial_number_list.append(zed.get_camera_information().serial_number)
if get_pcd:
zed.retrieve_measure(pcd,sl.MEASURE.XYZRGBA)
pcd_ocv=pcd.get_data()
pcd_list.append(pcd_ocv.copy())
if get_depth:
zed.retrieve_measure(depth,sl.MEASURE.DEPTH)
dep_ocv=depth.get_data()
dep_list.append()(dep_ocv.copy())
data={
'serial_number':serial_number_list,
'img':img_list,
'pcd':pcd_list,
'dep':dep_list
}
return data
if __name__=='__main__':
cams=Cameras(['192.168.10.242','192.168.10.242','192.168.10.242'],[30000,30002,30004])
data=cams.get_img(get_pcd=True)
pass
the reciever logs:
[2024-07-15 05:42:12 UTC][ZED][INFO] Logging level INFO
[Streaming] Warning : receiving port 30000 is not available (already used)... switching to port 30002. Retrying...
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] No backward compatibility required.
[Streaming] Warning: Corrupted frame chunk received (recv: 196 / expect 16100) from ip : 192.168.10.242 at ts 1721022132929(ms)
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[2024-07-15 05:42:14 UTC][ZED][INFO] [Init] Depth mode: PERFORMANCE
[2024-07-15 05:42:14 UTC][ZED][INFO] [Init] Serial Number: S/N 47253491
[2024-07-15 05:42:16 UTC][ZED][INFO] Logging level INFO
[Streaming] Warning : receiving port 30002 is not available (already used)... switching to port 30004. Retrying...
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] No backward compatibility required.
[Streaming] Warning: Corrupted frame chunk received (recv: 196 / expect 16100) from ip : 192.168.10.242 at ts 1721022136070(ms)
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[2024-07-15 05:42:17 UTC][ZED][INFO] [Init] Depth mode: PERFORMANCE
[2024-07-15 05:42:17 UTC][ZED][INFO] [Init] Serial Number: S/N 45705924
[2024-07-15 05:42:18 UTC][ZED][INFO] Logging level INFO
[Streaming] Warning : receiving port 30004 is not available (already used)... switching to port 30006. Retrying...
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] No backward compatibility required.
[Streaming] Warning: Corrupted frame chunk received (recv: 196 / expect 16100) from ip : 192.168.10.242 at ts 1721022138437(ms)
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.
[2024-07-15 05:42:20 UTC][ZED][INFO] [Init] Depth mode: PERFORMANCE
[2024-07-15 05:42:20 UTC][ZED][INFO] [Init] Serial Number: S/N 42570003
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.
[Streaming] Metadata timeout. the size is equal to 16100 instead of 21960. Skipping.