Zed2i cannot use depth viewer on jetson?
I have a Jetson nano installed with sdk3.5.6 and a Jetson NX installed with 3.7.2. Both nano and NX are ubuntu18.04,cuda10.2
And Zed2 works well on jetson Nano and NX.
However, zed2i encountered the following error on the Jetson nano.
And as long as the depth viewer is opened on the Jetson NX, it will flash back.