Hello,
I am experiencing SVO2 recording errors with a ZED X Mini connected to a ZED BOX Mini (Orin NX 16 GB). I recently updated to ZED SDK 5.6.0 and ZED X driver 1.5.0.
The camera opens successfully, but errors appear immediately after recording starts with H264_LOSSLESS or H265_LOSSLESS.
Environment
-
ZED SDK 5.6.0, pyzed 5.6, Python 3.14.3 in Conda.
-
Kernel:
5.15.148-tegra. -
NVIDIA L4T core, camera and multimedia packages:
36.4.7-20250918154033. -
Driver package:
stereolabs-zedbox-mini, version1.5.0-SL-MAX9296-ZEDBOX-MINI-L4T36.4.0. -
Camera firmware: 2001.
Recording configuration and results
I use a Python script with HD1200, 30 FPS, DEPTH_MODE.NONE, SVO2, and the default encoding preset. I tested the following compression modes using the same script and camera settings, saving each run to a separate file. Approximately 133 GB of disk space was available.
| Compression mode | Observed recording behavior |
|---|---|
H264 |
No recording errors observed |
H264_LOSSLESS |
Encoder errors immediately after starting |
H265 |
No recording errors observed |
H265_LOSSLESS |
Repeated NVMAP errors immediately after starting |
LOSSLESS |
No recording errors observed |
The script uses enable_recording() followed by a grab() loop. Its Ctrl+C handler calls disable_recording() and then close().
Error messages
With H264_LOSSLESS:
VENC: NvVideoEncBlockReportError: 2469: BlockSide error 0x4
NvVideoEnc: BlockError
NvVideoEncTransferOutputBufferToBlock: DoWork failed line# 680
NvVideoEnc: NvVideoEncTransferOutputBufferToBlock TransferBufferToBlock failed line=691
With H265_LOSSLESS, these messages repeat:
NVMAP_IOC_READ:1077431815 failed [22]
NVMAP_IOC_WRITE:1077431814 failed [22]
Opening an affected H265_LOSSLESS recording also failed with:
Opening in BLOCKING MODE
NvMMLiteOpen : Block : BlockType = 279
NvMMLiteBlockCreate : Block : BlockType = 279
Segmentation fault (core dumped)
Is there a recommended fix or configuration change?
Thank you.