ZED ROS2 wrapper: restarting one camera changes FPS of all cameras on Jetson

Hi,

I have problem when using zed_ros2_wrapper with 3 zed x mini camera.

Environment:

  • Jetson Orin AGX

  • ZED link duo with 1.4.1 driver

  • ROS2

  • zed-ros2-wrapper run in docker with zedsdk 5.2.3

  • Multiple ZED cameras

  • Each camera runs with a separate ros2 launch command in separate ros2 container with separate config file

  • Each camera uses its own ROS2 launch process

Issue:

When I restart one camera with a lower FPS configuration, the FPS of the other running cameras also decreases automatically.

Example:

  • Camera A: 30 FPS

  • Camera B: 30 FPS

  • Camera C: 30 FPS

If I restart Camera C with 15 FPS:

  • Camera A also drops close to 15 FPS

  • Camera B also drops close to 15 FPS

Questions:

  1. Does the ZED SDK synchronize FPS globally across cameras on Jetson?

  2. Could this be related to USB bandwidth renegotiation or shared GPU/CUDA resources?

  3. Is there a recommended way to isolate FPS/resource scheduling between multiple ZED cameras?

  4. Are there known limitations for multi-camera setups with separate configs on Jetson platforms?

Thank you so much

Hi @vietlh
In a multicamera setup, the cameras of the same block share the same frame rate.
Read more here:

If you want to run a node with a different rate, you can:

You can also dynamically change the publishing rate of the topics.

I recommend you read this section of the documentation for all the details:

Thank you so much, @Myzhar

It is very helpful for me.