ZED Mini Box Carrier Board UART Connection

We have a StereoLabs Mini Carrier Board and are trying to connect a serial device (gimbal) over UART (PINOUT GPIO #09, #10 with ground #08). We are currently unable to get any communication with the serial device.

To isolate the problem, we did a physical loopback test (connecting pin #09 to #10) and could not receive any messages we sent (using pyserial). Tried ttyTHS1, ttyTHS2, and ttyAMA0 (there is no ttyTHS0). Repeated same test with an oscilloscope; same results. On boot, with the oscilloscope attached, we see data output when the boot text scrolls across the screen before the login screen. We have confirmed the same behavior with two Orin NX modules (we only have 1 carrier board).

The user is part of both tty and dialout groups as per this.

What is the configuration to use pins #09 and #10?

Hi @penguin
The UART of the Mini carrier board is connected to the pins of the UART2 of the NVIDIA Jetson module.
UART2 is configured by default as a debug port, and we are working to provide a guide to reconfigure it as a general-purpose UART if possible.

You can read more on this NVIDIA Developer Forum thread

Do you have an approximate timeframe on the guide? We have a deadline approaching and may need to pursue a different solution in the interim. Is there a less ‘invasive’ method to setup a serial device with the carrier board?

Unfortunately, it seems that the debug port cannot be easily reconfigured as a general-purpose port.
We are still investigating to find a way to do that.

If the Mini Carrier Board UART is connected to NVIDIA Module UART2, what is the Mini Carrier Board “DEBUG” (Micro-USB) connected to?

Also, is there a wiring diagram available?

It’s connected to USB0, not to a serial-USB converter.

This is not publicly available.

Hi @Myzhar,

any update on this thread?

Can we then conclude that the UART from the GPIO port of ZED mini carrier cannot be used as a general UART?

Thanks!

Yes, this is the current status.

Hi Myzhar @Myzhar ,

Thanks for the reply.

Then, although I like your carrier design, I still highly suggest you extend the connectivities of the ZED Jetson carrier board in the next generation to make it more competitive. At least +1 USB 3.2 port, + more GPIOs, + UART1. Maybe also a mini PCIe.

Cheers,

Haoming

Hi @hz658832

Thank you for the suggestions. Improvements for the new carrier boards are on the roadmap for 2026.

Would the below work:

sudo systemctl stop nvgetty.service
sudo systemctl disable nvgetty.service

I know in the Jetson Orin Nano Dev kit, this is how you enable the UART port(Pin 8 and 10 on the Expansion Header) to unlock the UART to be used. By default it is used for Debug.

Could the same be applied on the mini carrier board or is it connected to other UART?

Have you tested these commands?

Yes, I have used these on the Jetson Orin Nano Dev Kit and unlocked the UART. Unfortunately, I do not possess a Zed Mini Carrier board or Zed Mini Box to test on them. However, I am keen to know if the commands work as I am planning on buying the mini carrier board.

I tested this idea, trying to use the debugging serial port /dev/ttyTCU0 to connect to Mavros.

Results: It did not work as this is a combined port. It is currently outputting ASCII text (Linux kernel logs). MAVROS is looking at that text, seeing random bytes that accidentally match a MAVLink header start-byte ($0xFD$ or $0xFE$), and then interpreting the following text characters as System and Component IDs.

Cheers,

Haoming

Any updates?

we have our project setup only missing a good way to talk to the autopilot.

Is there a way to get the UART working? in theory Jetson has 2 more UART where did you guys wired them? maybe HW solution is easier?

Yes, a HW upgrade is required. Nothing that can be done without voiding the warranty.

Can you explain more about this HW upgrade? because looks like for now i am stuck with 10 units where the specs say have both CAN and UART, then the manual says there is no CAN transiver and now the forum says no UART. For the intended drone usage, there are not a lot of ways to communicate with the autopilot.

what am I expected to do?

I think you guys need to update the store page for this device these are just wrong

tried a lot with claude to see if i find a solution since all your guys comments here a very vague, this is the result attached, TLDR no way to fix in software.

trying to share the result i either get a not allowed to attach or can have more than 2 links even thou there are no links, i’ll email the result.

You can copy and paste the result if the system does not yet allow you to add a link.

On our side, I can confirm these features for Rev.2 of the Mini Carrier board that will be available starting from July 2026:

  • Support of SUPER mode (40W, MAXN_SUPER)
  • General-purpose UART exposed on GPIO output
  • Automatic Latch reset on shutdown request

I also confirm that the CAN on GPIO will still require a dedicated transceiver before using this connection as a CAN BUS.

So if I will have Rev.2 of the Mini Carrier board,I won’t have the debug UART available?