ZED link Mono compatibility with Seeed j401 carrier board

Hello,

I have been working on setting up the zed x mini cam on the j401 carrier board jetson.

The board is a Jetson Orin Nano dev kit with a non-native seeed studio j401 carrier board (the old carrier board was damaged). I have encountered multiple issues with this setup and have not been able to achieve a camera pipeline. I have reached a stage where it is showing the cam model on the ZED_Explorer, and passing all tests on ZED_Diagnostics except the most critical… the camera test.

I have explored the installed Jetpack versions, the i2c, the pin configuration, the linuxext config file etc. Any tips would be much appreciated - particularly if this could be related to the driver installation for the capture card not being suitable for the j401 carrier board?

Hi @fishinthewater
Welcome to the Stereolabs community.

The ZED GMSL2 cameras are not currently compatible with SeeedStudio carrier boards and devices.

We are working with them to release compatible drivers as soon as possible.
Please stay tuned.

It’s possible to get working without the source code but it’s not ideal. I’ve requested access to the source so I can build a better version but I have this working on reComputer Robotics J4012 with GMSL Extension. Happy to answer any questions @fishinthewater


Hi @night9, I’ve got the same setup, a reComputer Robotics J4012 with the GMSL board, and I’m deciding whether to put a ZED X Mini on it. Honestly a bit surprised there’s still no proper driver for the SeeedStudio boards. How well does it actually work for you, and does the full ZED SDK run (depth, body tracking) or just the raw stream? Thanks!