ZED Link Duo: Is 2x ZED X One 4K + ZED X + ZED X Mini supported simultaneously

Hi,

I’m trying to set up a multi-camera configuration using the ZED Link Duo capture card and running into streaming issues when mixing the ZED X One 4K with other camera models. I’ve done extensive testing and documented all results below.

Environment:

  • Platform: NVIDIA Jetson AGX Orin, JetPack 6.2.1, L4T R36.4.7
  • ZED SDK: v5.2.2 (ZED_SDK_Tegra_L4T36.4_v5.2.2)
  • ZED Link Driver: v1.4.1 (stereolabs-zedlink-duo_1.4.1-LI-MAX96712-L4T36.4.0_arm64)

Port configuration (per documentation):

  • Port #0 (Group B): ZED X One 4K
  • Port #1 (Group B): ZED X
  • Port #2 (Group A): ZED X One 4K
  • Port #3 (Group A): ZED X Mini

Test Results

Test 1 — ZED X + ZED X Mini only (2 cameras)

Ports: #1 (ZED X), #3 (ZED X Mini)

  • :white_check_mark: Detection: OK
  • :white_check_mark: ZED Explorer: Both cameras produce images
  • :white_check_mark: ZED Studio: Simultaneous streaming works perfectly

Test 2 — 2x ZED X One 4K only (2 cameras)

Ports: #0 and #2 (per documentation)

  • :white_check_mark: Detection: OK
  • :white_check_mark: ZED Explorer: Both cameras produce images
  • :white_check_mark: ZED Studio: Simultaneous streaming works perfectly

Test 3 — ZED X + ZED X Mini + ZED X One 4K (3 cameras, 4K on port #2)

Ports: #1 (ZED X), #2 (ZED X One 4K), #3 (ZED X Mini)

  • :white_check_mark: Detection: All 3 cameras recognized
  • :white_check_mark: ZED Explorer: Each camera produces images individually
  • :warning: ZED Studio (attempt A): Opened ZED X first → image OK. Opened ZED X Mini → no image. Tried ZED X One 4K → CAMERA STREAM FAILED TO START (code 28) (See Screenshot 1)
  • :warning: ZED Studio (attempt B): Opened ZED X One 4K first (3840x1200 @ 30fps) → OK. Opened ZED X (1920x1200 @ 30fps) → OK. Tried ZED X Mini → CAMERA STREAM FAILED TO START (code 28) (See Screenshot 2)
  • → Only 2 cameras can stream simultaneously. The 3rd always fails with code 28.

Test 4 — ZED X + ZED X Mini + ZED X One 4K (3 cameras, 4K on port #0)

Ports: #0 (ZED X One 4K), #1 (ZED X), #3 (ZED X Mini)

  • :white_check_mark: Detection: All 3 cameras recognized
  • :warning: ZED Explorer: Unstable — 1st attempt: only ZED X One 4K produces images. 2nd attempt: ZED X One 4K and ZED X Mini produce images but ZED X does not. Results vary each time.
  • :warning: ZED Studio: ZED X One 4K + ZED X Mini stream simultaneously, but ZED X does not produce an image.
  • → Behavior is inconsistent and changes between attempts.

Test 5 — 2x ZED X One 4K + ZED X Mini (3 cameras)

Ports: #0 (ZED X One 4K), #2 (ZED X One 4K), #3 (ZED X Mini)

  • :white_check_mark: Detection: All 3 cameras recognized
  • :warning: ZED Explorer: ZED X One 4K units produce images, but ZED X Mini does not
  • :warning: ZED Studio: ZED X Mini does not produce an image. After closing ZED X Mini and attempting to open a ZED X One 4K, it fails with CAMERA STREAM FAILED TO START (code 28)

Test 6 — All 4 cameras

Ports: #0 (ZED X One 4K), #1 (ZED X), #2 (ZED X One 4K), #3 (ZED X Mini)

  • :white_check_mark: Detection: All 4 cameras recognized
  • :warning: ZED Explorer: Only the two ZED X One 4K units produce images. ZED X and ZED X Mini show either a black screen or the ZED Explorer logo.
  • :warning: ZED Studio: Streaming is very unstable. Opening ZED X and ZED X Mini simultaneously fails with "Couldn't open camera 58252258. Error: CAMERA STREAM FAILED TO START (code 28)". Even opening both ZED X One 4K units simultaneously is inconsistent — sometimes works, sometimes fails with the same error.

Questions:

  1. Is mixing ZED X One 4K with stereo cameras (ZED X / ZED X Mini) on the ZED Link Duo a supported configuration for simultaneous streaming?
  2. If so, is there a specific resolution/FPS setting or driver configuration required to make 3+ cameras stream simultaneously?
  3. Is the code 28 error a known bandwidth limitation of the ZED X One 4K, or could this indicate a hardware/driver issue?

Thank you!


Hi,
Thank you for contacting us and the issue description.

To assist you better, we need additional information regarding your device’s condition and system setup with the 4 cameras connected.
Please open a terminal console (Ctrl+Alt+t) and run these commands:

  • sudo ZED_Diagnostic --dmesg
  • ZED_Diagnostic -c

After executing the commands, kindly send me the files dmesg.log and ZED_Diagnostic_Results.json located in the folder where the commands were run.

Best regards,

Stereolabs Support