ZED Link Duo camera limit clarification - Do ZED X Minis count as 2 cameras each?

Hello,

I have been testing a setup with a Jetson Orin Nano Dev Kit, ZED Link Duo capture card, and a mix of ZED X Mini and ZED X One S cameras (not the 4K variant).

The datasheet states that the Duo capture card “supports up to 4 ZED X GS / ZED X Mini GS / ZED X One GS and up to 2 ZED One 4K”. However, during my testing I encountered unexpected behavior that suggests ZED X Mini cameras may count as two cameras toward this limit rather than one.

my setup:

  • ZED X Mini cameras

  • ZED X One S cameras

  • x1 ZED Link Duo capture card (zed-link-duo driver v1.4.0)

  • x1 Jetson Orin Nano Dev Kit (running Jetpack 6.1 L4T36.4)

  • x1 GMSL2 Fakra 1-to-4 M-F Cable

  • x2 MIPI cables connecting Jetson to capture card

  • Using ZED SDK 4.2.5 with Python (pyzed)

I observed the following:

  • With only x2 ZED X Mini’s connected, I can successfully open all camera streams (L/R of each)

  • With only x4 ZED X One S cameras connected, I can successfully open all streams.

  • With x2 ZED X Mini’s and x2 ZED X One S cameras connected, I get CAMERA_NOT_DETECTED for the monocular cameras, and the X Mini will sometimes work but usually not.

    • dmesg shows all 4 cameras are detected & bound to tegra-capture-vi at boot
    • 6 cameras appear as video0-5, in /dev/video*

My main question is does each ZED X Mini count as 2 cameras toward the 4-camera limit of the duo capture card since it’s stereo? Are there any ways around this that allow us to consider a ZED X Mini as a single camera and capture both feeds? My goal is to have multiple camera streams running as ROS topics at once but I want to be clear on the limitations of the duo capture card.

Thank you!

Hi @marcel123
Welcome to the Stereolabs community.

No, it doesn’t. Each Stereo camera counts as a single connected device.

I recommend you check the supported multi-camera combination and be sure that you connected the devices in the correct way: