ZED Link Drivers v1.3.0 is missing support for JP6.2.1 (l4t 36.4.4)

Hello,

when trying to install ZED Link Mono v1.3.0 (stereolabs-zedlink-mono_1.3.0-SL-MAX9296-all-L4T36.4.0_arm64.deb) on a freshly flashed Nvidia Jetson Orin NX with Jetpack 6.2.1 the installation fails with:

sudo dpkg -i ./stereolabs-zedlink-mono_1.3.0-SL-MAX9296-all-L4T36.4.0_arm64.deb 
Selecting previously unselected package stereolabs-zedlink-mono.
(Reading database ... 193624 files and directories currently installed.)
Preparing to unpack .../stereolabs-zedlink-mono_1.3.0-SL-MAX9296-all-L4T36.4.0_arm64.deb ...
Unpacking stereolabs-zedlink-mono (1.3.0-SL-MAX9296-all-L4T36.4.0) ...
dpkg: dependency problems prevent configuration of stereolabs-zedlink-mono:
 stereolabs-zedlink-mono depends on nvidia-l4t-kernel (<= 5.15.148-tegra-36.4.3-20250107174145); however:
  Version of nvidia-l4t-kernel on system is 5.15.148-tegra-36.4.4-20250616085344.

dpkg: error processing package stereolabs-zedlink-mono (--install):
 dependency problems - leaving unconfigured
Errors were encountered while processing:
 stereolabs-zedlink-mono

when is support fot JP6.2.1 expected to be added?
Thanks!

Hi @beniaminopozzan
Jetson Linux v36.4.4 (JP6.2.1) has just been released.
The team is working on an upgrade of the ZED X Driver to support it.
The release is expected in a few days. It’s currently in the QA stage.

Hi Myzhar,
can you tell when the new driver will be available?
Thank you

Hi @Jana
Welcome to the StereoLabs community.
The driver will be available very soon.