Zed Fusion silent crashing in both python and c++

Hey, I have an issue using ZED Fusion. I am developing a python app that uses 2 Zed2i cameras for spatial mapping. The cameras both work fine on their own, and work fine when used together without Fusion.
When I tried using Fusion my python app silent crashes, I looked into it and found this discussion, so I decided to try to do it in C++. I copied the multi camera spatial mapping project from this link. When I tried to build it and the run it I ran into the same issue I had with Python. The viewer screen popped up, switched to a gray background and then it crashed without any error messages.

I tried using Zed SDK versions 5.2.0 and 5.2.1 and got the same result.

I have the config file and I can also provide my Python code but it won’t let me upload files because I am a new user.

Also it might be connected to this issue, when I try running the Zed Diagnostic tool with both cameras connected it works fine, but when I try to run it with only one of the cameras it crashes at the “Camera Test“ part with 10% . It does the same for both of my cameras if only one of them is connected.

Hi @vass.kornel
Welcome to the Stereolabs community.

Please add details concerning your setup:

  • PC type
  • OS Type
  • OS version
  • GPU type
  • …

PC type: Laptop
OS type: Windows 11 Enterprise
OS version: 25H2
GPU type: NVIDIA 3070 Laptop GPU

I tried running it on multiple devices and got the same issue.

Hi @vass.kornel
We noted the issue. It will be fixed with one of the next versions of the ZED SDK.

Hello

Is there an update on this issue, is it fixed now or is it still not working?