ZED Fusion offline

Hello,

I have the following setup:

ZEDBox Orin NX16GB

ZEDX camera GMSL

ZEDX mini camera GMSL

Both cameras attached to a mobile rig, and setup calibrated with ZED360 app.

Question #1: is this assimetric configuration valid for Fusion?

I have written an app that runs capture to SVO in parallel on both cameras. For higher FPS, I used NEURAL_LIGHT depth mode.

Question #2 : Would it be possible to configure the fusion of the two SVO files with a higher depth mode(NEURAL_PLUS), considering the fusion will run offline (Windows PC , RTX 5090)?

Thank you.

Yes, you can use any kind of camera as long as the Field of Views overlap.

Yes, the SVO does not store depth information. The depth is processed at runtime while the SVO file is read.
You can disable the depth processing (Depth Mode = NONE) to improve the performance while recording.

I recommend you explore this example: zed-sdk/recording/recording/multi camera at master · stereolabs/zed-sdk · GitHub