Hi, thanks!
To reproduce it you just need to create an empty Unity project (3d core), import the Zed unity package and add one Zed_Rig_Mono prefab and then the Zed_Rig_Stereo prefab to your scene.
-At this point none of the cameras should work.
-If you now remove the Zed_Rig_Mono prefab from your scene the Right_eye camera should start to work, but not the left.
Below is my Diagnostic result, I dont have a camera connected, but I shouldnt need to for this?
{
“AI Models”: {
“info”: [
“MULTI CLASS DETECTION is not optimized”,
“MULTI CLASS MEDIUM DETECTION is not optimized”,
“MULTI CLASS ACCURATE DETECTION is not optimized”,
“HUMAN BODY FAST DETECTION is not optimized”,
“HUMAN BODY MEDIUM DETECTION is not optimized”,
“HUMAN BODY ACCURATE DETECTION is not optimized”,
“HUMAN BODY 38 FAST DETECTION is not optimized”,
“HUMAN BODY 38 MEDIUM DETECTION is not optimized”,
“HUMAN BODY 38 ACCURATE DETECTION is not optimized”,
“PERSON HEAD DETECTION is not optimized”,
“PERSON HEAD ACCURATE DETECTION is not optimized”,
“REID ASSOCIATION is not optimized”,
“NEURAL DEPTH is not optimized”
]
},
“Camera Test”: {
“InternalDevicesCount”: 0,
“ZEDCount”: 0,
“error”: [
“Camera not detected
Make sure the camera is plugged in or try another USB 3.0 port.”
]
},
“Devices”: {
“ASMediaFound”: false,
“CorruptedFirmware”: false,
“OC_Cam_Detected”: false,
“OtherUSBDevices”: [
{
“USBMode”: 3,
“USB_path”: “/3/2”,
“bDescriptorType”: 1,
“bDeviceProtocol”: 0,
“bLength”: 18,
“bMaxPacketSize0”: 9,
“bNumConfigurations”: 2,
“bcdDevice”: “49.0”,
“bcdUSB”: “3.0”,
“bcdUSBClass”: 0,
“bcdUSBSubClass”: 0,
“busNumber”: 3,
“iManufacturer”: 1,
“iProduct”: 2,
“iSerial”: 6,
“idProduct”: 33107,
“idVendor”: 3034
}
],
“USBList”: [
{
“USB_path”: “/3”,
“idProduct”: “0x0820”,
“idVendor”: “0x2109”
},
{
“USB_path”: “/1/1”,
“idProduct”: “0xc412”,
“idVendor”: “0x06c4”
},
{
“USB_path”: “/10”,
“idProduct”: “0x1866”,
“idVendor”: “0x0b05”
},
{
“USB_path”: “/10”,
“idProduct”: “0x1866”,
“idVendor”: “0x0b05”
},
{
“USB_path”: “/3/2”,
“idProduct”: “0x8153”,
“idVendor”: “0x0bda”
},
{
“USB_path”: “/4”,
“idProduct”: “0xc52b”,
“idVendor”: “0x046d”
},
{
“USB_path”: “/3”,
“idProduct”: “0xc05b”,
“idVendor”: “0x046d”
},
{
“USB_path”: “/1”,
“idProduct”: “0x2820”,
“idVendor”: “0x2109”
},
{
“USB_path”: “/14”,
“idProduct”: “0x0026”,
“idVendor”: “0x8087”
},
{
“USB_path”: “/5”,
“idProduct”: “0xc215”,
“idVendor”: “0x046d”
}
],
“ZEDDetected”: null,
“captureDevices”: [
],
“controllers”: [
{
“CompatibleIDs”: “”,
“Description”: “USB Root Hub (USB 3.0)”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0005”,
“Location”: “”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-2”
},
{
“CompatibleIDs”: “PCI\VEN_8086&DEV_15E9&REV_06”,
“Description”: “USB xHCI Compliant Host Controller”,
“DeviceName”: “Intel(R) USB 3.1 eXtensible Host Controller - 1.10 (Microsoft)”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0002”,
“Location”: “PCI bus 6, device 0, function 0”,
“Manufacturer”: “Generic USB xHCI Host Controller”,
“Name”: “PCI”,
“PhysicalName”: “\Device\NTPNP_PCI0029”
},
{
“CompatibleIDs”: “USB\USB30_HUB”,
“Description”: “Generic SuperSpeed USB Hub”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0031”,
“Location”: “Port_#0003.Hub_#0003”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-3”
},
{
“CompatibleIDs”: “PCI\VEN_8086&DEV_06ED&REV_00”,
“Description”: “USB xHCI Compliant Host Controller”,
“DeviceName”: “Intel(R) USB 3.1 eXtensible Host Controller - 1.10 (Microsoft)”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0000”,
“Location”: “PCI bus 0, device 20, function 0”,
“Manufacturer”: “Generic USB xHCI Host Controller”,
“Name”: “PCI”,
“PhysicalName”: “\Device\NTPNP_PCI0006”
},
{
“CompatibleIDs”: “USB\USB20_HUB”,
“Description”: “Generic USB Hub”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0011”,
“Location”: “Port_#0001.Hub_#0001”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-5”
},
{
“CompatibleIDs”: “PCI\VEN_10DE&DEV_1ADA&REV_A1”,
“Description”: “USB xHCI Compliant Host Controller”,
“DeviceName”: “NVIDIA USB 3.10 eXtensible Host Controller - 1.10 (Microsoft)”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0001”,
“Location”: “PCI bus 1, device 0, function 2”,
“Manufacturer”: “Generic USB xHCI Host Controller”,
“Name”: “PCI”,
“PhysicalName”: “\Device\NTPNP_PCI0021”
},
{
“CompatibleIDs”: “”,
“Description”: “USB Root Hub (USB 3.0)”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0003”,
“Location”: “”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-1”
},
{
“CompatibleIDs”: “”,
“Description”: “USB Root Hub (USB 3.0)”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0004”,
“Location”: “”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-0”
}
],
“notTested”: [
“Please connect a camera to test the USB connection.”
]
},
“Graphics Card”: {
“deviceCount”: 1,
“deviceDriverVersion”: 12010,
“devices”: [
{
“arch”: “Turing”,
“computeCapability”: “7.5”,
“cores”: 4608,
“name”: “NVIDIA GeForce RTX 2070 with Max-Q Design”,
“totalMemoryBytes”: “8589606912”,
“totalMemoryMB”: 8191.6875
}
],
“initResult”: 0,
“valid”: [
“Graphics card: NVIDIA GeForce RTX 2070 with Max-Q Design”
]
},
“Processor”: {
“OS”: “Windows 10 FallCreators”,
“avxSupported”: true,
“coreCount”: “6”,
“cpu”: “Intel(R) Core™ i7-10750H CPU @ 2.60GHz”,
“datetime”: “2024-04-04 11:17:19”,
“hyperThreading”: “1”,
“motherboard”: “GU502LW, ASUSTeK COMPUTER INC.”,
“ramCapacity”: “15.7875”,
“ramUsage”: “0”,
“ramUsed”: “8.91037”,
“threadCount”: “12”,
“valid”: [
“Processor: Intel(R) Core™ i7-10750H CPU @ 2.60GHz”,
“Motherboard: GU502LW, ASUSTeK COMPUTER INC.”
]
},
“ZED SDK”: {
“CUDA Toolkit version”: “V12.1.105 -->located in C:/Program Files/NVIDIA GPU Computing Toolkit/CUDA/v12.1/bin/nvcc.exe”,
“CUDA loading”: false,
“ZED SDK Version (Diag)”: “4.0.8”,
“ZED SDK Version (RT)”: “4.0.8”,
“ai”: {
“checkAI”: true,
“cudaVersion”: 12010,
“cudnnCudartVersion”: 12000,
“cudnnVersion”: 8801,
“cudnnVersionExpected”: 8801,
“tensorVersion”: 8600
},
“binFiles”: [
“cudnn64_8.dll”,
“cudnn_adv_infer64_8.dll”,
“cudnn_adv_train64_8.dll”,
“cudnn_cnn_infer64_8.dll”,
“cudnn_cnn_train64_8.dll”,
“cudnn_ops_infer64_8.dll”,
“cudnn_ops_train64_8.dll”,
“nvinfer.dll”,
“nvinfer_builder_resource.dll”,
“nvinfer_dispatch.dll”,
“nvinfer_lean.dll”,
“nvinfer_plugin.dll”,
“nvinfer_vc_plugin.dll”,
“nvonnxparser.dll”,
“nvparsers.dll”,
“sl_ai64.dll”,
“sl_zed64.dll”,
“zlibwapi.dll”
],
“driverVersion”: “531.14”,
“drivervDllVersion”: “31.0.15.3114”,
“resourcesFiles”: [
],
“resourcesFilesExpected”: [
“objects_performance_3.2”
],
“runtimeDllVersion”: 12010,
“valid”: [
“ZED SDK version: 4.0.8”,
“CUDA version: V12.1.105”
]
}
}