[ZED][Encoding] Critical Error : No Video Enc [enc_0]

I cannot record on GPU. When I use the H.264 or H.265, It shows this

han@ubuntu:/usr/local/zed/tools$ sudo ./ZED_Explorer 
[sudo] password for han: 
QStandardPaths: XDG_RUNTIME_DIR not set, defaulting to '/tmp/runtime-root'
 ** [SVO] Hardware compression (NVENC) available **
[ZED][Encoding] Critical Error : No Video Enc [enc_0]
[ZED][Encoding] Critical Error : No Video Enc [enc_0]
[ZED][Streaming] Failed to create encoder [0.0] at resolution 1920x1080
[ERROR] Can't start streaming with the provided parameters 
Stack trace (most recent call last):
#31   Object "/usr/lib/aarch64-linux-gnu/libc.so.6", at 0xffffa56c73fb, in 
#30   Object "./ZED_Explorer", at 0x43cb6b, in 
#29   Object "/usr/lib/aarch64-linux-gnu/libQt5Core.so.5", at 0xffffa5df41cb, in QCoreApplication::exec()
#28   Object "/usr/lib/aarch64-linux-gnu/libQt5Core.so.5", at 0xffffa5deb06b, in QEventLoop::exec(QFlags<QEventLoop::ProcessEventsFlag>)
#27   Object "/usr/lib/aarch64-linux-gnu/libQt5Core.so.5", at 0xffffa5e4b523, in QEventDispatcherGlib::processEvents(QFlags<QEventLoop::ProcessEventsFlag>)
#26   Object "/usr/lib/aarch64-linux-gnu/libglib-2.0.so.0", at 0xffffa21b2f13, in g_main_context_iteration
#25   Object "/usr/lib/aarch64-linux-gnu/libglib-2.0.so.0", at 0xffffa220aebb, in 
#24   Object "/usr/lib/aarch64-linux-gnu/libglib-2.0.so.0", at 0xffffa21b5a6f, in g_main_context_dispatch
#23   Object "/usr/lib/aarch64-linux-gnu/libQt5XcbQpa.so.5", at 0xffff9afcf267, in 
#22   Object "/usr/lib/aarch64-linux-gnu/libQt5Gui.so.5", at 0xffffa6199393, in QWindowSystemInterface::sendWindowSystemEvents(QFlags<QEventLoop::ProcessEventsFlag>)
#21   Object "/usr/lib/aarch64-linux-gnu/libQt5Gui.so.5", at 0xffffa61c211f, in QGuiApplicationPrivate::processMouseEvent(QWindowSystemInterfacePrivate::MouseEvent*)
#20   Object "/usr/lib/aarch64-linux-gnu/libQt5Core.so.5", at 0xffffa5decb8f, in QCoreApplication::notifyInternal2(QObject*, QEvent*)
#19   Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa82c2abf, in QApplicationPrivate::notify_helper(QObject*, QEvent*)
#18   Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa832298b, in 
#17   Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa831fd0f, in 
#16   Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa82c96e3, in QApplicationPrivate::sendMouseEvent(QWidget*, QMouseEvent*, QWidget*, QWidget*, QWidget**, QPointer<QWidget>&, bool, bool)
#15   Object "/usr/lib/aarch64-linux-gnu/libQt5Core.so.5", at 0xffffa5decb8f, in QCoreApplication::notifyInternal2(QObject*, QEvent*)
#14   Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa82cafcb, in QApplication::notify(QObject*, QEvent*)
#13   Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa82c2abf, in QApplicationPrivate::notify_helper(QObject*, QEvent*)
#12   Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa8306377, in QWidget::event(QEvent*)
#11   Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa84af263, in QToolButton::mouseReleaseEvent(QMouseEvent*)
#10   Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa83aea13, in QAbstractButton::mouseReleaseEvent(QMouseEvent*)
#9    Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa83ae78b, in 
#8    Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa83acb5b, in 
#7    Object "/usr/lib/aarch64-linux-gnu/libQt5Widgets.so.5", at 0xffffa83ac8bb, in QAbstractButton::clicked(bool)
#6    Object "/usr/lib/aarch64-linux-gnu/libQt5Core.so.5", at 0xffffa5e27913, in 
#5    Object "./ZED_Explorer", at 0x49982f, in 
#4    Object "./ZED_Explorer", at 0x4be1b3, in 
#3    Object "./ZED_Explorer", at 0x611fb3, in 
#2    Object "./ZED_Explorer", at 0x611ad3, in 
#1    Object "./ZED_Explorer", at 0x65a11b, in 
#0    Object "/usr/lib/aarch64-linux-gnu/libc.so.6", at 0xffffa5720610, in pthread_mutex_lock
Segmentation fault (Address not mapped to object [0x118])
Segmentation fault```

Hi @han12580
What’s your host device or GPU model?

No host. Do you mean this?


The Jetson Orin Nano is your host, the ZED is the device.
The Jetson Orin Nano has no hardware encoders, so you cannot use H264/H265 compression when recording SVOs.

OK THANKS.
When recording SVOs, It has many dropped frames. The FPS just is 10. How to up? The Jetson Orin Nano(8G) uses SSD.

You need and SSD with a fast write speed and you must be sure that the resolution/framerate settings are correctly handled by the Orin Nano.
You should also set the Orin into 15W power mode (10W if an Orin Nano 4GB) and run the jetson_clocks.sh script to use the maximum available computing power.

I’ve run into the same issue. Could you let me know which Jetson or other edge devices support using H264/H265 compression for recording SVOs? Looking forward to your reply.

Only the Jetson Orin Nano does not have hardware encoders.

You could consider using our ZED Box, ZED Box Mini, or Mini Carrier board with a Jetson Orin NX module