ZED Depth Viewer crash. (Version 3.7.5)

ZED Depth Viewer crash, and in Unity example some scene works fine but skeleton demo and others will crash while play the scene.
However ZED Depth Viewer works with zed sdk 3.6.5…
And also I found that while running the Zed Diagnostic, it will crash on the ‘AI Model’ step.

ps : I Noticed that there is a warning while Diagnostic on step ‘ZED SDK’. It says ‘Object detection module corrupted. Please reinstall the ZED SDK and enable the Object Detection option.’.
And I reinstalled it but there are no option for that …

I tried on different pc but still same issue. These are my environments:

Environment 1

Issue : 1. Diagnostic crash while step ‘AI Model’. 2. Depth Viewer crash. 3. Unity skeleton demo scene crash while playing. 4. Normal while using Zed 3.6.5 sdk, Cuda 11.5, Unity sample 3.6.4

  • ZED2 Stereo Camera
  • Zed 3.7.5 sdk
  • Cuda 11.7
  • Victus by HP Laptop 16-e0xxx
  • Windows 11 Pro 64bit
  • AMD Ryzen 7 5800H with Radeon Graphics (16CPUs), ~3.2GHz
  • 32768MB RAM
  • NVIDIA GeForce RTX 3060 Laptop GPU

Environment 2

Issue : Same as last one.

  • ZED2 Stereo Camera
  • Zed 3.7.5 sdk
  • Cuda 11.7
  • Windows 10 Pro 64bit
  • Intel(R) Core™ i9-10900KF CPU @ 3.70GHz (20CPUs), ~3.7GHz
  • 65534MB RAM
  • NVIDIA GeForce RTX 3080

2022 07 19 17:06

Recently I tried on another computer.. So strange that on this computer has no such issue..

Environment 3

No issue.

  • ZED2 Stereo Camera
  • Zed 3.7.5 sdk
  • Cuda 11.7
  • Windows 10 Home 64bit
  • Intel(R) Core™ i7-9700K CPU @ 3.60Hz (8 CPUs), ~3.6GHz
  • 32768MB RAM
  • NIVIDIA GeForce RTX 2070

ps: Even with normal environment, I found that it’s so long time to wait for initialize at unity skeleton demo scene while playing it first time. Almost need to wait for 3 ~ 4 min for first play that scene and unity stops until it initialized completely.

We are sorry for the inconvenience, but the new SDK v3.7.5 has a problem with Windows. The team is working on a patch and we will release it as soon as possible.

Meanwhile, you can download and install the previous version:
https://stereolabs.sfo2.cdn.digitaloceanspaces.com/zedsdk/3.7/ZED_SDK_Windows10_cuda11.5_v3.7.4.exe

A new release is out