Myzhar
November 17, 2023, 2:44pm
2
Hi @stalbot
Welcome to the Stereolabs community.
The problem is that you are trying to build a Linux package with the ZED SDK installed in the Windows OS.
You must install the ZED SDK also in Ubuntu in WSL2 and use this to build the ROS 2 Wrapper.
Your problem is similar to this:
Good Morning, i have this problem with zed-wrapper package.
Conf.
Ubuntu 22.04 - WSL2
ROS 2 Humble
SDK (on windows) 4.0.8
zed-ros2-wrapper got from git clone --recursive GitHub - stereolabs/zed-ros2-wrapper: ROS 2 wrapper for the ZED SDK
I have this error and can’t build zed-wrapper. Had some problems with zed-component but i fixed it with the installation of the right version of CUDA and SDK but can’t figure out of this.
Finished <<< zed_components [1min 14s]
Starting >>> zed_wrapper
[Pr…