ZED Calibration Tool is always stuck during camera opening, Jetson AGX Orin 64gb, L4T 36.4.7, ZED SDK 5.1.1, 3 ZEDx Mini via Quad Capture Card

Hi there,

I realized that the point cloud of a flat box surface gets bent significantly when moving the object more than a meter away from the ZEDx mini. I am using the NEURAL depth mode at 30Hz with SVGA resolution. Self-calibration is always skipped, even though I am already placing many different objects, including a calibration board, into the scene. I tried using the ZED calibration tool, but it is stuck during camera opening. What could be the problem with the calibration tool? ZED Diagnosis shows no issues, and with ZED Explorer, I can open all three connected ZEDx mini cameras.

Thanks for your help!