ZED Box Orin NX for running two Zed 2i cameras

Before purchasing a ZED Box, i would like to know
For the 2 options ZED Box Orin NX 8GB and 16GB.
If i am only running the recording module of ZED SDK, such as ZED_Explorer, can it run two or even more Zed 2i cameras simultaneously? as the vRAM should only affect AI computations when retrieving depth from the SDK?

Thanks in advance!

Hi @jerrytamchiho
Welcome to the Stereolabs community

For multicamera configuration, the 16GB version is recommended.
Recording is a high demanding task

Hi again.
I have just tried running 2 sessions of ZED_Explorer for recording on 2 Zed 2i cameras on the 16GB version box. However, once i use the 1080p30 config for both cameras, the frame drop is huge, dropping around 10% of frames. The settings works totally fine if one of the camera if tunned down to 720p30.
Is that an expected behavior?