Zed Box orin NX 16gb fsia6b kernel

I am currently working with the Zed Box and trying to enable the FlySky FS-iA6B joystick driver in the kernel. However, after configuring and building the kernel, the device fails to boot properly, and I am presented with a blinking cursor.
Steps Taken So Far:

Kernel Configuration:

  • Used the linux-source-5.15.0 provided with the system.

  • Configured the kernel using:
    make defconfig
    make menuconfig

  • Enabled the FlySky driver under Device Drivers > Input Device Support > Joystick Interface.

Kernel Build and Installation:
Built the kernel and modules using:

    make -j$(nproc)
    sudo make modules_install
    sudo cp arch/arm64/boot/Image /boot/Image

Rebooted the system.

Outcome:
After rebooting, the system gets stuck at a blinking cursor. I can access the shell from the UEFI interface but cannot boot successfully into the system.

Questions:

  • Is the FlySky FS-iA6B driver fully supported on the Zed Box’s custom kernel (5.15.136-tegra)?
  • Are there any known compatibility issues or additional steps required to make this work on the Jetson Orin NX platform?
  • Does the Zed Box require a custom patch or kernel source for hardware-specific features?
  • Could the issue be related to the custom bootloader or initramfs setup on this platform?

System Information:

Device: NVIDIA Jetson Orin NX (Custom Zed Box)
Kernel Version: 5.15.136-tegra
JetPack Version: 36.3.0
OS: Ubuntu 22.04.5 LTS (aarch64)

Any guidance or suggestions would be greatly appreciated. Let me know if additional logs or system details are required.

I have the same issue with USB Prolific PL2303 Single Port Serial Driver

I have tried it with Jetpack version: 34.4.1 there the usbs both get shown but the jstest-gtk still does not work