On the installation side, is there a known connection issue if the ZED Box Mini connects to a wall plate which runs back to a patch bay and then to the switch?
Hi @brian1,
Welcome to the StereoLabs community.
No, there is no known issue with this kind of installation. The ZED Box Mini uses a standard Gigabit Ethernet port, and a structured cabling path (device, wall plate, permanent run, patch panel, switch) is electrically seen as a single passive link, exactly like a direct cable to the switch.
To get a reliable Gigabit link, the cabling must respect the standard IEEE 802.3 requirements:
- total channel length (patch cords plus permanent run) within 100 m;
- Cat5e cable or better along the whole path, including wall plate and patch panel;
- all 4 pairs correctly terminated, with the same scheme (T568A or T568B) on both ends and no split pairs.
If you are already experiencing connection problems, a few checks can quickly isolate the cause:
- run
ethtool <interface>on the ZED Box Mini to verify the negotiated speed and duplex; a link stuck at 100 Mb/s is a typical sign of a damaged pair or a bad termination in the building cabling; - run
ip -s link show <interface>to check for RX/TX errors; - connect the ZED Box Mini directly to the switch with a known-good patch cord to compare the behavior;
- verify the switch port configuration (VLAN, port security, 802.1X), which is common in managed networks and can block or restrict the connection.
If you share more details about the symptoms you observe (no link, low speed, disconnections, streaming issues), we can help you further.
You can find more information about the setup in the ZED Box Mini installation guide and about the full ZED Box family on the StereoLabs website.
Best regards,
Walter