Zed box mini installation

Hello,

While trying to install the zed box mini I immidetiatly ran into errors while trying to do a sudo apt upgrade.

dpkg: error processing package nvidia-l4t-kernel-dtbs (–configure):
dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of stereolabs-zedbox-mini:
stereolabs-zedbox-mini depends on nvidia-l4t-rt-kernel (>= 5.15.148-rt-tegra-36.4.0-20240912212859) | nvidia-l4t-kernel (>= 5.15.148-tegra-36.4.0-20240912212859); however:
Package nvidia-l4t-rt-kernel is not installed.
Package nvidia-l4t-kernel is not configured yet.
stereolabs-zedbox-mini depends on nvidia-l4t-rt-kernel (<= 5.15.148-rt-tegra-36.4.4-20250616085344) | nvidia-l4t-kernel (<= 5.15.148-tegra-36.4.4-20250616085344); however:
Package nvidia-l4t-rt-kernel is not installed.
Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package stereolabs-zedbox-mini (–configure):
dependency problems - leaving unconfigured
Processing triggers for nvidia-l4t-initrd (36.4.4-20250616085344) …

Errors were encountered while processing:
nvidia-l4t-bootloader
nvidia-l4t-kernel
nvidia-l4t-kernel-headers
nvidia-l4t-jetson-io
nvidia-l4t-kernel-oot-modules
nvidia-l4t-display-kernel
nvidia-l4t-kernel-oot-headers
nvidia-l4t-kernel-dtbs
stereolabs-zedbox-mini
E: Sub-process /usr/bin/dpkg returned an error code (1)

I haven’t really done anything yet… Can you please help me resolve this, should i do a flash to reset/upgrade?

this is my nv_tegra_release

user@GTW-ONX1-D2KU7YCE:~$ cat /etc/nv_tegra_release
# R36 (release), REVISION: 4.4, GCID: 41062509, BOARD: generic, EABI: aarch64, DATE: Mon Jun 16 16:07:13 UTC 2025
# KERNEL_VARIANT: oot
TARGET_USERSPACE_LIB_DIR=nvidia
TARGET_USERSPACE_LIB_DIR_PATH=usr/lib/aarch64-linux-gnu/nvidia

Kind regards

Ceder Wink

Hi Ceder,

This is the procedure to fix the issue:

sudo apt-get autocleansudo mv /var/lib/dpkg/info/ /var/lib/dpkg/backup/sudo mkdir /var/lib/dpkg/info/sudo apt-get updatesudo apt-get -f install

Then reinstall the ZED X Driver.

Please confirm that it works for you.

Best regards,

Gabriel Enzo
Stereolabs Support

Have you solved the issue?
I got a similar problem and the solution proposed by “system” user did not work:
sudo apt-get autoclean
sudo mv /var/lib/dpkg/info/ /var/lib/dpkg/backup/
sudo mkdir /var/lib/dpkg/info/
sudo apt-get update
sudo apt-get -f install

My output is the following when reinstalling the driver:

Preparing to unpack …/stereolabs-zedbox-mini_1.3.1-SL-MAX9296-all-ZEDBOX-MINI-L4T36.4.0_arm64.deb …
Unpacking stereolabs-zedbox-mini (1.3.1-SL-MAX9296-all-ZEDBOX-MINI-L4T36.4.0) …
dpkg: dependency problems prevent configuration of stereolabs-zedbox-mini:
stereolabs-zedbox-mini depends on nvidia-l4t-rt-kernel (<= 5.15.148-rt-tegra-36.4.4-20250616085344) | nvidia-l4t-kernel (<= 5.15.148-tegra-36.4.4-20250616085344); however:
Package nvidia-l4t-rt-kernel is not installed.
Version of nvidia-l4t-kernel on system is 5.15.148-tegra-36.4.7-20250918154033.

dpkg: error processing package stereolabs-zedbox-mini (–install):
dependency problems - leaving unconfigured
Errors were encountered while processing:
stereolabs-zedbox-mini

The error “Package nvidia-l4t-kernel is not configured” yet is solved but the other errors are still there.

Hey alessio,

The fix proposed by stereolabs did fix my issue… Sorry i can’t be of more help