ZED Box Mini exposes only one Argus device with two ZED X One GS

Hardware: ZED Box Mini (Orin NX 8GB), 2x ZED X One GS

Each camera streams fine alone, but nothing lets both stream concurrently:

  • Single sl.CameraOne — OK
  • Two sl.CameraOne (one process, or two processes) — FAIL
  • sl.Camera.set_virtual_stereo_from_serial_numbers(...) — FAIL
  • ZED_Media_Server --cli — FAIL, crashes nvargus-daemon

Every failure is the same Argus error:
(Argus) Error AlreadyAllocated: Device 0 (of 1) is in use

Kernel side looks healthy — both sensors bind in dmesg with correct serials, both /dev/video{0,1} present, CameraOne.get_device_list() returns both serials as AVAILABLE. The collapse happens in nvargus-daemon, which only advertises one device.

Docs list Box Mini as a supported host for dual ZED X One, so I assume this should work. Has anyone gotten two ZED X One GS streaming concurrently on a Box Mini? Is there a DTBO / driver update, or a step missing?

Hi @Suveen
Welcome to the StereoLabs community.

To assist you better, we need additional information regarding your device’s condition and system setup.

Please open a terminal console (Ctrl+Alt+t) and run these commands:

  • sudo ZED_Diagnostic --dmesg
  • sudo ZED_Diagnostic -c

After executing the commands, kindly send me the content of the files dmesg.log and ZED_Diagnostic_Results.json located in the folder where the commands were run.

thank you for the quick reply.

ZED_Diagnostic_Results.json :backhand_index_pointing_down:
{
“AI Models”: {
“info”: [
“MULTI CLASS DETECTION is not optimized”,
“MULTI CLASS MEDIUM DETECTION is not optimized”,
“MULTI CLASS ACCURATE DETECTION is not optimized”,
“HUMAN BODY FAST DETECTION is not optimized”,
“HUMAN BODY MEDIUM DETECTION is not optimized”,
“HUMAN BODY ACCURATE DETECTION is not optimized”,
“HUMAN BODY 38 FAST DETECTION is not optimized”,
“HUMAN BODY 38 MEDIUM DETECTION is not optimized”,
“HUMAN BODY 38 ACCURATE DETECTION is not optimized”,
“PERSON HEAD DETECTION is not optimized”,
“PERSON HEAD ACCURATE DETECTION is not optimized”,
“REID ASSOCIATION is not optimized”,
“NEURAL LIGHT DEPTH is not optimized”,
“NEURAL DEPTH is not optimized”,
“NEURAL PLUS DEPTH is not optimized”
]
},
“CUDA Operations”: {
“cudaDeviceCount”: 1,
“cudaDriverVersion”: 12060,
“cudaDriverVersionString”: “12.6”,
“cudaGetDeviceCountResult”: 0,
“cudaRuntimeLoaded”: true,
“cudaRuntimeVersion”: 12060,
“cudaRuntimeVersionString”: “12.6”,
“cudaTestVersion”: “1.0”,
“gpuTests”: [
{
“clockRateMHz”: 765,
“computeCapability”: “8.7”,
“computeCapabilityMajor”: 8,
“computeCapabilityMinor”: 7,
“freeResult”: 0,
“freeSuccess”: true,
“gpuId”: 0,
“gpuName”: “Orin”,
“mallocResult”: 0,
“mallocSuccess”: true,
“memcpyD2HResult”: 0,
“memcpyD2HSuccess”: true,
“memcpyH2DResult”: 0,
“memcpyH2DSuccess”: true,
“memoryBusWidthBits”: 128,
“memoryClockRateMHz”: 612,
“memsetResult”: 0,
“memsetSuccess”: true,
“multiProcessorCount”: 4,
“pciBusId”: 0,
“pciDeviceId”: 0,
“pciDomainId”: 0,
“setDeviceResult”: 0,
“testElements”: 1048576,
“testPassed”: true,
“testSizeBytes”: 4194304,
“totalGlobalMemMB”: 7619,
“validationPassed”: true
}
],
“testSizeMB”: 1,
“valid”: [
“GPU 0 (Orin): CUDA operations working correctly”
]
},
“Camera Test”: {
“CorruptedFirmware”: [
],
“GMSL driver”: [
],
“GMSLList”: [
{
“Serial”: “303626954”,
“id”: 0,
“path”: “/dev/i2c-2”,
“state”: “Not Available”
},
{
“Serial”: “308588307”,
“id”: 1,
“path”: “/dev/i2c-2”,
“state”: “Available”
},
{
“Serial”: “303626954”,
“id”: 0,
“path”: “/dev/i2c-2”,
“state”: “Not Available”
},
{
“Serial”: “308588307”,
“id”: 1,
“path”: “/dev/i2c-2”,
“state”: “Available”
}
],
“InternalDevicesCount (GMSL)”: [
],
“InternalDevicesCount (USB)”: [
],
“USBList”: [
{
“USB_path”: “/1”,
“idProduct”: “0x0626”,
“idVendor”: “0x05e3”
},
{
“USB_path”: “/3”,
“idProduct”: “0x0032”,
“idVendor”: “0x8087”
},
{
“USB_path”: “/2/3”,
“idProduct”: “0x608d”,
“idVendor”: “0x17ef”
},
{
“USB_path”: “/2/2”,
“idProduct”: “0x6100”,
“idVendor”: “0x17ef”
},
{
“USB_path”: “/2”,
“idProduct”: “0x0610”,
“idVendor”: “0x05e3”
}
],
“ZEDCount”: [
],
“ZEDs”: [
]
},
“Data collection”: {
“dmesg”: {
“DMESG [DTS] LOG “: [
“dmesg: read kernel buffer failed: Operation not permitted”
],
“DMESG [MAX9x] LOG”: [
“dmesg: read kernel buffer failed: Operation not permitted”
],
“DMESG [PCA] LOG “: [
“dmesg: read kernel buffer failed: Operation not permitted”
],
“DMESG [ZEDX] LOG”: [
“dmesg: read kernel buffer failed: Operation not permitted”
],
“DTB list SLabs”: [
“board.py”,
“extlinux.py”,
“fio.py”,
“Headers”,
“Jetson”,
“Linux”,
“pycache”,
“Utils”,
“zlconfig”
],
“DTB list original”: [
“/boot/dtb/A_kernel-dtb.cursor-pre-restore-20260422-235633.bin”,
“/boot/dtb/B_kernel-dtb.cursor-pre-restore-20260422-235633.bin”,
“/boot/dtb/kernel_tegra234-p3768-0000+p3767-0001-nv.dtb”
],
“Dpkg list Stereolabs”: [
“ii stereolabs-zedbox-mini 1.4.1-SL-MAX9296-ZEDBOX-MINI-L4T36.4.0 arm64 NVIDIA Kernel DTB Modified Package by Stereolabs”
],
“Dpkg list zed”: [
],
“Driver list”: {
“/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/max9295/sl_max9295.ko”: “exists”,
“/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/max9296/max9296.ko”: “not found”,
“/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/max9296/sl_max9296.ko”: “exists”,
“/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/max96712/max96712.ko”: “not found”,
“/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/max96712/sl_max96712.ko”: “not found”,
“/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/zedone4k/sl_zedxone_uhd.ko”: “exists”,
“/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/zedx/max96712.ko”: “not found”,
“/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/zedx/sl_zedx.ko”: “exists”,
“/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/zedxpro/sl_zedxpro.ko”: “not found”
},
“EXTlinux file”: [
“TIMEOUT 30”,
“DEFAULT Stereolabs”,
“MENU TITLE L4T boot options”,
“LABEL primary”,
" MENU LABEL primary kernel”,
" LINUX /boot/Image”,
" INITRD /boot/initrd”,
" APPEND ${cbootargs} root=PARTUUID=3d6c9b45-b861-43b6-a618-c79cee89a6b9 rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 firmware_class.path=/etc/firmware fbcon=map:0 video=efifb:off console=tty0”,
“# When testing a custom kernel, it is recommended that you create a backup of”,
“# the original kernel and add a new entry to this file so that the device can”,
“# fallback to the original kernel. To do this:”,
“#”,
“# 1, Make a backup of the original kernel”,
“# sudo cp /boot/Image /boot/Image.backup”,
“#”,
“# 2, Copy your custom kernel into /boot/Image”,
“#”,
“# 3, Uncomment below menu setting lines for the original kernel”,
“#”,
“# 4, Reboot”,
“# LABEL backup”,
“# MENU LABEL backup kernel”,
“# LINUX /boot/Image.backup”,
“# INITRD /boot/initrd”,
“# APPEND ${cbootargs}”,
“LABEL Stereolabs”,
“\tMENU LABEL Stereolabs kernel”,
“\tLINUX /boot/Image”,
“\tFDT /boot/dtb/kernel_tegra234-p3768-0000+p3767-0001-nv.dtb”,
“\tINITRD /boot/initrd”,
“\tAPPEND ${cbootargs} root=PARTUUID=3d6c9b45-b861-43b6-a618-c79cee89a6b9 rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 firmware_class.path=/etc/firmware fbcon=map:0 video=efifb:off console=tty0”,
“\tOVERLAYS /boot/tegra234-p3768-camera-zedbox-mini-sl-overlay.dtbo”
],
“I2C Trace list”: {
“I2C Trace /dev/i2C-0”: [
" 0 1 2 3 4 5 6 7 8 9 a b c d e f",
"00: – – – – – – – – ",
"10: – – – – – – – – – – – – – – – – ",
"20: – – – – – – – – – – – – – – – – ",
"30: – – – – – – – – – – – – – – – – ",
"40: – – – – – – – – – – – – – – – – ",
"50: UU – – – – – – UU – – – – – – – – ",
"60: – – – – – – – – – – – – – – – – ",
“70: – – – – – – – – "
],
“I2C Trace /dev/i2C-1”: [
" 0 1 2 3 4 5 6 7 8 9 a b c d e f”,
"00: – – – – – – – – ",
"10: – – – – – – – – – – – – – – – – ",
"20: – – – – – – – – – – – – – – – – ",
"30: – – – – – – – – – – – – – – – – ",
"40: UU – – – – – – – – – – – – – – – ",
"50: – – – – – – – – – – – – – – – – ",
"60: – – – – – – – – – – – – – – – – ",
“70: – – – – – – – – "
],
“I2C Trace /dev/i2C-2”: [
" 0 1 2 3 4 5 6 7 8 9 a b c d e f”,
"00: – – – – – – – – ",
"10: UU UU – – – – – – 18 – – – – – – – ",
"20: – – – – – – – – 28 – – – – – – – ",
"30: – – – – – – – – – – – UU 3c – – – ",
"40: – – – – – – – – UU – – UU 4c – – – ",
"50: – – – – – – 56 57 – – – – – – – – ",
"60: – – – – – – UU UU 68 – – – – – – – ",
“70: – – – – – – – – "
],
“I2C Trace /dev/i2C-7”: [
" 0 1 2 3 4 5 6 7 8 9 a b c d e f”,
"00: – – – – – – – – ",
"10: – – – – – – – – – – – – – – – – ",
"20: – – – – – – – – – – – – – – – – ",
"30: – – – – – – – – – – – – – – – – “,
“40: – – – – – – – – – – – – – – – – “,
“50: – – – – – – – – – – – – – – – – “,
“60: – – – – – – – – – – – – – – – – “,
“70: – – – – – – – – "
]
},
“Jetpack”: [
“# R36 (release), REVISION: 4.7, GCID: 42132812, BOARD: generic, EABI: aarch64, DATE: Thu Sep 18 22:54:44 UTC 2025”,
“# KERNEL_VARIANT: oot”,
“TARGET_USERSPACE_LIB_DIR=nvidia”,
“TARGET_USERSPACE_LIB_DIR_PATH=usr/lib/aarch64-linux-gnu/nvidia”
],
“Linux_uname”: [
“Linux GTW-ONX2-D2V1GWBI 5.15.148-tegra #1 SMP PREEMPT Thu Sep 18 15:08:33 PDT 2025 aarch64 aarch64 aarch64 GNU/Linux”
],
“ZED SDK Version”: {
“Diag”: “5.2.3”,
“RT”: “5.2.3”
},
“ZEDX Daemon Status LS”: [
“● zed_x_daemon.service - ZED-X Daemon service”,
" Loaded: loaded (/etc/systemd/system/zed_x_daemon.service; enabled; vendor preset: enabled)”,
" Active: active (running) since Fri 2026-04-24 02:50:34 UTC; 2min 49s ago”,
" Main PID: 3646 (ZEDX_Daemon)”,
" Tasks: 5 (limit: 8808)”,
" Memory: 600.0K”,
" CPU: 178ms”,
" CGroup: /system.slice/zed_x_daemon.service”,
" └─3646 /usr/sbin/ZEDX_Daemon”,
“Apr 24 02:50:34 GTW-ONX2-D2V1GWBI systemd[1]: Started ZED-X Daemon service.”
],
“ZEDX Driver State”: [
“sl_zedxone_uhd 36864 0”,
“sl_zedx 28672 1”,
“sl_zedxhdr 20480 0”,
“sl_max9295 16384 3 sl_zedxhdr,sl_zedxone_uhd,sl_zedx”,
“sl_max9296 32768 4 sl_zedxhdr,sl_zedxone_uhd,sl_max9295,sl_zedx”,
“tegra_camera 217088 11 nvhost_isp5,nvhost_nvcsi_t194,sl_zedxhdr,sl_zedxone_uhd,nvhost_vi5,sl_zedx”,
“videodev 249856 8 v4l2_async,sl_zedxhdr,videobuf2_v4l2,tegra_camera,sl_zedxone_uhd,videobuf2_common,sl_zedx”
],
“i2C Trace”: [
“i2c-0\ti2c \t3160000.i2c \tI2C adapter”,
“i2c-1\ti2c \tc240000.i2c \tI2C adapter”,
“i2c-2\ti2c \t3180000.i2c \tI2C adapter”,
“i2c-4\ti2c \tTegra BPMP I2C adapter \tI2C adapter”,
“i2c-5\ti2c \t31b0000.i2c \tI2C adapter”,
“i2c-7\ti2c \tc250000.i2c \tI2C adapter”
]
}
},
“GMSL DRIVER”: {
“GMSL driver”: “ii stereolabs-zedbox-mini 1.4.1-SL-MAX9296-ZEDBOX-MINI-L4T36.4.0 arm64 NVIDIA Kernel DTB Modified Package by Stereolabs\n”,
“error”: [
“No camera stream
Unable to establish a proper stream. Please reboot the device. If the problem persists, contact Stereolabs support.”
]
},
“Graphics Card”: {
“deviceCount”: 1,
“deviceDriverVersion”: 12060,
“devices”: [
{
“arch”: “Ampere”,
“computeCapability”: “8.7”,
“cores”: 512,
“name”: “Orin”,
“totalMemoryBytes”: “7989571584”,
“totalMemoryMB”: 7619.44921875
}
],
“glx_info”: “OpenGL vendor string: NVIDIA Corporation\nOpenGL renderer string: NVIDIA Tegra Orin (nvgpu)/integrated\nOpenGL core profile version string: 4.6.0 NVIDIA 540.4.0\nOpenGL core profile shading language version string: 4.60 NVIDIA\nOpenGL core profile context flags: (none)\nOpenGL core profile profile mask: core profile\nOpenGL core profile extensions:\nOpenGL version string: 4.6.0 NVIDIA 540.4.0\nOpenGL shading language version string: 4.60 NVIDIA\nOpenGL context flags: (none)\nOpenGL profile mask: (none)\nOpenGL extensions:\nOpenGL ES profile version string: OpenGL ES 3.2 NVIDIA 540.4.0\nOpenGL ES profile shading language version string: OpenGL ES GLSL ES 3.20\nOpenGL ES profile extensions:\n”,
“initResult”: 0,
“valid”: [
“Graphics card: Orin”
]
},
“Processor”: {
“L4T version”: “36.4.7”,
“OS”: “Ubuntu 22.04.5 LTS “,
“avxSupported”: false,
“coreCount”: “6”,
“cpu”: " ARMv8 Processor rev 1 (v8l)”,
“datetime”: “2026-04-24 02:53:21 AM”,
“hyperThreading”: “0”,
“motherboard”: “Jetson, NVIDIA”,
“ramCapacity”: “7.989572”,
“ramUsage”: “”,
“ramUsed”: “3.777151”,
“threadCount”: “6”,
“valid”: [
“Processor: ARMv8 Processor rev 1 (v8l)”,
“Motherboard: Jetson, NVIDIA”
]
},
“ZED SDK”: {
“CUDA Toolkit version”: “V12.6.68 -->located in /usr/local/cuda-12.6/bin/nvcc”,
“CUDA loading”: false,
“GPU Driver Version”: “Driver Version : 540.4.0”,
“GPU Performance”: " Performance State : N/A”,
“ZED SDK Version (Diag)”: “5.2.3”,
“ZED SDK Version (RT)”: “5.2.3”,
“ai”: {
“checkAI”: true,
“cudaVersion”: 12060,
“tensorVersion”: 100300
},
“binFiles”: [
“libsl_ai.so”,
“libsl_zed.so”
],
“resourcesFiles”: [
“neural_depth_5.3.model”,
“neural_depth_light_5.2.model”
],
“resourcesFilesExpected”: [
“objects_performance_3.2”
],
“valid”: [
“ZED SDK version: 5.2.3”,
“CUDA version: V12.6.68”
]
}
}

dmseg.log

Created: Fri Apr 24 2026

###########################################
############ ZED SDK VERSION #############
###########################################

ZED SDK Version (Diag): 5.2.3
ZED SDK Version (RT): 5.2.3

###########################################
############ Linux Uname #############
###########################################

Linux GTW-ONX2-D2V1GWBI 5.15.148-tegra #1 SMP PREEMPT Thu Sep 18 15:08:33 PDT 2025 aarch64 aarch64 aarch64 GNU/Linux

###########################################
############ DMESG [ZEDX] LOG #############
###########################################

[    3.905690] i2c i2c-2: of_i2c: modalias failure on /bus@0/i2c@3180000/zedxone_uhd_ser@44
[    3.905698] i2c i2c-2: Failed to create I2C device for /bus@0/i2c@3180000/zedxone_uhd_ser@44
[    3.905703] i2c i2c-2: of_i2c: modalias failure on /bus@0/i2c@3180000/zedxone_uhd@1a
[    3.905706] i2c i2c-2: Failed to create I2C device for /bus@0/i2c@3180000/zedxone_uhd@1a
[  369.285823] zedx 2-0011: Driver Version : v1.4.1
[  369.286025] zedx 2-0011: tegracam sensor driver:video9_v2.0.6
[  369.612812] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 2-0011 bound
[  369.622355] zedx 2-0011: ZED-X sensor initialisation done
[  369.622364] zedx 2-0011: zedx_probe: Serial Number : 303626954
[  369.627114] zedx 2-0011: zedx_probe: success
[  369.631381] zedx 2-0010: Driver Version : v1.4.1
[  369.631577] zedx 2-0010: tegracam sensor driver:video2_v2.0.6
[  369.952925] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 2-0010 bound
[  369.954053] zedx 2-0010: ZED-X sensor initialisation done
[  369.954062] zedx 2-0010: zedx_probe: Serial Number : 308588307
[  369.954120] zedx 2-0010: zedx_probe: success

###########################################
############ DMESG [MAX9x] LOG #############
###########################################

[   16.221580] sl_max9296 2-0048: Driver Version : v1.4.1
[   16.223421] sl_max9296 2-0048: write_reg_Dser: addr = 0x10, val = 0x80
[   17.406395] sl_max9296 2-0048: No camera found on gmsl 0
[   18.466282] sl_max9296 2-0048: No camera found on gmsl 1
[   18.466295] sl_max9296 2-0048: sl_max9296_probe: No camera found on any gmsl
[   18.466349] sl_max9296: probe of 2-0048 failed with error -1
[  365.564678] sl_max9296 2-0048: Driver Version : v1.4.1
[  365.565332] sl_max9296 2-0048: write_reg_Dser: addr = 0x10, val = 0x80
[  367.056708] sl_max9296 2-0048: sl_max9296_probe: Camera connected to GMSL port 0
[  367.056723] sl_max9296 2-0048: sl_max9296_probe: zedonegs camera connected to this port
[  367.188326] sl_max9296 2-0048: sl_max9296_probe: camera pipeline operational
[  368.576640] sl_max9296 2-0048: sl_max9296_probe: Camera connected to GMSL port 1
[  368.576653] sl_max9296 2-0048: sl_max9296_probe: zedonegs camera connected to this port
[  368.724260] sl_max9296 2-0048: sl_max9296_probe: camera pipeline operational
[  368.832266] sl_max9296 2-0048: sl_max9296_probe: success
[  368.839054] sl_max9295 2-0067: Driver Version : v1.4.1
[  369.052259] sl_max9295 2-0067: probe_serializer: Serializer pipeline operational
[  369.053235] sl_max9295 2-0067: probe_serializer: Serializer for zedonegs detect success
[  369.053693] sl_max9295 2-0066: Driver Version : v1.4.1
[  369.268554] sl_max9295 2-0066: probe_serializer: Serializer pipeline operational
[  369.269757] sl_max9295 2-0066: probe_serializer: Serializer for zedonegs detect success

###########################################
############ DMESG [PCA] LOG #############
###########################################

###########################################
############ DMESG [DTS] LOG #############
###########################################

###########################################
############ DTB list original  ###########
###########################################

/boot/dtb/A_kernel-dtb.cursor-pre-restore-20260422-235633.bin
/boot/dtb/B_kernel-dtb.cursor-pre-restore-20260422-235633.bin
/boot/dtb/kernel_tegra234-p3768-0000+p3767-0001-nv.dtb

###########################################
############ DTB list SLabs     ###########
###########################################

board.py
extlinux.py
fio.py
Headers
Jetson
Linux
pycache
Utils
zlconfig

###########################################
############ EXTlinux file      ###########
###########################################

TIMEOUT 30
DEFAULT Stereolabs

MENU TITLE L4T boot options

LABEL primary
MENU LABEL primary kernel
LINUX /boot/Image
INITRD /boot/initrd
APPEND ${cbootargs} root=PARTUUID=3d6c9b45-b861-43b6-a618-c79cee89a6b9 rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 firmware_class.path=/etc/firmware fbcon=map:0 video=efifb:off console=tty0

When testing a custom kernel, it is recommended that you create a backup of

the original kernel and add a new entry to this file so that the device can

fallback to the original kernel. To do this:



1, Make a backup of the original kernel

sudo cp /boot/Image /boot/Image.backup



2, Copy your custom kernel into /boot/Image



3, Uncomment below menu setting lines for the original kernel



4, Reboot

LABEL backup

MENU LABEL backup kernel

LINUX /boot/Image.backup

INITRD /boot/initrd

APPEND ${cbootargs}

LABEL Stereolabs
MENU LABEL Stereolabs kernel
LINUX /boot/Image
FDT /boot/dtb/kernel_tegra234-p3768-0000+p3767-0001-nv.dtb
INITRD /boot/initrd
APPEND ${cbootargs} root=PARTUUID=3d6c9b45-b861-43b6-a618-c79cee89a6b9 rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 firmware_class.path=/etc/firmware fbcon=map:0 video=efifb:off console=tty0
OVERLAYS /boot/tegra234-p3768-camera-zedbox-mini-sl-overlay.dtbo

###########################################
############ Jetpack      ###########
###########################################

R36 (release), REVISION: 4.7, GCID: 42132812, BOARD: generic, EABI: aarch64, DATE: Thu Sep 18 22:54:44 UTC 2025

KERNEL_VARIANT: oot

TARGET_USERSPACE_LIB_DIR=nvidia
TARGET_USERSPACE_LIB_DIR_PATH=usr/lib/aarch64-linux-gnu/nvidia

###########################################
############ Dpkg list      ###########
###########################################

ii  stereolabs-zedbox-mini                       1.4.1-SL-MAX9296-ZEDBOX-MINI-L4T36.4.0           arm64        NVIDIA Kernel DTB Modified Package by Stereolabs

####################################
############ Driver list ###########
####################################

/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/max9296/sl_max9296.ko==> exists
/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/zedx/sl_zedx.ko==> exists
/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/zedone4k/sl_zedxone_uhd.ko==> exists
/usr/lib/modules/5.15.148-tegra/kernel/drivers/stereolabs/max9295/sl_max9295.ko==> exists

################################################
############ ZEDX Daemon Status LS #############
################################################

● zed_x_daemon.service - ZED-X Daemon service
Loaded: loaded (/etc/systemd/system/zed_x_daemon.service; enabled; vendor preset: enabled)
Active: active (running) since Fri 2026-04-24 02:50:34 UTC; 8min ago
Main PID: 3646 (ZEDX_Daemon)
Tasks: 5 (limit: 8808)
Memory: 616.0K
CPU: 310ms
CGroup: /system.slice/zed_x_daemon.service
└─3646 /usr/sbin/ZEDX_Daemon

Apr 24 02:50:34 GTW-ONX2-D2V1GWBI systemd[1]: Started ZED-X Daemon service.

################################################
############ ZEDX Driver State     #############
################################################

Note : If the following drivers has a id-state <0, reboot is required

sl_zedxone_uhd         36864  0
sl_zedx                28672  1
sl_zedxhdr             20480  0
sl_max9295             16384  3 sl_zedxhdr,sl_zedxone_uhd,sl_zedx
sl_max9296             32768  4 sl_zedxhdr,sl_zedxone_uhd,sl_max9295,sl_zedx
tegra_camera          217088  11 nvhost_isp5,nvhost_nvcsi_t194,sl_zedxhdr,sl_zedxone_uhd,nvhost_vi5,sl_zedx
videodev              249856  8 v4l2_async,sl_zedxhdr,videobuf2_v4l2,tegra_camera,sl_zedxone_uhd,videobuf2_common,sl_zedx

################################################
############ I2C Trace  [-l]       #############
################################################

i2c-0	i2c       	3160000.i2c                     	I2C adapter
i2c-1	i2c       	c240000.i2c                     	I2C adapter
i2c-2	i2c       	3180000.i2c                     	I2C adapter
i2c-4	i2c       	Tegra BPMP I2C adapter          	I2C adapter
i2c-5	i2c       	31b0000.i2c                     	I2C adapter
i2c-7	i2c       	c250000.i2c                     	I2C adapter

################################################
############ I2C Trace /dev/i2C-0 #############
################################################

 0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f

00:                         – – – – – – – –
10: – – – – – – – – – – – – – – – –
20: – – – – – – – – – – – – – – – –
30: – – – – – – – – – – – – – – – –
40: – – – – – – – – – – – – – – – –
50: UU – – – – – – UU – – – – – – – –
60: – – – – – – – – – – – – – – – –
70: – – – – – – – –

################################################
############ I2C Trace /dev/i2C-1 #############
################################################

 0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f

00:                         – – – – – – – –
10: – – – – – – – – – – – – – – – –
20: – – – – – – – – – – – – – – – –
30: – – – – – – – – – – – – – – – –
40: UU – – – – – – – – – – – – – – –
50: – – – – – – – – – – – – – – – –
60: – – – – – – – – – – – – – – – –
70: – – – – – – – –

################################################
############ I2C Trace /dev/i2C-2 #############
################################################

 0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f

00:                         – – – – – – – –
10: UU UU – – – – – – 18 – – – – – – –
20: – – – – – – – – 28 – – – – – – –
30: – – – – – – – – – – – UU 3c – – –
40: – – – – – – – – UU – – UU 4c – – –
50: – – – – – – 56 57 – – – – – – – –
60: – – – – – – UU UU 68 – – – – – – –
70: – – – – – – – –

No bus available at index 3
No bus available at index 6
################################################
############ I2C Trace /dev/i2C-7 #############
################################################

 0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f

00:                         – – – – – – – –
10: – – – – – – – – – – – – – – – –
20: – – – – – – – – – – – – – – – –
30: – – – – – – – – – – – – – – – –
40: – – – – – – – – – – – – – – – –
50: – – – – – – – – – – – – – – – –
60: – – – – – – – – – – – – – – – –
70: – – – – – – – –

No bus available at index 8
No bus available at index 9
No bus available at index 10
No bus available at index 11
No bus available at index 12
No bus available at index 13
No bus available at index 14
No bus available at index 15
No bus available at index 16
No bus available at index 30
No bus available at index 31
No bus available at index 32
No bus available at index 33
No bus available at index 34
No bus available at index 35
No bus available at index 36
No bus available at index 37
No bus available at index 38
No bus available at index 39
No bus available at index 40


The ZED X Driver detects both cameras:

[  369.622364] zedx 2-0011: zedx_probe: Serial Number : 303626954
[  369.954062] zedx 2-0010: zedx_probe: Serial Number : 308588307

What’s the output of the command ZED_Explorer -a?
Can you open both simultaneously using the ZED_Studio tool?