ZED Box cant detect camera

Hi

I trying to connect zed 2i at zed box. cant connect…
I think is matter kind of sdk. But changing sdk version latest, it also didnt work…
It it cable issue?

ZED_Diagnostic_Results.json (9.6 KB)

ZED_Diagnostic
libpng warning: iCCP: known incorrect sRGB profile
libpng warning: iCCP: known incorrect sRGB profil

“Errors occurred
A detailed report can be saved to be shared with support if needed.
”
“Specific resolutions are not available
Replug your device or connect the camera to another USB 3.0 port.”
“USB 2.0 connection detected
Please connect your camera to an USB 3.0 port.”

Hi @Hamin242
The ZED SDK detects a USB 2 connection instead of USB 3, so only VGA resolution is available.

Please check that:

  • The cable is connected to the USB 3 port
  • You are not using USB 3 hubs
  • You are not using long extension cables
  • The screws of the USB 3 connector are strongly strengthened
  • The cable is not damaged