Hi Stereolabs team,
According to the ZED Box 2 – Using GMSL documentation, setting sync_mode=1 enables internal hardware synchronization across all eight GMSL2 ports.
However, the documentation only explains how to enable internal synchronization, without specifying its supported frequencies or how to configure them.
We also found the ZED Link Quad – GPIO Triggering documentation, which describes internally generated trigger frequencies of 15, 30, 60, and 120 Hz, depending on the camera frame rate.
We would like to clarify two points specifically for ZED Box 2 internal synchronization (sync_mode=1):
-
What internal synchronization frequencies are supported? Are they limited to 15, 30, 60, and 120 Hz, or are other frequencies possible? What determines these limitations?
-
How can we configure the internal synchronization frequency? We have only found instructions for enabling
sync_mode=1. Does the frequency automatically follow the camera FPS configured through the ZED SDK, or is there a separate setting?
To clarify, this question concerns internal hardware synchronization only, without using the Sync + IO connector or an external trigger.
Thanks!