Dear Community,
I am now using ZED Hub to calibrate multiple ZED cameras connected to Jetson orin boards and cameras are installed in a common space.
Environments
- Hub’s Camera Manager is now 0.1.4 version.
- Orin’s board tegra # R35 (release), REVISION: 2.1
- Nvidia jetson packages
libnvidia-container0/stable,now 0.11.0+jetpack arm64 [installed,automatic]
nvidia-jetpack-dev/stable,now 5.1-b147 arm64 [installed,automatic]
nvidia-jetpack-runtime/stable,now 5.1-b147 arm64 [installed,automatic]
nvidia-jetpack/stable,now 5.1-b147 arm64 [installed]
Step 1) When I add a new device, I run the script appearing on the portal but it exists quickly without any error and the installation was unsuccessful (no edge_cli installed).
Step 2) Then I download the script manually but the option -qO- does not download anything. Without the option, I find
ERROR: cannot verify hub.stereolabs.com’s certificate, issued by ‘CN=R3,O=Let’s Encrypt,C=US’:
Issued certificate not yet valid.
To connect to hub.stereolabs.com insecurely, use `–no-check-certificate’.
Step 3) Obviously I use --no-check-certificate option to download. After I get the file, I run it manually with this command output
Edge Agent 0.73.2 installer for mydevicename
Analysing operating system and platform
Downloading installer for Jetpack 5.1
Installing certificate
Running Edge Agent installer
but again this is unsuccessful.
Step 4) Then, I download the Edge_Agent_ script for Jetpack 5.1 manually. and again I need to use --no-check-certificate option. Finally, when I run the script, I find this error
Verifying archive integrity… 100% MD5 checksums are OK. All good.
Uncompressing ‘ZED IoT 0.73.2 SDK by Stereolabs’ 100%
Stereolabs Edge Agent v0.73.2 Installation.
Certificate detected in /etc/sl_iot_token.conf
Failed to retrieve access token, please verify your credentials at /etc/sl_iot_token.conf.
I already check /etc/sl_iot_token.conf to be installed successfully.
I would appreciate any assistance this community may kindly offer.
Thank you very much,
Patrick