Hello,
I wanted to implement multi camera fusion with two ZED X cameras. But ZED 360 crashes when two ZED X cameras are connected. It worked fine when only one X camera was connected. The software detects both of the cameras with auto discover but when I click “Setup the room” it loads for a second and then crashes. Any ideas how to fix this?
Edit: This is the output when I run ZED 360 from the terminal. I tried restarting the computer multiple times but this is always the same output. Other Zed Tools work fine for both cameras.
Running the fusion for 2 devices.
INIT FUSION
Setup ZED 42255191
camera 42255191 failed to open
Setup ZED 48314490
camera 48314490 failed to open
Unable to subscribe to 42255191 . MEMORY ALREADY USED
Unable to subscribe to 48314490 . MEMORY ALREADY USED
START RUN FUSION
Segmentation fault (core dumped)
Thanks!