ZED 2i not detected on Jetson Nano

Hi

My Zed-2i is not detected on Jetson Nano.
I am using a usb 3.0 cable and connecting Zed to a usb 3.0 port.

Below is my dmesg output on plugging it in
hidraw2: USB HID v1.11 Device [STEREOLABS ZED-2i HID INTERFACE] on usb-70090000.xusb-2.3.2/input0
[ 1352.172004] usb 1-2.3.1: new high-speed USB device number 12 using tegra-xusb
[ 1352.196309] usb 1-2.3.1: New USB device found, idVendor=2b03, idProduct=f880
[ 1352.196373] usb 1-2.3.1: New USB device strings: Mfr=1, Product=2, SerialNumber=4
[ 1352.196419] usb 1-2.3.1: Product: ZED 2i
[ 1352.196464] usb 1-2.3.1: Manufacturer: Technologies, Inc.
[ 1352.196507] usb 1-2.3.1: SerialNumber: OV0001
[ 1352.200435] uvcvideo: Found UVC 1.10 device ZED 2i (2b03:f880)
[ 1352.201711] uvcvideo 1-2.3.1:1.0: Entity type for entity ZED 2i was not initialized!
[ 1352.209682] uvcvideo 1-2.3.1:1.0: Entity type for entity ZED 2i was not initialized!
[ 1352.217659] uvcvideo 1-2.3.1:1.0: Entity type for entity Camera 1 was not initialized!
[ 1352.226313] input: ZED 2i as /devices/70090000.xusb/usb1/1-2/1-2.3/1-2.3.1/1-2.3.1:1.0/input/input6

I ran the diagnostic and it gave a camera detection error. I am copy pasting the file as attachments are not supported from new users

"AI Models": {
    "info": [
        "REID ASSOCIATION is not optimized",
        "NEURAL PLUS DEPTH is not optimized"
    ],
    "valid": [
        "MULTI CLASS DETECTION is optimized",
        "MULTI CLASS MEDIUM DETECTION is optimized",
        "MULTI CLASS ACCURATE DETECTION is optimized",
        "HUMAN BODY FAST DETECTION is optimized",
        "HUMAN BODY MEDIUM DETECTION is optimized",
        "HUMAN BODY ACCURATE DETECTION is optimized",
        "HUMAN BODY 38 FAST DETECTION is optimized",
        "HUMAN BODY 38 MEDIUM DETECTION is optimized",
        "HUMAN BODY 38 ACCURATE DETECTION is optimized",
        "PERSON HEAD DETECTION is optimized",
        "PERSON HEAD ACCURATE DETECTION is optimized",
        "NEURAL DEPTH is optimized"
    ]
},
"Camera Test": {
    "InternalDevicesCount": 2,
    "ZEDCount": 0,
    "error": [
        "<b>Camera not detected</b> <br/> Make sure the camera is plugged in or try another USB 3.0 port."
    ]
},
"Devices": {
    "CorruptedFirmware": false,
    "GMSL driver": "",
    "GMSL driver compatiblity": "Unknown",
    "GMSLList": [
    ],
    "MCUDetected": true,
    "USBList": [
        {
            "USB_path": "/1",
            "idProduct": "0x0411",
            "idVendor": "0x0bda"
        },
        {
            "USBMode": 2,
            "USB_path": "/2/3/2",
            "bDescriptorType": 1,
            "bDeviceProtocol": 0,
            "bLength": 18,
            "bMaxPacketSize0": 64,
            "bNumConfigurations": 1,
            "bcdDevice": "3.9",
            "bcdUSB": "2.0",
            "bcdUSBClass": 0,
            "bcdUSBSubClass": 0,
            "busNumber": 1,
            "device": "ZED2i MCU",
            "iManufacturer": 1,
            "iProduct": 2,
            "iSerial": 3,
            "idProduct": "0xf881",
            "idVendor": "0x2b03"
        },
        {
            "USBMode": 2,
            "USB_path": "/2/3/1",
            "bDescriptorType": 1,
            "bDeviceProtocol": 1,
            "bLength": 18,
            "bMaxPacketSize0": 64,
            "bNumConfigurations": 1,
            "bcdDevice": "1.0",
            "bcdUSB": "2.16",
            "bcdUSBClass": 239,
            "bcdUSBSubClass": 2,
            "busNumber": 1,
            "device": "ZED2i",
            "iManufacturer": 1,
            "iProduct": 2,
            "iSerial": 4,
            "idProduct": "0xf880",
            "idVendor": "0x2b03"
        },
        {
            "USB_path": "/2/3",
            "idProduct": "0x2512",
            "idVendor": "0x0424"
        },
        {
            "USB_path": "/2/1",
            "idProduct": "0x00bd",
            "idVendor": "0x04ca"
        },
        {
            "USB_path": "/2",
            "idProduct": "0x5411",
            "idVendor": "0x0bda"
        }
    ],
    "USBMode": 2,
    "ZED Camera Module Detected": 63616,
    "ZED MCU Module Detected": 63617,
    "ZEDDetected": true,
    "warning": [
        "<b>No GMSL driver found.</b><br/> USB camera are not impacted by this."
    ]
},
"Graphics Card": {
    "deviceCount": 1,
    "deviceDriverVersion": 10020,
    "devices": [
        {
            "arch": "Maxwell",
            "computeCapability": "5.3",
            "cores": 128,
            "name": "NVIDIA Tegra X1",
            "totalMemoryBytes": "4148043776",
            "totalMemoryMB": 3955.8828125
        }
    ],
    "glx_info": "OpenGL vendor string: NVIDIA Corporation\nOpenGL renderer string: NVIDIA Tegra X1 (nvgpu)/integrated\nOpenGL core profile version string: 4.6.0 NVIDIA 32.7.5\nOpenGL core profile shading language version string: 4.60 NVIDIA\nOpenGL core profile context flags: (none)\nOpenGL core profile profile mask: core profile\nOpenGL core profile extensions:\nOpenGL version string: 4.6.0 NVIDIA 32.7.5\nOpenGL shading language version string: 4.60 NVIDIA\nOpenGL context flags: (none)\nOpenGL profile mask: (none)\nOpenGL extensions:\nOpenGL ES profile version string: OpenGL ES 3.2 NVIDIA 32.7.5\nOpenGL ES profile shading language version string: OpenGL ES GLSL ES 3.20\nOpenGL ES profile extensions:\n",
    "initResult": 0,
    "valid": [
        "<b>Graphics card: </b> NVIDIA Tegra X1"
    ]
},
"Processor": {
    "L4T version": "32.7.5",
    "OS": "Ubuntu 18.04.6 LTS ",
    "avxSupported": false,
    "coreCount": "4",
    "cpu": " ARMv8 Processor rev 1 (v8l)",
    "datetime": "2024-07-15 06:04:13",
    "hyperThreading": "0",
    "motherboard": ", ",
    "ramCapacity": "4,148044",
    "ramUsage": "",
    "ramUsed": "3,604955",
    "threadCount": "4",
    "valid": [
        "<b>Processor: </b>  ARMv8 Processor rev 1 (v8l)"
    ]
},
"ZED SDK": {
    "CUDA Toolkit version": "V10.2.300 -->located in /usr/local/cuda-10.2/bin/nvcc",
    "CUDA loading": false,
    "ZED SDK Version (Diag)": "4.1.2",
    "ZED SDK Version (RT)": "4.1.2",
    "ai": {
        "checkAI": true,
        "cudaVersion": 10020,
        "cudnnCudartVersion": 10020,
        "cudnnVersion": 8201,
        "cudnnVersionExpected": 8000,
        "tensorVersion": 8201
    },
    "binFiles": [
        "libsl_ai.so",
        "libsl_zed.so",
        "libsl_zed_static.a"
    ],
    "resourcesFiles": [
        "neural_depth_3.6.model",
        "person_reid_1.4.model"
    ],
    "resourcesFilesExpected": [
        "objects_performance_3.2"
    ],
    "valid": [
        "<b>ZED SDK version:</b> 4.1.2",
        "<b>CUDA version:</b> V10.2.300"
    ]
}

}

Hi @srinath
your ZED 2i is correctly detected and initialized by the ZED SDK.
What program are you using to open it?
Did you test ZED Explorer or ZED Depth Viewer?
What error do you get?

Hi Walter

I used ZED explorer. But it just displays waiting for camera.

Regards
Srinath

And please see the below output from diagnostic
“Camera Test”: {
“InternalDevicesCount”: 2,
“ZEDCount”: 0,
“error”: [
“Camera not detected
Make sure the camera is plugged in or try another USB 3.0 port.”
]
},

Entire diagnostic is attached

Hi Walter

I used ZED explorer. But it just displays waiting for camera.

Regards
Srinath

Hi Srinath,
I just noted that the camera is recognized as a USB2 device instead of USB3:

  • check the cable
  • check the screws of the cable, they must be strongly strengthened
  • check that you connected the camera to the USB3 port, not the USB2 port

Best regards,

Walter

Walter Lucetti
Senior Computer Engineer
SDK / Robotics / HW
Stereolabs Support

Hi Walter

All the USB ports on Jetson Nano are USB 3.0
I am using a USB 3.0 cable (I lost the original one that came with the camera)
Should i get a replacement cable from Stereolabs ?

Hi Srinath,
Thank you for reaching out to us.

I am using a USB 3.0 cable (I lost the original one that came with the camera)

It is possible that the cable is not good for high-speed data transfer.
I recommend you test a different cable and order the original cable as a replacement.

Best regards,

Walter

Walter Lucetti
Senior Computer Engineer
SDK / Robotics / HW
Stereolabs Support