ZED 2i All SDK Applications and ZED Explorer Crashing After a Few Seconds

I’m experiencing a critical issue with my ZED 2i camera where all SDK applications and ZED Explorer crash after just a few seconds of running.

System Configuration:

  • Camera: ZED 2i
  • ZED SDK: Version 5.1.2
  • CUDA: Version 12.3
  • Operating System: Windows
  • GPU: NVIDIA (CUDA-enabled)

Issue Description:
Whenever I launch any of the ZED SDK sample applications or the ZED Explorer tool, they start successfully but crash after approximately 3-5 seconds. This happens consistently across all applications.

What I’ve Tried:

  • Verified CUDA installation (version 12.3 is correctly installed)
  • Reinstalled ZED SDK 5.1.2
  • Checked camera connections and USB ports
  • Updated GPU drivers

Additional Information:
The camera is detected initially and appears to start streaming, but then the application terminates unexpectedly without any clear error messages.

Has anyone encountered similar issues with ZED 2i on Windows with SDK 5.1.2 and CUDA 12.3? Any suggestions for troubleshooting or resolving this problem would be greatly appreciated.

Thank you!

SDK 5.1.2 is very unstable or at least all apps that come with it, explorer zed360, studio etc. Explorer was not receiving any streams with cuda 12 version and sdk. Cuda 13 version at least gets the stream but still feels very “crumbly”.

What version do you suggest then? What is the most “stable” version?

Thanks!

I have also when we call cam.open(init) we get

Camera Open Internal Error: 1811

Hi @artur-leonel
Welcome to the StereoLabs community.

Please connect the camera, run the ZED Diagnostic tool, then copy and paste the content of the saved report to this thread.

Hey! Thanks for the response. Even the diagnostic tool is crashing. It reaches 10% on the camera item, then crashes and closes

Do you have an NVIDIA GPU card? What model is it? Is the driver installed and updated to the latest version?

"Hi Myzhar,

I am experiencing the exact same issue as @artur-leonel. When I call cam.open(init), I receive the Camera Open Internal Error: 1811. Additionally, my ZED Diagnostic tool crashes and closes automatically as soon as it reaches 10% during the camera check.

My system specs are:

  • GPU: NVIDIA GeForce RTX 3070

  • OS: Windows 10 64-bit

  • Driver: Latest Game Ready Driver

  • CUDA: 12.8

It seems like the SDK might be having trouble communicating with the latest CUDA 12.8 environment. Should I downgrade to a specific CUDA version (like 12.1) to resolve the diagnostic crash?"

@bugbuger97 same request for you too.

I am having the same issue. And before you ask for the output, it crashes at the camera step, meaning I can not in any way save out the diag report. It doesn’t even finish the report for me to save out.

Hello. I just received my ZED camera this week. Im getting the same issue. it reached 10% and crashes. @Myzhar can you please help with this?

@Myzhar Every single ZED app crashes after a few seconds, making the camera disfunctional. I have all software updated - Cuda 13 / Nvidia drivers etc. I am working on a very time sensitive project that needs to be completed in a few weeks - please help me understand how to address this issue.

@Alin please post your FULL system setup.

Have the same exact issue → It seems like the ZED 2i in general just is not complying at all with the newest SDK version. CUDA 13 + SDK 5.2 is bricked for me

Can you all please post the FULL setup?

  • Operating system
  • Operating system version
  • CPU model
  • GPU model
  • NVIDIA driver version
  • CUDA version
  • other relevant information (laptop, desktop, …)

Diagnostic crashes at 10% of camera check, single streaming sender sample fails to launch with error

[ZED][SLHW] Failed to create encoder. Err : NvEncoder::CreateEncoder : m_nvenc.nvEncInitializeEncoder(m_hEncoder, &m_initializeParams) returned error 8 at C:\builds\sl\ZEDKit\lib\src\sl_input\NVCompression\NvCodec\NvEncoder\NvEncoder.cpp:275

[ZED][Streaming] Failed to create encoder [0.0] at resolution 1280x720
[2026-04-14 11:49:14 UTC][ZED][ERROR] [Streaming]  Cannot enable streaming: Err Code -4
Streaming initialization error:  NO GPU COMPATIBLE

Setup description:
OS: Windows 11 Pro For Workstations 64-bit (10.0, Build 26200)
CPU: AMD Ryzen 9 7950X 16-Core Processor (32 CPUs), ~4.5GHz
GPU: NVIDIA GeForce RTX 4090
NVIDIA Driver version: 595.97
CUDA version:

nvcc: NVIDIA (R) Cuda compiler driver
Copyright (c) 2005-2025 NVIDIA Corporation
Built on Tue_Dec_16_19:27:18_Pacific_Standard_Time_2025
Cuda compilation tools, release 13.1, V13.1.115
Build cuda_13.1.r13.1/compiler.37061995_0

It is a desktop setup, Camera is a Zed2i, ZED SDK installation is from ZED_SDK_Windows_cuda13.0_tensorrt10.13_v5.2.1.exe

I have copied .dlls from the sdk directory to be in the bin subdirectory of the streaming sample.

@Jwako-TUAS Please create a new post with your issue next time.

Updating your SDK to 5.2.3 should solve the issue. This version fixes compatibility with newer NVIDIA GPU driver versions (v590+) on Desktop.