You might need to update your OpenGL packages.
You can find the latest versions on that page. You need to download PyOpenGL and PyOpenGL_accelerate packages.
To install them, download the .whl files matching your Python version and run the command : python3 -m pip install <name_of_your_whl_file>
Thanks for the reply, i currently have both installed and is version 3.1.5
I am currently running it on windows 10
Cuda 10.2
and an RTX 5000
if that information helps
What version of Python are you using ? Are you running the sample inside a virtual environment ?
If that is the case, make sure to install the packages inside your virtual environment.
Otherwise, can you try running python3 -m pip install --ignore-installed <name_of_your_whl_file> instead and see if that helps with your issue ? This will overwrite existing packages on your system.
No, I’m running it on my base environment and i have all the packages installed i have been able to use the Zed explorer and so on. but not to run the python script , object detection
im using python 3.6.8 and this is the packages that i have installed