ZED 2 Camera not recognized on Jetson AGX Xavier

Hi Stereolabs Support Team,

I am writing to report a recognition issue with my ZED 2 camera when connected to a Jetson AGX Xavier.

To provide some context, the camera and its cable are perfectly fine. When connected to my old Jetson TX2 (even with a USB extension cable), it is recognized as a USB 2.0 device, and all tools run smoothly, and I can record .svo files (VGA mode, 30fps). However, it completely fails to connect to Xavier.

System Environment:

  • Device: NVIDIA Jetson AGX Xavier Developer Kit (32GB)

  • OS: Ubuntu 20.04.6 LTS

  • ZED SDK: 4.1.4

Troubleshooting steps & symptoms on AGX Xavier: I have thoroughly tested all physical ports, including the USB port and type-C port (using a high-quality OTG adapter), as well as trying a powered USB 3.0 Hub and then reinstalling the OS. I even borrowed another Xavier (successfully forced to 5000M) to test. But the results are always the same:

  1. Standard UVC apps like ‘Cheese’ can open the low-res stream via the Type-C port, but fail completely on the eSATAp port.

  2. ZED_Explorer completely fails to open the camera, getting stuck in an infinite “Waiting for camera”.

  3. ZED_Sensor_Viewer also fails to open, meaning I cannot retrieve any IMU or environmental sensor data either.

Since the same camera works fine on the TX2 (with limited resolution). I would like to confirm if there are known compatibility issues between ZED 2 and the AGX Xavier on this OS version

Thank you for your support.

Hi @BachThu
Welcome to the Stereolabs community.

According to the information that you provided, I’m pretty sure that the cable of the camera is damaged.
We do not provide repair/replacement service for cameras out of warranty.

You can try to unmount it and replace the cable by following this unofficial guide.