When I run ZED_Depth_Viewer , it keeps flashing back

(wcf) wangchaofei@wangchaofei-Lenovo-Legion-R70002021:/usr/local/zed/tools$ ./ZED_Depth_Viewer
in bool ImageHandler::initialize(sl::Mat&) : Err [304]: OS call failed or operation not supported on this OS.
Stack trace (most recent call last):
#26 Object “[0xffffffffffffffff]”, at 0xffffffffffffffff, in
#25 Object “./ZED_Depth_Viewer”, at 0x5606d84063e4, in
#24 Object “/lib/x86_64-linux-gnu/libc.so.6”, at 0x7f72c6e29e3f, in __libc_start_main
#23 Object “/lib/x86_64-linux-gnu/libc.so.6”, at 0x7f72c6e29d8f, in
#22 Object “./ZED_Depth_Viewer”, at 0x5606d8405651, in
#21 Object “./ZED_Depth_Viewer”, at 0x5606d8430d4a, in
#20 Object “./ZED_Depth_Viewer”, at 0x5606d842bb4e, in
#19 Object “./ZED_Depth_Viewer”, at 0x5606d8441479, in
#18 Object “/lib/x86_64-linux-gnu/libQt5Core.so.5”, at 0x7f72c78b875a, in QEventLoop::exec(QFlagsQEventLoop::ProcessEventsFlag)
#17 Object “/lib/x86_64-linux-gnu/libQt5Core.so.5”, at 0x7f72c79130b7, in QEventDispatcherGlib::processEvents(QFlagsQEventLoop::ProcessEventsFlag)
#16 Object “/lib/x86_64-linux-gnu/libglib-2.0.so.0”, at 0x7f72c71193e2, in g_main_context_iteration
#15 Object “/lib/x86_64-linux-gnu/libglib-2.0.so.0”, at 0x7f72c7171257, in
#14 Object “/lib/x86_64-linux-gnu/libglib-2.0.so.0”, at 0x7f72c711bd3a, in g_main_context_dispatch
#13 Object “/lib/x86_64-linux-gnu/libQt5Core.so.5”, at 0x7f72c7912ceb, in
#12 Object “/lib/x86_64-linux-gnu/libQt5Core.so.5”, at 0x7f72c79123ea, in QTimerInfoList::activateTimers()
#11 Object “/lib/x86_64-linux-gnu/libQt5Core.so.5”, at 0x7f72c78b9e39, in QCoreApplication::notifyInternal2(QObject*, QEvent*)
#10 Object “/lib/x86_64-linux-gnu/libQt5Widgets.so.5”, at 0x7f72c856c712, in QApplicationPrivate::notify_helper(QObject*, QEvent*)
#9 Object “/lib/x86_64-linux-gnu/libQt5Core.so.5”, at 0x7f72c78e733e, in QObject::event(QEvent*)
#8 Object “/lib/x86_64-linux-gnu/libQt5Core.so.5”, at 0x7f72c78f57fd, in QTimer::timeout(QTimer::QPrivateSignal)
#7 Object “/lib/x86_64-linux-gnu/libQt5Core.so.5”, at 0x7f72c78f17c7, in
#6 Object “./ZED_Depth_Viewer”, at 0x5606d8431901, in
#5 Object “./ZED_Depth_Viewer”, at 0x5606d842cb94, in
#4 Object “./ZED_Depth_Viewer”, at 0x5606d843b103, in
#3 Object “./ZED_Depth_Viewer”, at 0x5606d8439c12, in
#2 Object “./ZED_Depth_Viewer”, at 0x5606d849b52d, in
#1 Object “./ZED_Depth_Viewer”, at 0x5606d845770d, in
#0 Object “/lib/x86_64-linux-gnu/libcuda.so.1”, at 0x7f72d1930b60, in
Segmentation fault (Signal sent by the kernel [(nil)])

When I run ZED_Depth_Viewer, it gets an error.

And then this is my environment configuration:
ubuntu22.04
cuda12.1
sdk4.07
opencv4.7

And when i use the ZED_Diagnostic,ti said ‘Unable to identify your processor,make sure that it fits the requirements.’
what should i do for this.

Hi @daiwei125
Welcome to the Stereolabs community.

Please send me the report file that the ZED Diagnostic tool generated.

{
    "AI Models": {
        "valid": [
            "MULTI CLASS DETECTION is optimized",
            "MULTI CLASS MEDIUM DETECTION is optimized",
            "MULTI CLASS ACCURATE DETECTION is optimized",
            "HUMAN BODY FAST DETECTION is optimized",
            "HUMAN BODY MEDIUM DETECTION is optimized",
            "HUMAN BODY ACCURATE DETECTION is optimized",
            "HUMAN BODY 38 FAST DETECTION is optimized",
            "HUMAN BODY 38 MEDIUM DETECTION is optimized",
            "HUMAN BODY 38 ACCURATE DETECTION is optimized",
            "PERSON HEAD DETECTION is optimized",
            "PERSON HEAD ACCURATE DETECTION is optimized",
            "REID ASSOCIATION is optimized",
            "NEURAL DEPTH is optimized"
        ]
    },
    "Camera Test": {
        "InternalDevicesCount": 1,
        "ZEDCount": 1,
        "camera": {
            "Device ID": 0,
            "Firmware": 1523,
            "Init Output": "OK",
            "Model": "ZED",
            "Serial Number": 8452341,
            "valid": [
                "<b>Camera: </b>ZED",
                "<b>Firmware: </b>1523"
            ]
        },
        "resolutions": {
            "HD1080@15": {
                "fps (input)": 15,
                "fps (output)": 15,
                "height (input)": 1080,
                "height (output)": 1080,
                "initialization": "OK",
                "status": true,
                "width (input)": 1920,
                "width (output)": 1920
            },
            "HD1080@30": {
                "fps (input)": 30,
                "fps (output)": 30,
                "height (input)": 1080,
                "height (output)": 1080,
                "initialization": "OK",
                "status": true,
                "width (input)": 1920,
                "width (output)": 1920
            },
            "HD2K@15": {
                "fps (input)": 15,
                "fps (output)": 15,
                "height (input)": 1242,
                "height (output)": 1242,
                "initialization": "OK",
                "status": true,
                "width (input)": 2208,
                "width (output)": 2208
            },
            "HD720@15": {
                "fps (input)": 15,
                "fps (output)": 15,
                "height (input)": 720,
                "height (output)": 720,
                "initialization": "OK",
                "status": true,
                "width (input)": 1280,
                "width (output)": 1280
            },
            "HD720@30": {
                "fps (input)": 30,
                "fps (output)": 30,
                "height (input)": 720,
                "height (output)": 720,
                "initialization": "OK",
                "status": true,
                "width (input)": 1280,
                "width (output)": 1280
            },
            "HD720@60": {
                "dropCount": 7,
                "fps (input)": 60,
                "fps (output)": 60,
                "height (input)": 720,
                "height (output)": 720,
                "imageCount": 493,
                "initialization": "OK",
                "status": true,
                "tearingCount": 0,
                "width (input)": 1280,
                "width (output)": 1280
            },
            "VGA@100": {
                "fps (input)": 100,
                "fps (output)": 100,
                "height (input)": 376,
                "height (output)": 376,
                "initialization": "OK",
                "status": true,
                "width (input)": 672,
                "width (output)": 672
            },
            "VGA@15": {
                "fps (input)": 15,
                "fps (output)": 15,
                "height (input)": 376,
                "height (output)": 376,
                "initialization": "OK",
                "status": true,
                "width (input)": 672,
                "width (output)": 672
            },
            "VGA@30": {
                "fps (input)": 30,
                "fps (output)": 30,
                "height (input)": 376,
                "height (output)": 376,
                "initialization": "OK",
                "status": true,
                "width (input)": 672,
                "width (output)": 672
            },
            "VGA@60": {
                "fps (input)": 60,
                "fps (output)": 60,
                "height (input)": 376,
                "height (output)": 376,
                "initialization": "OK",
                "status": true,
                "width (input)": 672,
                "width (output)": 672
            }
        },
        "sensors": {
        }
    },
    "Devices": {
        "CorruptedFirmware": false,
        "USBList": [
            {
                "USB_path": "/4",
                "idProduct": "0xe0cd",
                "idVendor": "0x0489"
            },
            {
                "USBMode": 3,
                "USB_path": "/2/2",
                "bDescriptorType": 1,
                "bDeviceProtocol": 1,
                "bLength": 18,
                "bMaxPacketSize0": 9,
                "bNumConfigurations": 1,
                "bcdDevice": "1.0",
                "bcdUSB": "3.0",
                "bcdUSBClass": 239,
                "bcdUSBSubClass": 2,
                "busNumber": 2,
                "device": "ZED",
                "iManufacturer": 1,
                "iProduct": 2,
                "iSerial": 0,
                "idProduct": "0xf582",
                "idVendor": "0x2b03"
            },
            {
                "USB_path": "/2",
                "idProduct": "0x0620",
                "idVendor": "0x05e3"
            },
            {
                "USB_path": "/4",
                "idProduct": "0xc101",
                "idVendor": "0x048d"
            },
            {
                "USB_path": "/2/1",
                "idProduct": "0xfa3b",
                "idVendor": "0x09da"
            },
            {
                "USB_path": "/2",
                "idProduct": "0x0610",
                "idVendor": "0x05e3"
            }
        ],
        "USBMode": 3,
        "ZED Camera Module Detected": 62850,
        "ZEDDetected": true,
        "valid": [
            "<b>USB Bandwidth: </b> OK"
        ]
    },
    "Graphics Card": {
        "deviceCount": 1,
        "deviceDriverVersion": 12020,
        "devices": [
            {
                "arch": "Ampere",
                "computeCapability": "8.6",
                "cores": 2048,
                "name": "NVIDIA GeForce RTX 3050 Laptop GPU",
                "totalMemoryBytes": "4082892800",
                "totalMemoryMB": 3893.75
            }
        ],
        "glx_info": "OpenGL vendor string: Mesa\nOpenGL renderer string: llvmpipe (LLVM 15.0.7, 256 bits)\nOpenGL core profile version string: 4.5 (Core Profile) Mesa 23.0.4-0ubuntu1~22.04.1\nOpenGL core profile shading language version string: 4.50\nOpenGL core profile context flags: (none)\nOpenGL core profile profile mask: core profile\nOpenGL core profile extensions:\nOpenGL version string: 4.5 (Compatibility Profile) Mesa 23.0.4-0ubuntu1~22.04.1\nOpenGL shading language version string: 4.50\nOpenGL context flags: (none)\nOpenGL profile mask: compatibility profile\nOpenGL extensions:\nOpenGL ES profile version string: OpenGL ES 3.2 Mesa 23.0.4-0ubuntu1~22.04.1\nOpenGL ES profile shading language version string: OpenGL ES GLSL ES 3.20\nOpenGL ES profile extensions:\n",
        "initResult": 0,
        "valid": [
            "<b>Graphics card: </b> NVIDIA GeForce RTX 3050 Laptop GPU"
        ]
    },
    "Processor": {
        "OS": "Ubuntu 22.04.3 LTS ",
        "avxSupported": true,
        "coreCount": "",
        "cpu": " AMD Ryzen 5 5600H with Radeon Graphics",
        "datetime": "2023-10-17 15时31分55秒",
        "hyperThreading": "0",
        "motherboard": "INVALID, LENOVO",
        "ramCapacity": "16.603492",
        "ramUsage": "",
        "ramUsed": "13.424210",
        "threadCount": "0",
        "valid": [
            "<b>Motherboard: </b> INVALID, LENOVO"
        ],
        "warning": [
            "Unable to identify your processor, make sure that it fits the requirements."
        ]
    },
    "ZED SDK": {
        "CUDA Toolkit version": "V12.1.66 -->located in /usr/local/cuda-12.1/bin/nvcc",
        "CUDA loading": false,
        "GPU Driver Version": "Driver Version                            : 535.104.05",
        "GPU Performance": "    Performance State                     : P8",
        "ZED SDK Version (Diag)": "4.0.7",
        "ZED SDK Version (RT)": "4.0.7",
        "ai": {
            "checkAI": true,
            "cudaVersion": 12010,
            "cudnnCudartVersion": 12020,
            "cudnnVersion": 8905,
            "cudnnVersionExpected": 8801,
            "tensorVersion": 8600
        },
        "binFiles": [
            "libsl_ai.so",
            "libsl_zed.so",
            "libsl_zed_static.a"
        ],
        "resourcesFiles": [
            "neural_depth_2.0.model",
            "objects_accurate_3.2.model",
            "objects_medium_3.2.model",
            "objects_performance_3.2.model",
            "person_head_accurate_2.4.model",
            "person_head_performance_2.4.model",
            "person_reid_1.4.model",
            "skeleton_body18_3.2.model",
            "skeleton_body38_3.5.model"
        ],
        "resourcesFilesExpected": [
            "objects_performance_3.2"
        ],
        "valid": [
            "<b>ZED SDK version:</b> 4.0.7",
            "<b>CUDA version:</b> V12.1.66"
        ]
    }
}

The configuration of your system and the camera are good.
You can ignore the warning, it is caused by your language.

I advise you to follow this guide to try to fix the problem:

also be sure that secure boot is not enable at the bios level.

When I run it, it doesn’t show nvidia.

$ glxinfo | grep OpenGL
OpenGL vendor string: AMD
OpenGL renderer string: RENOIR (renoir, LLVM 15.0.7, DRM 3.49, 6.2.0-34-generic)
OpenGL core profile version string: 4.6 (Core Profile) Mesa 23.0.4-0ubuntu1~22.04.1
OpenGL core profile shading language version string: 4.60
OpenGL core profile context flags: (none)
OpenGL core profile profile mask: core profile
OpenGL core profile extensions:
OpenGL version string: 4.6 (Compatibility Profile) Mesa 23.0.4-0ubuntu1~22.04.1
OpenGL shading language version string: 4.60
OpenGL context flags: (none)
OpenGL profile mask: compatibility profile
OpenGL extensions:
OpenGL ES profile version string: OpenGL ES 3.2 Mesa 23.0.4-0ubuntu1~22.04.1
OpenGL ES profile shading language version string: OpenGL ES GLSL ES 3.20
OpenGL ES profile extensions:

But this is nvidia

~$ sudo prime-select query
nvidia

But when I run ZED_Depth_Viewer, it still flashes

/usr/local/zed/tools$ ./ZED_Depth_Viewer
in bool ImageHandler::initialize(sl::Mat&) : Err [304]: OS call failed or operation not supported on this OS.
Stack trace (most recent call last):
#26   Object "[0xffffffffffffffff]", at 0xffffffffffffffff, in 
#25   Object "./ZED_Depth_Viewer", at 0x557f12cf43e4, in 
#24   Object "/lib/x86_64-linux-gnu/libc.so.6", at 0x7f4d30029e3f, in __libc_start_main
#23   Object "/lib/x86_64-linux-gnu/libc.so.6", at 0x7f4d30029d8f, in 
#22   Object "./ZED_Depth_Viewer", at 0x557f12cf3651, in 
#21   Object "./ZED_Depth_Viewer", at 0x557f12d1ed4a, in 
#20   Object "./ZED_Depth_Viewer", at 0x557f12d19b4e, in 
#19   Object "./ZED_Depth_Viewer", at 0x557f12d2f479, in 
#18   Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x7f4d30ab875a, in QEventLoop::exec(QFlags<QEventLoop::ProcessEventsFlag>)
#17   Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x7f4d30b130b7, in QEventDispatcherGlib::processEvents(QFlags<QEventLoop::ProcessEventsFlag>)
#16   Object "/lib/x86_64-linux-gnu/libglib-2.0.so.0", at 0x7f4d2f3193e2, in g_main_context_iteration
#15   Object "/lib/x86_64-linux-gnu/libglib-2.0.so.0", at 0x7f4d2f371257, in 
#14   Object "/lib/x86_64-linux-gnu/libglib-2.0.so.0", at 0x7f4d2f31bd3a, in g_main_context_dispatch
#13   Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x7f4d30b12ceb, in 
#12   Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x7f4d30b123ea, in QTimerInfoList::activateTimers()
#11   Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x7f4d30ab9e39, in QCoreApplication::notifyInternal2(QObject*, QEvent*)
#10   Object "/lib/x86_64-linux-gnu/libQt5Widgets.so.5", at 0x7f4d3176c712, in QApplicationPrivate::notify_helper(QObject*, QEvent*)
#9    Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x7f4d30ae733e, in QObject::event(QEvent*)
#8    Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x7f4d30af57fd, in QTimer::timeout(QTimer::QPrivateSignal)
#7    Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x7f4d30af17c7, in 
#6    Object "./ZED_Depth_Viewer", at 0x557f12d1f901, in 
#5    Object "./ZED_Depth_Viewer", at 0x557f12d1ab94, in 
#4    Object "./ZED_Depth_Viewer", at 0x557f12d29103, in 
#3    Object "./ZED_Depth_Viewer", at 0x557f12d27c12, in 
#2    Object "./ZED_Depth_Viewer", at 0x557f12d8952d, in 
#1    Object "./ZED_Depth_Viewer", at 0x557f12d4570d, in 
#0    Object "/lib/x86_64-linux-gnu/libcuda.so.1", at 0x7f4d3ab34e80, in 
Segmentation fault (Signal sent by the kernel [(nil)])
段错误 (核心已转储)

And here’s the diagnosis

{
    "AI Models": {
        "valid": [
            "MULTI CLASS DETECTION is optimized",
            "MULTI CLASS MEDIUM DETECTION is optimized",
            "MULTI CLASS ACCURATE DETECTION is optimized",
            "HUMAN BODY FAST DETECTION is optimized",
            "HUMAN BODY MEDIUM DETECTION is optimized",
            "HUMAN BODY ACCURATE DETECTION is optimized",
            "HUMAN BODY 38 FAST DETECTION is optimized",
            "HUMAN BODY 38 MEDIUM DETECTION is optimized",
            "HUMAN BODY 38 ACCURATE DETECTION is optimized",
            "PERSON HEAD DETECTION is optimized",
            "PERSON HEAD ACCURATE DETECTION is optimized",
            "REID ASSOCIATION is optimized",
            "NEURAL DEPTH is optimized"
        ]
    },
    "Camera Test": {
        "InternalDevicesCount": 1,
        "ZEDCount": 1,
        "camera": {
            "Device ID": 0,
            "Firmware": 1523,
            "Init Output": "OK",
            "Model": "ZED",
            "Serial Number": 8452341,
            "valid": [
                "<b>Camera: </b>ZED",
                "<b>Firmware: </b>1523"
            ]
        },
        "resolutions": {
            "HD1080@15": {
                "fps (input)": 15,
                "fps (output)": 15,
                "height (input)": 1080,
                "height (output)": 1080,
                "initialization": "OK",
                "status": true,
                "width (input)": 1920,
                "width (output)": 1920
            },
            "HD1080@30": {
                "fps (input)": 30,
                "fps (output)": 30,
                "height (input)": 1080,
                "height (output)": 1080,
                "initialization": "OK",
                "status": true,
                "width (input)": 1920,
                "width (output)": 1920
            },
            "HD2K@15": {
                "fps (input)": 15,
                "fps (output)": 15,
                "height (input)": 1242,
                "height (output)": 1242,
                "initialization": "OK",
                "status": true,
                "width (input)": 2208,
                "width (output)": 2208
            },
            "HD720@15": {
                "fps (input)": 15,
                "fps (output)": 15,
                "height (input)": 720,
                "height (output)": 720,
                "initialization": "OK",
                "status": true,
                "width (input)": 1280,
                "width (output)": 1280
            },
            "HD720@30": {
                "fps (input)": 30,
                "fps (output)": 30,
                "height (input)": 720,
                "height (output)": 720,
                "initialization": "OK",
                "status": true,
                "width (input)": 1280,
                "width (output)": 1280
            },
            "HD720@60": {
                "dropCount": -1,
                "fps (input)": 60,
                "fps (output)": 60,
                "height (input)": 720,
                "height (output)": 720,
                "imageCount": 502,
                "initialization": "OK",
                "status": true,
                "tearingCount": 0,
                "width (input)": 1280,
                "width (output)": 1280
            },
            "VGA@100": {
                "fps (input)": 100,
                "fps (output)": 100,
                "height (input)": 376,
                "height (output)": 376,
                "initialization": "OK",
                "status": true,
                "width (input)": 672,
                "width (output)": 672
            },
            "VGA@15": {
                "fps (input)": 15,
                "fps (output)": 15,
                "height (input)": 376,
                "height (output)": 376,
                "initialization": "OK",
                "status": true,
                "width (input)": 672,
                "width (output)": 672
            },
            "VGA@30": {
                "fps (input)": 30,
                "fps (output)": 30,
                "height (input)": 376,
                "height (output)": 376,
                "initialization": "OK",
                "status": true,
                "width (input)": 672,
                "width (output)": 672
            },
            "VGA@60": {
                "fps (input)": 60,
                "fps (output)": 60,
                "height (input)": 376,
                "height (output)": 376,
                "initialization": "OK",
                "status": true,
                "width (input)": 672,
                "width (output)": 672
            }
        },
        "sensors": {
        }
    },
    "Devices": {
        "CorruptedFirmware": false,
        "USBList": [
            {
                "USB_path": "/4",
                "idProduct": "0xe0cd",
                "idVendor": "0x0489"
            },
            {
                "USBMode": 3,
                "USB_path": "/2/2",
                "bDescriptorType": 1,
                "bDeviceProtocol": 1,
                "bLength": 18,
                "bMaxPacketSize0": 9,
                "bNumConfigurations": 1,
                "bcdDevice": "1.0",
                "bcdUSB": "3.0",
                "bcdUSBClass": 239,
                "bcdUSBSubClass": 2,
                "busNumber": 2,
                "device": "ZED",
                "iManufacturer": 1,
                "iProduct": 2,
                "iSerial": 0,
                "idProduct": "0xf582",
                "idVendor": "0x2b03"
            },
            {
                "USB_path": "/2",
                "idProduct": "0x0620",
                "idVendor": "0x05e3"
            },
            {
                "USB_path": "/4",
                "idProduct": "0xc101",
                "idVendor": "0x048d"
            },
            {
                "USB_path": "/2/3",
                "idProduct": "0xfa3b",
                "idVendor": "0x09da"
            },
            {
                "USB_path": "/2",
                "idProduct": "0x0610",
                "idVendor": "0x05e3"
            }
        ],
        "USBMode": 3,
        "ZED Camera Module Detected": 62850,
        "ZEDDetected": true,
        "valid": [
            "<b>USB Bandwidth: </b> OK"
        ]
    },
    "Graphics Card": {
        "deviceCount": 1,
        "deviceDriverVersion": 12030,
        "devices": [
            {
                "arch": "Ampere",
                "computeCapability": "8.6",
                "cores": 2048,
                "name": "NVIDIA GeForce RTX 3050 Laptop GPU",
                "totalMemoryBytes": "4091478016",
                "totalMemoryMB": 3901.9375
            }
        ],
        "glx_info": "OpenGL vendor string: AMD\nOpenGL renderer string: RENOIR (renoir, LLVM 15.0.7, DRM 3.49, 6.2.0-34-generic)\nOpenGL core profile version string: 4.6 (Core Profile) Mesa 23.0.4-0ubuntu1~22.04.1\nOpenGL core profile shading language version string: 4.60\nOpenGL core profile context flags: (none)\nOpenGL core profile profile mask: core profile\nOpenGL core profile extensions:\nOpenGL version string: 4.6 (Compatibility Profile) Mesa 23.0.4-0ubuntu1~22.04.1\nOpenGL shading language version string: 4.60\nOpenGL context flags: (none)\nOpenGL profile mask: compatibility profile\nOpenGL extensions:\nOpenGL ES profile version string: OpenGL ES 3.2 Mesa 23.0.4-0ubuntu1~22.04.1\nOpenGL ES profile shading language version string: OpenGL ES GLSL ES 3.20\nOpenGL ES profile extensions:\n",
        "initResult": 0,
        "valid": [
            "<b>Graphics card: </b> NVIDIA GeForce RTX 3050 Laptop GPU"
        ]
    },
    "Processor": {
        "OS": "Ubuntu 22.04.3 LTS ",
        "avxSupported": true,
        "coreCount": "",
        "cpu": " AMD Ryzen 5 5600H with Radeon Graphics",
        "datetime": "2023-10-18 20时42分53秒",
        "hyperThreading": "0",
        "motherboard": "INVALID, LENOVO",
        "ramCapacity": "14.489514",
        "ramUsage": "",
        "ramUsed": "6.061777",
        "threadCount": "0",
        "valid": [
            "<b>Motherboard: </b> INVALID, LENOVO"
        ],
        "warning": [
            "Unable to identify your processor, make sure that it fits the requirements."
        ]
    },
    "ZED SDK": {
        "CUDA Toolkit version": "V12.1.66 -->located in /usr/local/cuda-12.1/bin/nvcc",
        "CUDA loading": false,
        "GPU Driver Version": "Driver Version                            : 545.23.06",
        "GPU Performance": "    Performance State                     : P8",
        "ZED SDK Version (Diag)": "4.0.7",
        "ZED SDK Version (RT)": "4.0.7",
        "ai": {
            "checkAI": true,
            "cudaVersion": 12010,
            "cudnnCudartVersion": 12020,
            "cudnnVersion": 8905,
            "cudnnVersionExpected": 8801,
            "tensorVersion": 8600
        },
        "binFiles": [
            "libsl_ai.so",
            "libsl_zed.so",
            "libsl_zed_static.a"
        ],
        "resourcesFiles": [
            "neural_depth_2.0.model",
            "objects_accurate_3.2.model",
            "objects_medium_3.2.model",
            "objects_performance_3.2.model",
            "person_head_accurate_2.4.model",
            "person_head_performance_2.4.model",
            "person_reid_1.4.model",
            "skeleton_body18_3.2.model",
            "skeleton_body38_3.5.model"
        ],
        "resourcesFilesExpected": [
            "objects_performance_3.2"
        ],
        "valid": [
            "<b>ZED SDK version:</b> 4.0.7",
            "<b>CUDA version:</b> V12.1.66"
        ]
    }
}

Should I re-download the sdk or do some other work

Did you reboot after setting nvidia?
Have you checked the BIOS for Secure Boot? You should disable it.

yes,but when I finished using the method you mentioned, it now shows mesa again.

:~$ glxinfo | grep OpenGL
OpenGL vendor string: Mesa
OpenGL renderer string: llvmpipe (LLVM 15.0.7, 256 bits)
OpenGL core profile version string: 4.5 (Core Profile) Mesa 23.0.4-0ubuntu1~22.04.1
OpenGL core profile shading language version string: 4.50
OpenGL core profile context flags: (none)
OpenGL core profile profile mask: core profile
OpenGL core profile extensions:
OpenGL version string: 4.5 (Compatibility Profile) Mesa 23.0.4-0ubuntu1~22.04.1
OpenGL shading language version string: 4.50
OpenGL context flags: (none)
OpenGL profile mask: compatibility profile
OpenGL extensions:
OpenGL ES profile version string: OpenGL ES 3.2 Mesa 23.0.4-0ubuntu1~22.04.1
OpenGL ES profile shading language version string: OpenGL ES GLSL ES 3.20
OpenGL ES profile extensions:

Hi @daiwei125
you must use the support page that I linked above and the suggestion that I gave to find the correct configuration for you PC.
Unfortunately, not all laptops behave in the same way and it’s not easy to provide a solution that rules all the possible problems.
In your case, I’m sure that the NVIDIA GPU is not enabled by default, so you must find the correct way to do that for your PC.
I recommend contacting the Lenovo support in case you find nothing useful on the internet

@daiwei125 I have the same problem with you, but my ubuntu version is 20.04, have you solved the problem? I need some help.

Hello, you can try to go to this website to try to solve your problem. If that doesn’t work, you can always try to reinstall the nvidia driver. I did not succeed at first, and then I reinstall the nvidia driver, and then can use