I wonder if 2K give a better recognition or further view?
For my another application, I may need to go further than 20m in my ZEDi, is it possible? ZEDx also has 20m max range it seems…
From my testing so far, 2K and 1080HD give similar result of object detection and skeleton.
If they are the same, when I do the recording later, I will use 1080HD as it use so much memory space…
Hi @AK51
2K and 1080p are two different image frame resolutions corresponding to different depth maps. The depth map generated using the 2K resolution is more detailed and dense.
The performance while detecting objects and skeletons is similar, with the 2K resolution the relative 3D information is more precise.
From the point of view of the range, the performance is similar.
What is the furthest possible distance away from the camera? If the accuracy decrease, I can still accept.
My another application may need up to 40m range… Guess ZED is not suitable?