Hey there,
i´m looking for the right hardware to make a blob detection/body tracking in an area of 10 to 10 meter. the cameras could be mounted in a heigth of around 3-5 meter. what is important to me is to keep track of the Person´s IDs, for instance when people start to move around, big people cover small people as kids etc. …
i guess the FUSION API with ZED360 is the right start. lets say i would go for the centralized workflow.
- i would go for two ZED 2 cameras.
- mount them at around 3m height, ( does the height affect the detection quality of the trained networks? because i guess the networks are trained from a certain angle right? would use COCO18 skeleton representation)
- adjust each camera to angle downward slightly, aiming towards the center of the area or slightly overlapping in the middle.
- as computer i could use a PC ( i7 6700 8-Thread CPU, 4.0 GHz | 32GB DDR4| Geforce RTX 3060 12GB DDR6 | 1TB SSD | Windows11 ) or an ZED Box NX Orin 16GB
i do not necessarily need all the body tracking data. mainly position with steady ID is important.
am I on the right track with this test setup?
could i maybe also have a camera setup of multiple monocular cameras as ZED X One, consequently have more perspectives?
Best