Hi, Team @Myzhar
I am working on Creating GeoReferenced Point Cloud using ZED SDK, So far I have tried almost all avilable possibilities and it seems like the SDK is either lacking the capabilities or I am doing something wrong.
I am new to the SDK and will appreciate the help. I have tried using the code from the fusion, spatial mapping & positional tracking modules merged in a single script to process the svo file and get the point cloud which is georeferenced but while doing this I have stucked where I get the position from the getGeoPose function from fusion object and then used camera2Geo as suggested in various topics. But there is no luck, it would be great if you review my code and let me know if there is something I am doing wrong or just tell that this is not possible.
Here is the attached code for your reference ![]()
#include <sl/Camera.hpp>
#include <sl/Fusion.hpp>
#include <cmath>
#include <nlohmann/json.hpp>
using json = nlohmann::json;
using namespace std;
using namespace sl;
inline bool is_microseconds(uint64_t timestamp) {
// Check if the timestamp is in microseconds
return (1'000'000'000'000'000 <= timestamp && timestamp < 10'000'000'000'000'000ULL);
}
inline bool is_nanoseconds(uint64_t timestamp) {
// Check if the timestamp is in microseconds
return (1'000'000'000'000'000'000 <= timestamp && timestamp < 10'000'000'000'000'000'000ULL);
}
int main() {
// Create a ZED camera object
Camera zed;
sl::FusedPointCloud finalObj;
// Set configuration parameters
InitParameters init_parameters;
init_parameters.coordinate_system = COORDINATE_SYSTEM::IMAGE; // Use a right-handed Y-up coordinate system
init_parameters.coordinate_units = UNIT::METER; // Set units in meters
init_parameters.depth_mode = DEPTH_MODE::ULTRA; // Set units in meters
init_parameters.input.setFromSVOFile("zed-sdk/global localization/recording/python/output/ZED_SN35169074_25-03-2025_17-08-22.svo2");
init_parameters.sdk_verbose = 1;
// Open the camera
auto returned_state = zed.open(init_parameters);
if (returned_state != ERROR_CODE::SUCCESS) {
cout << "Error " << returned_state << ", exit program.\n";
return EXIT_FAILURE;
}
// Enable positional tracking with default parameters. Positional tracking needs to be enabled before using spatial mapping
sl::PositionalTrackingParameters tracking_parameters;
tracking_parameters.mode = sl::POSITIONAL_TRACKING_MODE::GEN_2;
returned_state = zed.enablePositionalTracking(tracking_parameters);
if (returned_state != ERROR_CODE::SUCCESS) {
cout << "Error " << returned_state << ", exit program.\n";
return EXIT_FAILURE;
}
auto display_resolution = sl::Resolution(1280, 720);
sl::Fusion fusion;
sl::InitFusionParameters init_fusion_param;
init_fusion_param.coordinate_units = UNIT::METER;
init_fusion_param.coordinate_system = COORDINATE_SYSTEM::IMAGE;
init_fusion_param.output_performance_metrics = true;
init_fusion_param.verbose = true;
init_fusion_param.timeout_period_number = 66;
sl::FUSION_ERROR_CODE fusion_init_code = fusion.init(init_fusion_param);
if (fusion_init_code != sl::FUSION_ERROR_CODE::SUCCESS) {
std::cerr << "[Fusion][ERROR] Failed to initialize fusion, error: " << fusion_init_code << std::endl;
return EXIT_FAILURE;
}
// Enable odometer publishing:
sl::CommunicationParameters configuration;
zed.startPublishing(configuration);
/// Run a first grab for starting sending data:
while (zed.grab() != sl::ERROR_CODE::SUCCESS) {
}
sl::CameraIdentifier uuid(zed.getCameraInformation().serial_number);
fusion.subscribe(uuid, configuration, sl::Transform());
// Enable positional tracking for Fusion object
sl::PositionalTrackingFusionParameters tracking_fusion_param;
tracking_fusion_param.enable_GNSS_fusion = true;
sl::GNSSCalibrationParameters gnss_calibration_parameters;
gnss_calibration_parameters.target_yaw_uncertainty = 1e-2;
gnss_calibration_parameters.enable_translation_uncertainty_target = false;
gnss_calibration_parameters.target_translation_uncertainty = 15e-2;
gnss_calibration_parameters.enable_reinitialization = false;
gnss_calibration_parameters.gnss_vio_reinit_threshold = 5;
gnss_calibration_parameters.enable_rolling_calibration = true;
gnss_calibration_parameters.gnss_antenna_position = sl::float3 (1.0, 0.0, 0.25);
tracking_fusion_param.gnss_calibration_parameters = gnss_calibration_parameters;
if(sl::FUSION_ERROR_CODE tracking_error_code = fusion.enablePositionalTracking(tracking_fusion_param); tracking_error_code != sl::FUSION_ERROR_CODE::SUCCESS){
std::cout << "[Fusion][ERROR] Could not start tracking, error: " << tracking_error_code << std::endl;
return EXIT_FAILURE;
}
SpatialMappingParameters spatial_mapping_parameters;
spatial_mapping_parameters.set(SpatialMappingParameters::MAPPING_RANGE::AUTO);
spatial_mapping_parameters.set(SpatialMappingParameters::MAPPING_RESOLUTION::HIGH);
spatial_mapping_parameters.max_memory_usage = 2560;
spatial_mapping_parameters.save_texture = false;
spatial_mapping_parameters.use_chunk_only = true;
spatial_mapping_parameters.reverse_vertex_order = false;
spatial_mapping_parameters.map_type = SpatialMappingParameters::SPATIAL_MAP_TYPE::FUSED_POINT_CLOUD;
spatial_mapping_parameters.stability_counter = 2;
FusedPointCloud zed_mesh;
FusedPointCloud fusion_mesh;
RuntimeParameters runtime_parameters;
// Use low depth confidence to avoid introducing noise in the constructed model
runtime_parameters.measure3D_reference_frame = REFERENCE_FRAME::WORLD;
runtime_parameters.enable_depth = true;
runtime_parameters.confidence_threshold = 50;
Mat left_image(display_resolution, MAT_TYPE::U8_C4, sl::MEM::GPU);
Mat point_cloud(display_resolution, MAT_TYPE::F32_C4, sl::MEM::GPU);
POSITIONAL_TRACKING_STATE tracking_state = POSITIONAL_TRACKING_STATE::OFF;
Pose pose;
sl::Timestamp last_timestamp = 0;
bool is_running = true;
std::string gnss_key;
try {
gnss_key = zed.getSVODataKeys()[0];
}catch (const std::runtime_error &e) {
std::cerr << "Error while Locating GNSS Key in SVO File: " << e.what() << std::endl;
}
bool mapping_enable = false;
bool spatial_mapping_fusion_status = false;
while(is_running) {
if (zed.grab(runtime_parameters) == ERROR_CODE::SUCCESS) {
// Retrieve the left image
zed.retrieveImage(left_image, VIEW::LEFT, MEM::GPU, display_resolution);
zed.retrieveMeasure(point_cloud, MEASURE::XYZBGRA, MEM::GPU, display_resolution);
// Retrieve the camera pose data
tracking_state = zed.getPosition(pose, REFERENCE_FRAME::WORLD);
if (tracking_state != POSITIONAL_TRACKING_STATE::OK) {
std::cout << "Waiting for Positional Tracking to Begin" << std::endl;
}
auto current_ts = zed.getTimestamp(TIME_REFERENCE::IMAGE);
// auto status use status in real problem
if (gnss_key.empty()) {
std::cout << "GNSS Key is empty. Killing Program" << std::endl;
break;
}
std::map<sl::Timestamp, sl::SVOData> data_map;
zed.retrieveSVOData(gnss_key,
data_map,
last_timestamp,
current_ts);
sl::GNSSData input_gnss;
for (auto &[fst, snd] : data_map) {
SVOData& data = snd; // Accessing the value (SVOData)
std::string s;
bool data_string = data.getContent(s);
auto tmp_array = json::array();
try {
auto gnss_data_point = json::parse(s);
auto gnss_data_point_formatted = json::object();
if (!gnss_data_point["coordinates"].is_null()) {
gnss_data_point_formatted["coordinates"] = {
{"latitude", gnss_data_point["coordinates"]["latitude"].get<float>()},
{"longitude", gnss_data_point["coordinates"]["longitude"].get<float>()},
{"altitude", gnss_data_point["coordinates"]["altitude"].get<float>()},
};
gnss_data_point_formatted["ts"] = gnss_data_point["ts"];
float latitude_std = gnss_data_point["latitude_std"];
float longitude_std = gnss_data_point["longitude_std"];
float altitude_std = gnss_data_point["altitude_std"];
gnss_data_point_formatted["latitude_std"] = sqrt(latitude_std);
gnss_data_point_formatted["longitude_std"] = sqrt(longitude_std);
gnss_data_point_formatted["altitude_std"] = sqrt(altitude_std);
gnss_data_point_formatted["position_covariance"] = json::array({
longitude_std, 0, 0, 0, latitude_std, 0, 0, 0, altitude_std
});
gnss_data_point_formatted["original_gnss_data"] = gnss_data_point;
} else if (!gnss_data_point["coordinates"].is_null() && !gnss_data_point["latitude_std"].is_null() && !gnss_data_point["longitude_std"].is_null()) {
// no conversion
gnss_data_point_formatted = gnss_data_point;
}
tmp_array.push_back(gnss_data_point_formatted);
} catch (const std::runtime_error &e) {
std::cerr << "Error while reading GNSS data: " << e.what() << std::endl;
}
input_gnss.gnss_mode = GNSS_MODE::FIX_2D;
input_gnss.gnss_status = GNSS_STATUS::SINGLE;
input_gnss.longitude_std = tmp_array[0]["longitude_std"];
input_gnss.latitude_std = tmp_array[0]["latitude_std"];
input_gnss.altitude_std = tmp_array[0]["altitude_std"];
input_gnss.position_covariance = tmp_array[0]["position_covariance"];
if (is_microseconds(tmp_array[0]["ts"].get<uint64_t>())){
input_gnss.ts.setMicroseconds(tmp_array[0]["ts"].get<uint64_t>());
}
else if (is_nanoseconds(tmp_array[0]["ts"].get<uint64_t>())){
input_gnss.ts.setNanoseconds(tmp_array[0]["ts"].get<uint64_t>());
}
input_gnss.setCoordinates(tmp_array[0]["coordinates"]["latitude"],
tmp_array[0]["coordinates"]["longitude"],
tmp_array[0]["coordinates"]["altitude"],
false
);
sl::FUSION_ERROR_CODE ingest_status = fusion.ingestGNSSData(input_gnss);
if (ingest_status != sl::FUSION_ERROR_CODE::SUCCESS and ingest_status != sl::FUSION_ERROR_CODE::NO_NEW_DATA_AVAILABLE) {
std::cout << "Ingest error occurred when ingesting GNSSData: " << ingest_status << std::endl;
}else {
std::cout << "Ingest OK" << std::endl;
break;
}
}
last_timestamp = current_ts;
if (fusion.process() == sl::FUSION_ERROR_CODE::SUCCESS){
if (!mapping_enable) {
sl::ERROR_CODE mapping_status = zed.enableSpatialMapping(spatial_mapping_parameters);
if (mapping_status == sl::ERROR_CODE::SUCCESS) {
mapping_enable = true;
}
}
if (!spatial_mapping_fusion_status) {
sl::SpatialMappingFusionParameters spatial_mapping_fusion_parameters;
spatial_mapping_fusion_parameters.set(SpatialMappingParameters::MAPPING_RANGE::AUTO);
spatial_mapping_fusion_parameters.set(SpatialMappingParameters::MAPPING_RESOLUTION::HIGH);
spatial_mapping_fusion_parameters.max_memory_usage = 2000;
spatial_mapping_fusion_parameters.use_chunk_only = true;
spatial_mapping_fusion_parameters.map_type = SpatialMappingParameters::SPATIAL_MAP_TYPE::FUSED_POINT_CLOUD;
spatial_mapping_fusion_parameters.stability_counter = 2;
sl::FUSION_ERROR_CODE fusion_mapping_status = fusion.enableSpatialMapping(spatial_mapping_fusion_parameters);
if (fusion_mapping_status == sl::FUSION_ERROR_CODE::SUCCESS) {
spatial_mapping_fusion_status = true;
}
}
sl::Pose fused_pose;
sl::POSITIONAL_TRACKING_STATE state = fusion.getPosition(fused_pose);
float yaw_std;
sl::float3 position_std;
fusion.getCurrentGNSSCalibrationSTD(yaw_std, position_std);
if (yaw_std != -1.f) {
std::cout << ": calibration uncertainty yaw_std " << yaw_std << " rad position_std " << position_std
[0] << " m, " << position_std[1] << " m, " << position_std[2] << " m\t\t\t\r";
}
if (state == sl::POSITIONAL_TRACKING_STATE::OK) {
sl::GeoPose fused_geo_pose;
sl::GNSS_FUSION_STATUS gnss_fusion_status = fusion.getGeoPose(fused_geo_pose);
sl::GNSS_FUSION_STATUS geo_fusion_status = fusion.Camera2Geo(fused_pose, fused_geo_pose);
// zed.requestSpatialMapAsync();
fusion.requestSpatialMapAsync();
if (fusion.getSpatialMapRequestStatusAsync() == sl::FUSION_ERROR_CODE::SUCCESS) {
fusion.retrieveSpatialMapAsync(fusion_mesh);
fusion_mesh.save("test");
}
// zed.retrieveSpatialMapAsync(zed_mesh);
// fusion.getGeoPose();
// finalObj.updateFromChunkList(fused_geo_pose.pose_data)
}
}
}
else if (zed.grab() == ERROR_CODE::END_OF_SVOFILE_REACHED) {
is_running = false;
std::cout << "End of file";
break;
}
else {
is_running = false;
}
}
// zed.extractWholeSpatialMap(zed_mesh);
// zed_mesh.save("test-out.ply");
fusion_mesh.save("fused-out.ply");
fusion.disablePositionalTracking();
zed.disablePositionalTracking();
zed.disableSpatialMapping();
fusion.close();
zed.close();
}
Please help me resolving the issue.
Thanks
Aman Ranjan