I have a setup with a ZED Box Mini and 2 ZEDX cameras connected over GSML2.
I have connected an external trigger to the sync-in port which i for test control with a testapplication.
However the cameras are not leaving free-running mode? My SDK version is v5.0.0 and Ubuntu 22.04.5’
Help is very appreciated!
However the documentation makes me a bit confused. Is it even possible to operate in the way I want? I simply want to capture a frame when my trigger goes high … like if I had an external button. The document makes me worry I can only sync a number of devices to a common given fps?
hi .. i have a doubt….so the camera when in master mode generates signals (30 signals) per sec if its at 30 fps??also i have connected a strobing controller to the sync out pin so practically when the camera runs in free mode while being configured as master with sync_mode=0 then it should cnstantly send 30 signals every sec ryt?? also when i turn off the explorer will the signals be stopped or turn off the daemon ..??