USB custom extension cable

Hi,

I wornking with a ZED2i and I need to integrate the camera with a cable approximately 0.5 meters long. I have seen the lengths that are offered in the Stereolab Store and it does not offer similar dimensions (0.3m it short and 1.5m is too long for my application).

Is there any solution you can offer me to solve it without losing quality in data transmission performance??

Best regards.

Hi @cmcobosetrair
In the store, you can find the only available official solutions.

In any case, you can use a standard USB3 cable, which must support high communication speed.
Please note that not all the cables work as expected.