Unreal Plugin for 5.0.0 crashing on play

When hitting play in any level in Unreal Engine 5.4 ZEDSamples project (didn’t modify anything, downloaded from here), the editor crashes with this error:

Unhandled Exception: 0xc06d007e

KERNELBASE
UnrealEditor_Stereolabs!__delayLoadHelper2() [D:\a_work\1\s\src\vctools\delayimp\delayhlp.cpp:312]
UnrealEditor_Stereolabs!_tailMerge_sl_zed_c_dll()
UnrealEditor_Stereolabs!USlCameraProxy::CheckAIModelOptimization() [E:\UnrealProjects\Plugins\zed-UE5-5.0.0\Plugins\Stereolabs\Source\Stereolabs\Private\Core\StereolabsCameraProxy.cpp:1252]
UnrealEditor_ZED!AZEDPlayerController::Internal_OpenZedCamera() [E:\UnrealProjects\Plugins\zed-UE5-5.0.0\Plugins\Stereolabs\Source\ZED\Private\Core\ZEDPlayerController.cpp:416]
UnrealEditor_ZED!TBaseUObjectMethodDelegateInstance<0,AZEDPlayerController,void __cdecl(void),FNotThreadSafeNotCheckedDelegateUserPolicy>::Execute() [E:\Program Files\UE_5.4\Engine\Source\Runtime\Core\Public\Delegates\DelegateInstancesImpl.h:650]
UnrealEditor_Engine
UnrealEditor_Engine
UnrealEditor_Engine
UnrealEditor_UnrealEd
UnrealEditor_UnrealEd
UnrealEditor
UnrealEditor
UnrealEditor
UnrealEditor
UnrealEditor
UnrealEditor
kernel32
ntdll

All models are optimized, CUDA 12.8 is installed.

I tried with ZED SDK 5.0.1 and 5.0.2, in Windows 10 and 11 as well but the same thing happens.

What I noticed that it says “This version is compatible with version 5.0.0 only of the ZED SDK.” However, I can’t seem to find 5.0.0 release version of the ZED SDK. Could this be the problem?

Any help is appreciated!

Hi,

I have just pushed a fix to the main branch of the repository. Could you try it ? It should be good now.

Thanks.

Stereolabs Support

Hi,

Thank you so much for the quick response. I tried the updated version and it works perfectly now! I tested it in the Unreal Editor and in a packaged version as well, and both are working correctly.

Thank you! :slight_smile: