I’m trying to package an Unreal Engine project utilizing Zed body tracking, and it always results in an PackagingResults: Error: Unknown Error. The project is based on the sample project, which does not build successfully either. What gives?
Here are the logs:
UATHelper: Packaging (Windows): Building ZEDSamples...
UATHelper: Packaging (Windows): Using Visual Studio 2022 14.37.32825 toolchain (C:\Program Files\Microsoft Visual Studio\2022\Community\VC\Tools\MSVC\14.37.32822) and Windows 10.0.22621.0 SDK (C:\Program Files (x86)\Windows Kits\10).
UATHelper: Packaging (Windows): [Adaptive Build] Excluded from Stereolabs unity file: Stereolabs.cpp, StereolabsBaseTypes.cpp, StereolabsCameraProxy.cpp, StereolabsCoreGlobals.cpp, StereolabsMesh.cpp, StereolabsTexture.cpp, StereolabsTextureBatch.cpp, StereolabsAIDetectionRunnable.cpp, StereolabsGrabRunnable.cpp, StereolabsMeasureRunnable.cpp, StereolabsRunnable.cpp, StereolabsFunctionLibrary.cpp, StereolabsViewportHelper.cpp
UATHelper: Packaging (Windows): [Adaptive Build] Excluded from ZED unity file: ZED.cpp, AnimNode_ZEDPose.cpp, ZEDBaseTypes.cpp, ZEDCamera.cpp, ZEDCoreGlobals.cpp, ZEDInitializer.cpp, ZEDPawn.cpp, ZEDPlayerController.cpp, ZEDPointCloudRenderer.cpp, ZEDGameInstance.cpp, ZEDGameViewportClient.cpp, ZEDLocalPlayer.cpp, ZEDWidget.cpp, ZEDWidgetComponent.cpp, ZEDFunctionLibrary.cpp
UATHelper: Packaging (Windows): [Adaptive Build] Excluded from SpatialMapping unity file: SpatialMapping.cpp, SpatialMappingCubemapManager.cpp, SpatialMappingManager.cpp, SpatialMappingCubemapRunnable.cpp, SpatialMappingRunnable.cpp
UATHelper: Packaging (Windows): [Adaptive Build] Excluded from EnvironmentalLighting unity file: EnvironmentalLighting.cpp, EnvironmentalLightingManager.cpp
UATHelper: Packaging (Windows): Determining max actions to execute in parallel (12 physical cores, 24 logical cores)
UATHelper: Packaging (Windows): Executing up to 12 processes, one per physical core
UATHelper: Packaging (Windows): Using Parallel executor to run 4 action(s)
UATHelper: Packaging (Windows): ------ Building 4 action(s) started ------
LogDerivedDataCache: C:/Users/pasi/AppData/Local/UnrealEngine/Common/DerivedDataCache: Maintenance finished in +00:00:00.000 and deleted 0 files with total size 0 MiB and 0 empty folders. Scanned 0 files in 1 folders with total size 0 MiB.
UATHelper: Packaging (Windows): [1/4] Compile [x64] StereolabsAIDetectionRunnable.cpp
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(20): error C2061: syntax error: identifier 'ESlErrorCode'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(27): error C3646: 'ObjectDetectionModel': unknown override specifier
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(27): error C4430: missing type specifier - int assumed. Note: C++ does not support default-int
PackagingResults: Error: identifier 'ESlErrorCode'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(40): error C2061: syntax error: identifier 'ESlErrorCode'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(48): error C3646: 'BodyTrackingModel': unknown override specifier
PackagingResults: Error: identifier 'ESlErrorCode'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(48): error C4430: missing type specifier - int assumed. Note: C++ does not support default-int
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Public\Core\StereolabsCoreGlobals.h(2463): warning C4996: 'strcpy': This function or variable may be unsafe. Consider using strcpy_s instead. To disable deprecation, use _CRT_SECURE_NO_WARNINGS. See online help for details.
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Public\Core\StereolabsCoreGlobals.h(2464): warning C4996: 'strcpy': This function or variable may be unsafe. Consider using strcpy_s instead. To disable deprecation, use _CRT_SECURE_NO_WARNINGS. See online help for details.
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Public\Core\StereolabsCoreGlobals.h(2481): warning C4996: 'sprintf': This function or variable may be unsafe. Consider using sprintf_s instead. To disable deprecation, use _CRT_SECURE_NO_WARNINGS. See online help for details.
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(18): error C2065: 'ObjectDetectionModel': undeclared identifier
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(54): error C2065: 'ObjectDetectionModel': undeclared identifier
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(58): error C2660: 'FSlObjectDetectionRunnable::RetrieveObjects': function does not take 2 arguments
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(20): note: see declaration of 'FSlObjectDetectionRunnable::RetrieveObjects'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(58): note: while trying to match the argument list '(ESlErrorCode, const FSlTimestamp)'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(65): error C2511: 'void FSlObjectDetectionRunnable::RetrieveObjects(ESlErrorCode,const FSlTimestamp &)': overloaded member function not found in 'FSlObjectDetectionRunnable'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(11): note: see declaration of 'FSlObjectDetectionRunnable'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(67): error C4551: function call missing argument list
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(67): error C2597: illegal reference to non-static member 'FSlRunnable::bIsRunning'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(67): note: see declaration of 'FSlRunnable::bIsRunning'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(67): error C3867: 'FSlRunnable::bIsRunning': non-standard syntax; use '&' to create a pointer to member
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(67): error C2568: '&&': unable to resolve function overload
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(74): error C3536: 'ObjectDetectionTime': cannot be used before it is initialized
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(76): error C2597: illegal reference to non-static member 'FSlObjectDetectionRunnable::Fps'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(76): note: see declaration of 'FSlObjectDetectionRunnable::Fps'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(76): error C3867: 'FSlObjectDetectionRunnable::Fps': non-standard syntax; use '&' to create a pointer to member
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(76): error C2568: '+': unable to resolve function overload
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(77): error C2597: illegal reference to non-static member 'FSlObjectDetectionRunnable::PreviousTS'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(26): note: see declaration of 'FSlObjectDetectionRunnable::PreviousTS'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(95): error C2065: 'BodyTrackingModel': undeclared identifier
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(130): error C2065: 'BodyTrackingModel': undeclared identifier
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(135): error C2660: 'FSlBodyTrackingRunnable::RetrieveBodies': function does not take 2 arguments
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(40): note: see declaration of 'FSlBodyTrackingRunnable::RetrieveBodies'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(135): note: while trying to match the argument list '(ESlErrorCode, const FSlTimestamp)'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(142): error C2511: 'void FSlBodyTrackingRunnable::RetrieveBodies(ESlErrorCode,const FSlTimestamp &)': overloaded member function not found in 'FSlBodyTrackingRunnable'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(31): note: see declaration of 'FSlBodyTrackingRunnable'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(144): error C4551: function call missing argument list
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(144): error C2597: illegal reference to non-static member 'FSlRunnable::bIsRunning'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(144): note: see declaration of 'FSlRunnable::bIsRunning'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(144): error C3867: 'FSlRunnable::bIsRunning': non-standard syntax; use '&' to create a pointer to member
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(144): error C2568: '&&': unable to resolve function overload
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(151): error C3536: 'ObjectDetectionTime': cannot be used before it is initialized
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(153): error C2597: illegal reference to non-static member 'FSlBodyTrackingRunnable::Fps'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(153): note: see declaration of 'FSlBodyTrackingRunnable::Fps'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(153): error C3867: 'FSlBodyTrackingRunnable::Fps': non-standard syntax; use '&' to create a pointer to member
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(153): error C2568: '+': unable to resolve function overload
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.cpp(154): error C2597: illegal reference to non-static member 'FSlBodyTrackingRunnable::PreviousTS'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsAIDetectionRunnable.h(46): note: see declaration of 'FSlBodyTrackingRunnable::PreviousTS'
UATHelper: Packaging (Windows): [2/4] Compile [x64] StereolabsMeasureRunnable.cpp
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.h(105): error C2061: syntax error: identifier 'ESlErrorCode'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Public\Core\StereolabsCoreGlobals.h(2463): warning C4996: 'strcpy': This function or variable may be unsafe. Consider using strcpy_s instead. To disable deprecation, use _CRT_SECURE_NO_WARNINGS. See online help for details.
PackagingResults: Error: identifier 'ESlErrorCode'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Public\Core\StereolabsCoreGlobals.h(2464): warning C4996: 'strcpy': This function or variable may be unsafe. Consider using strcpy_s instead. To disable deprecation, use _CRT_SECURE_NO_WARNINGS. See online help for details.
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Public\Core\StereolabsCoreGlobals.h(2481): warning C4996: 'sprintf': This function or variable may be unsafe. Consider using sprintf_s instead. To disable deprecation, use _CRT_SECURE_NO_WARNINGS. See online help for details.
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(47): error C2660: 'FSlMeasureRunnable::GrabCallback': function does not take 1 arguments
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.h(105): note: see declaration of 'FSlMeasureRunnable::GrabCallback'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(47): note: while trying to match the argument list '(ESlErrorCode)'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(170): error C2511: 'void FSlMeasureRunnable::GrabCallback(ESlErrorCode)': overloaded member function not found in 'FSlMeasureRunnable'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.h(33): note: see declaration of 'FSlMeasureRunnable'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(174): error C2597: illegal reference to non-static member 'FSlMeasureRunnable::bDepthEnabled'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.h(109): note: see declaration of 'FSlMeasureRunnable::bDepthEnabled'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(174): error C2597: illegal reference to non-static member 'FSlMeasureRunnable::bNormalsEnabled'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.h(112): note: see declaration of 'FSlMeasureRunnable::bNormalsEnabled'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(180): error C2597: illegal reference to non-static member 'FSlMeasureRunnable::UpdateSection'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.h(121): note: see declaration of 'FSlMeasureRunnable::UpdateSection'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(180): error C2665: 'FScopeLock::FScopeLock': no overloaded function could convert all the argument types
UATHelper: Packaging (Windows): D:\Epic Games\UE_5.4\Engine\Source\Runtime\Core\Public\Misc\ScopeLock.h(63): note: could be 'FScopeLock::FScopeLock(const FScopeLock &)'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(180): note: 'FScopeLock::FScopeLock(const FScopeLock &)': cannot convert argument 1 from 'FCriticalSection FSlMeasureRunnable::* ' to 'const FScopeLock &'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(180): note: Reason: cannot convert from 'FCriticalSection FSlMeasureRunnable::* ' to 'const FScopeLock'
UATHelper: Packaging (Windows): D:\Epic Games\UE_5.4\Engine\Source\Runtime\Core\Public\Misc\ScopeLock.h(35): note: or 'FScopeLock::FScopeLock(FCriticalSection *)'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(180): note: 'FScopeLock::FScopeLock(FCriticalSection *)': cannot convert argument 1 from 'FCriticalSection FSlMeasureRunnable::* ' to 'FCriticalSection *'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(180): note: There is no context in which this conversion is possible
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(180): note: while trying to match the argument list '(FCriticalSection FSlMeasureRunnable::* )'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(181): error C2597: illegal reference to non-static member 'FSlMeasureRunnable::BuffersPool'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(181): note: see declaration of 'FSlMeasureRunnable::BuffersPool'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(181): error C3867: 'FSlMeasureRunnable::BuffersPool': non-standard syntax; use '&' to create a pointer to member
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(181): error C2568: '[': unable to resolve function overload
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(183): error C2597: illegal reference to non-static member 'FSlMeasureRunnable::bDepthEnabled'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(183): note: see declaration of 'FSlMeasureRunnable::bDepthEnabled'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(183): error C3867: 'FSlMeasureRunnable::bDepthEnabled': non-standard syntax; use '&' to create a pointer to member
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(183): error C2568: '=': unable to resolve function overload
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(184): error C2597: illegal reference to non-static member 'FSlMeasureRunnable::bNormalsEnabled'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(184): note: see declaration of 'FSlMeasureRunnable::bNormalsEnabled'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(184): error C3867: 'FSlMeasureRunnable::bNormalsEnabled': non-standard syntax; use '&' to create a pointer to member
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(184): error C2568: '=': unable to resolve function overload
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(204): error C2597: illegal reference to non-static member 'FSlMeasureRunnable::UpdateSection'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.h(121): note: see declaration of 'FSlMeasureRunnable::UpdateSection'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(204): error C2665: 'FScopeLock::FScopeLock': no overloaded function could convert all the argument types
UATHelper: Packaging (Windows): D:\Epic Games\UE_5.4\Engine\Source\Runtime\Core\Public\Misc\ScopeLock.h(63): note: could be 'FScopeLock::FScopeLock(const FScopeLock &)'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(204): note: 'FScopeLock::FScopeLock(const FScopeLock &)': cannot convert argument 1 from 'FCriticalSection FSlMeasureRunnable::* ' to 'const FScopeLock &'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(204): note: Reason: cannot convert from 'FCriticalSection FSlMeasureRunnable::* ' to 'const FScopeLock'
UATHelper: Packaging (Windows): D:\Epic Games\UE_5.4\Engine\Source\Runtime\Core\Public\Misc\ScopeLock.h(35): note: or 'FScopeLock::FScopeLock(FCriticalSection *)'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(204): note: 'FScopeLock::FScopeLock(FCriticalSection *)': cannot convert argument 1 from 'FCriticalSection FSlMeasureRunnable::* ' to 'FCriticalSection *'
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(204): note: There is no context in which this conversion is possible
UATHelper: Packaging (Windows): D:\Dropbox\Pasi\Taide\Type3\Huoneet\Katutila\katu_2024_12_26\Plugins\Stereolabs\Source\Stereolabs\Private\Threading\StereolabsMeasureRunnable.cpp(204): note: while trying to match the argument list '(FCriticalSection FSlMeasureRunnable::* )'
UATHelper: Packaging (Windows): Total time in Parallel executor: 16.35 seconds
UATHelper: Packaging (Windows): Total execution time: 20.07 seconds
UATHelper: Packaging (Windows): Took 20,16s to run dotnet.exe, ExitCode=6
UATHelper: Packaging (Windows): UnrealBuildTool failed. See log for more details. (C:\Users\pasi\AppData\Roaming\Unreal Engine\AutomationTool\Logs\D+Epic+Games+UE_5.4\UBA-ZEDSamples-Win64-Development.txt)
UATHelper: Packaging (Windows): AutomationTool executed for 0h 0m 22s
UATHelper: Packaging (Windows): AutomationTool exiting with ExitCode=6 (6)
UATHelper: Packaging (Windows): BUILD FAILED
PackagingResults: Error: Unknown Error