Unreal 5.3.2 and Zed SDK 4.0.8 Doesn't Open UProject file

Screenshot 2023-11-10 151858

All of the mentioned files in the popup are present in the downloaded Github zip.

When I click “yes” it errors and prompts to build from source.

Any clues?

I also upgrade to 4.0.8, now I can’t compile project, getting error “1>ZED SDK Patch Version mismatch : found 8 expected 7”. Really wish there would be warning to not upgrade until project is upgraded.
Especially since patch notes say " Unreal Engine* Update to UE 5.3" and now it actually don’t work with 5.3 lol

Sorry for the inconvenience.

I just created a release of the plugin that is compatible with the latest SDK version. You can find it here : https://github.com/stereolabs/zed-UE5/releases/tag/v1.8

Best

Stereolabs Support

Thank you! There is a broken link in BP_Crosshair.

Indeed, there is obselete code remaining in this blueprint.

I pushed a fix on the main branch of the repo but you can also delete that part safely.

Thanks again for the feedback.

Stereolabs Support