Unity 6 Passthrough

Hi, I’m working on implementing a passthrough window into a VR application I am developing. However, in the screenshot that I am attaching, you can see the cube behind the passthrough which is not my intention. I want to implement the passthrough OVER the digital objects and not have them visible if they are behind it. I tried enabling/disabling various options in ZED Manager script, including turning the Depth Occlusion setting on or off under AR Passthrough Settings but that didn’t seem to work.

Hi @smietanr
can you please record a video showing this problem and point the camera to something other than your screen?

This good enough?

The object is clipping when I put my hand in front of it.

The main idea behind the application that I’ll be developing would be to create a passthrough window to make the physical flight yoke visible when you’re in VR.

it’s clearly a depth estimation issue. What depth mode are you using ?

you can also try to change the confidence, it might help

image

imageThese are my settings.

Whenever I reduce any of those values, the cube becomes more visible.

And I’m using the Ultra Depth Mode

Bit of an update. Cranked up the confidence threshold to 100 and fiddled around with different depth modes. I ended up using Neural.

The cube is now no longer visible except when I outstretch my hand forward or whenever I point the camera at brighter surfaces.