Hello,
I am using the ZED2i camera and cloned the new zed_ros_wrapper. it asked me to update the sdk from 3.8 to 4.0, I was also asked to update the cuda version as I was using the cuda-11.7. And I updated it to cuda-12.1. Now when I catkin_make the ros_wrapper puts and error like this -
But I have the cuda12.1 installed. the result of the nvcc --version command is -
“”"
nvcc: NVIDIA (R) Cuda compiler driver
Copyright (c) 2005-2023 NVIDIA Corporation
Built on Tue_Feb__7_19:32:13_PST_2023
Cuda compilation tools, release 12.1, V12.1.66
Build cuda_12.1.r12.1/compiler.32415258_0
“”“”“”“”“”"
Please help me out.