Hi there! I am new to SDK and I am trying to install the API for python. I use Pycharm. When I launch get_python_api.py the output on the console is:
C:\Users\franc\PycharmProjects\venv\Scripts\python.exe “C:\Program Files (x86)\ZED SDK\get_python_api.py”
→ Downloading to ‘C:\Program Files (x86)\ZED SDK’
Detected platform:
win_amd64
Python 3.11
ZED SDK 3.8
→ Checking if https://download.stereolabs.com/zedsdk/3.8/whl/win_amd64/pyzed-3.8-cp311-cp311-win_amd64.whl exists and is available
Error downloading whl file (HTTP Error 403: Forbidden)
Unsupported platforms, no pyzed file available for this configuration
It can be manually installed from source GitHub - stereolabs/zed-python-api: Python API for the ZED SDK
Process finished with exit code 1
Anyone has some idea on what can I do? I have an Intel i7 core processor but the software detects win AMD64. Is it correct? Then the software *.whl has amd64 in the name… is it a problem? Moreover CUDA is installed but the code doesn’t detect it.