Thread sanitizer reports data races for open and grab for multiple mono cameras

We’ve been tracking the instability issues with our cameras and one of the issues we found is the following:

#include <chrono>
#include <iostream>
#include <iterator>
#include <mutex>
#include <ranges>
#include <syncstream>
#include <vector>
#include <thread>
#include <utility>

#include <sl/CameraOne.hpp>

int main(int argc, char* argv[]) {
//	std::mutex mutex { };
	auto func = [&](auto stopToken, auto& device) {
		sl::InitParametersOne initParams { };
		initParams.camera_resolution = sl::RESOLUTION::HD1080;
		initParams.camera_fps = 15;
		initParams.sdk_verbose = 1;
		initParams.input.setFromSerialNumber(device.serial_number);
		sl::CameraOne camera { };
		{
//			std::lock_guard lock { mutex };
			if (auto err = camera.open(initParams); err != sl::ERROR_CODE::SUCCESS) {
				std::cout << "open failed: " << sl::toString(err) << std::endl;
				return;
			}
		}
		std::size_t counter { 0 };
		while (!stopToken.stop_requested()) {
			auto t1 = std::chrono::steady_clock::now();
			if (auto err = camera.grab(); err != sl::ERROR_CODE::SUCCESS) {
				std::osyncstream(std::cout) << counter << " " << std::chrono::steady_clock::now() - t1 << " error" << std::endl;
			} else {
				std::osyncstream(std::cout) << counter << " " << std::chrono::steady_clock::now() - t1 << " ok" << std::endl;
			}
			++counter;
			std::this_thread::sleep_for(std::chrono::milliseconds { 10 });
		}
		std::osyncstream(std::cout) << "thread closing" << std::endl;
		camera.close();
		std::osyncstream(std::cout) << "thread done" << std::endl;
	};
	
	std::vector<std::jthread> threads { };
	std::ranges::copy(
		sl::CameraOne::getDeviceList() |
			std::ranges::views::filter([](auto&& d) {
				return d.camera_model == sl::MODEL::ZED_XONE_GS  ||
					d.camera_model == sl::MODEL::ZED_XONE_UHD ||
					d.camera_model == sl::MODEL::ZED_XONE_HDR;
			}) |
			std::ranges::views::take(3) | 
			std::ranges::views::transform([&](auto&& d) {
				return std::jthread { [d, &func](auto stopToken) {
					return func(stopToken, d);
				} };
			}),
		std::back_inserter(threads)
	);
	
	std::osyncstream(std::cout) << "sleeping for 15s" << std::endl;
	std::this_thread::sleep_for(std::chrono::seconds { 15 });
	
	std::ranges::for_each(
		threads,
		[](auto&& t) {
			t.request_stop();
			t.join();
		}
	);

	std::cout << "done" << std::endl;
	
	return 0;
}
cmake_minimum_required(VERSION 3.10)

project (zedone_tsan VERSION 0.1)

set(CMAKE_CXX_STANDARD 20)
set(CMAKE_CXX_STANDARD_REQUIRED ON)
SET(CMAKE_BUILD_TYPE "RelWithDebInfo")

# ASAN
#add_compile_options(-fsanitize=address -fno-omit-frame-pointer)
#add_link_options(-fsanitize=address)
# TSAN
add_compile_options(-fsanitize=thread)
add_link_options(-fsanitize=thread)
# UBSAN
#add_compile_options(-fsanitize=undefined)
#add_link_options(-fsanitize=undefined)

find_package(ZED REQUIRED)
find_package(CUDA ${ZED_CUDA_VERSION} REQUIRED)

add_executable(${PROJECT_NAME} zedone_tsan.cpp)

target_include_directories(${PROJECT_NAME} PRIVATE
    ${ZED_INCLUDE_DIRS}
    ${CUDA_INCLUDE_DIRS}
)

link_directories(${ZED_LIBRARY_DIR} ${CUDA_LIBRARY_DIRS})

target_link_libraries(${PROJECT_NAME} PRIVATE
    ${ZED_LIBRARIES}
    ${CUDA_CUDA_LIBRARY}
)

Three Zed X One cameras, Zed Link Capture Card Duo, ZedSDK 5.4.1, CUDA version: V13.2.86, on Jetson Orin NX with Jetpack 7.2.1, the program is compiled with gcc 13.3.0 with thread sanitizer enabled. ZED_Diagnostics is green. The program above gives the first report on `open` and the second one on `grab`:

WARNING: ThreadSanitizer: data race (pid=38839)
  Write of size 8 at 0xffffa0fe4510 by thread T12 (mutexes: write M0):
    #0 memcpy ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:115 (libtsan.so.2+0x930fc) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 memcpy ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:107 (libtsan.so.2+0x930fc)
    #2 <null> <null> (libnvargus_socketclient.so+0x196f2c) (BuildId: 66cda73d5955063b65e82a1c027dded2c727992b)
    #3 operator()<std::stop_token> <stripped>/zedone_tsan.cpp:56 (zedone_tsan+0x66a4) (BuildId: 82e9a6a46629fa6af7ccc2450f1549285a759ff0)
    #4 __invoke_impl<void, main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:61 (zedone_tsan+0x66a4)
    #5 __invoke<main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:96 (zedone_tsan+0x66a4)
    #6 _M_invoke<0, 1> /usr/include/c++/13/bits/std_thread.h:292 (zedone_tsan+0x66a4)
    #7 operator() /usr/include/c++/13/bits/std_thread.h:299 (zedone_tsan+0x66a4)
    #8 _M_run /usr/include/c++/13/bits/std_thread.h:244 (zedone_tsan+0x66a4)
    #9 <null> <null> (libstdc++.so.6+0xe1adc) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)

  Previous write of size 8 at 0xffffa0fe4510 by thread T13 (mutexes: write M1):
    #0 memcpy ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:115 (libtsan.so.2+0x930fc) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 memcpy ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:107 (libtsan.so.2+0x930fc)
    #2 <null> <null> (libnvargus_socketclient.so+0x196f2c) (BuildId: 66cda73d5955063b65e82a1c027dded2c727992b)
    #3 operator()<std::stop_token> <stripped>/zedone_tsan.cpp:56 (zedone_tsan+0x66a4) (BuildId: 82e9a6a46629fa6af7ccc2450f1549285a759ff0)
    #4 __invoke_impl<void, main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:61 (zedone_tsan+0x66a4)
    #5 __invoke<main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:96 (zedone_tsan+0x66a4)
    #6 _M_invoke<0, 1> /usr/include/c++/13/bits/std_thread.h:292 (zedone_tsan+0x66a4)
    #7 operator() /usr/include/c++/13/bits/std_thread.h:299 (zedone_tsan+0x66a4)
    #8 _M_run /usr/include/c++/13/bits/std_thread.h:244 (zedone_tsan+0x66a4)
    #9 <null> <null> (libstdc++.so.6+0xe1adc) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)

  Location is global '<null>' at 0x000000000000 (libnvargus_socketclient.so+0x294510)

  Mutex M0 (0xffffac4e5f30) created at:
    #0 pthread_mutex_lock ../../../../src/libsanitizer/tsan/tsan_interceptors_posix.cpp:1341 (libtsan.so.2+0x5cc14) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 sl::ArgusProvider::getInstance() <null> (libsl_zed.so+0x7c4518) (BuildId: 3584267cb36b2d701f8a7ce36ee700a9a1ea4514)
    #2 __libc_start_call_main ../sysdeps/nptl/libc_start_call_main.h:58 (libc.so.6+0x284c0) (BuildId: d5ef86dde36cbd3289566cf5098226035d76f2e1)

  Mutex M1 (0xffffac4e42e8) created at:
    #0 pthread_mutex_lock ../../../../src/libsanitizer/tsan/tsan_interceptors_posix.cpp:1341 (libtsan.so.2+0x5cc14) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 sl::ArgusCamera::getGMSLDevices(bool, bool) <null> (libsl_zed.so+0x7abfe4) (BuildId: 3584267cb36b2d701f8a7ce36ee700a9a1ea4514)
    #2 __libc_start_call_main ../sysdeps/nptl/libc_start_call_main.h:58 (libc.so.6+0x284c0) (BuildId: d5ef86dde36cbd3289566cf5098226035d76f2e1)

  Thread T12 (tid=38935, running) created by main thread at:
    #0 pthread_create ../../../../src/libsanitizer/tsan/tsan_interceptors_posix.cpp:1022 (libtsan.so.2+0x5dd98) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 std::thread::_M_start_thread(std::unique_ptr<std::thread::_State, std::default_delete<std::thread::_State> >, void (*)()) <null> (libstdc++.so.6+0xe1c64) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)
    #2 __libc_start_call_main ../sysdeps/nptl/libc_start_call_main.h:58 (libc.so.6+0x284c0) (BuildId: d5ef86dde36cbd3289566cf5098226035d76f2e1)

  Thread T13 (tid=38936, running) created by main thread at:
    #0 pthread_create ../../../../src/libsanitizer/tsan/tsan_interceptors_posix.cpp:1022 (libtsan.so.2+0x5dd98) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 std::thread::_M_start_thread(std::unique_ptr<std::thread::_State, std::default_delete<std::thread::_State> >, void (*)()) <null> (libstdc++.so.6+0xe1c64) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)
    #2 __libc_start_call_main ../sysdeps/nptl/libc_start_call_main.h:58 (libc.so.6+0x284c0) (BuildId: d5ef86dde36cbd3289566cf5098226035d76f2e1)

SUMMARY: ThreadSanitizer: data race ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:115 in memcpy
WARNING: ThreadSanitizer: data race (pid=38839)
  Write of size 8 at 0xffff92a03c78 by thread T18:
    #0 memcpy ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:115 (libtsan.so.2+0x930fc) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 memcpy ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:107 (libtsan.so.2+0x930fc)
    #2 sl::ArgusCamera::readSingle(unsigned char*, unsigned long long&) <null> (libsl_zed.so+0x7922ac) (BuildId: 3584267cb36b2d701f8a7ce36ee700a9a1ea4514)

  Previous read of size 8 at 0xffff92a03c78 by thread T11 (mutexes: write M0):
    #0 memcpy ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:115 (libtsan.so.2+0x930fc) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 memcpy ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:107 (libtsan.so.2+0x930fc)
    #2 <null> <null> (libsl_zed.so+0x202030c) (BuildId: 3584267cb36b2d701f8a7ce36ee700a9a1ea4514)
    #3 operator()<std::stop_token> <stripped>/zedone_tsan.cpp:56 (zedone_tsan+0x66a4) (BuildId: 82e9a6a46629fa6af7ccc2450f1549285a759ff0)
    #4 __invoke_impl<void, main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:61 (zedone_tsan+0x66a4)
    #5 __invoke<main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:96 (zedone_tsan+0x66a4)
    #6 _M_invoke<0, 1> /usr/include/c++/13/bits/std_thread.h:292 (zedone_tsan+0x66a4)
    #7 operator() /usr/include/c++/13/bits/std_thread.h:299 (zedone_tsan+0x66a4)
    #8 _M_run /usr/include/c++/13/bits/std_thread.h:244 (zedone_tsan+0x66a4)
    #9 <null> <null> (libstdc++.so.6+0xe1adc) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)

  Location is heap block of size 2792 at 0xffff92a03c00 allocated by thread T11:
    #0 operator new(unsigned long) ../../../../src/libsanitizer/tsan/tsan_new_delete.cpp:64 (libtsan.so.2+0xad458) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 sl::GMSLInput::setUp(int&, int, int, int, bool, sl::IMU_FREQ, bool, bool, int) <null> (libsl_zed.so+0x7e6a78) (BuildId: 3584267cb36b2d701f8a7ce36ee700a9a1ea4514)
    #2 operator()<std::stop_token> <stripped>/zedone_tsan.cpp:56 (zedone_tsan+0x66a4) (BuildId: 82e9a6a46629fa6af7ccc2450f1549285a759ff0)
    #3 __invoke_impl<void, main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:61 (zedone_tsan+0x66a4)
    #4 __invoke<main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:96 (zedone_tsan+0x66a4)
    #5 _M_invoke<0, 1> /usr/include/c++/13/bits/std_thread.h:292 (zedone_tsan+0x66a4)
    #6 operator() /usr/include/c++/13/bits/std_thread.h:299 (zedone_tsan+0x66a4)
    #7 _M_run /usr/include/c++/13/bits/std_thread.h:244 (zedone_tsan+0x66a4)
    #8 <null> <null> (libstdc++.so.6+0xe1adc) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)

  Mutex M0 (0xffff926056f8) created at:
    #0 pthread_mutex_trylock ../../../../src/libsanitizer/tsan/tsan_interceptors_posix.cpp:1354 (libtsan.so.2+0x5b0a4) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 <null> <null> (libsl_zed.so+0x2020758) (BuildId: 3584267cb36b2d701f8a7ce36ee700a9a1ea4514)
    #2 operator()<std::stop_token> <stripped>/zedone_tsan.cpp:56 (zedone_tsan+0x66a4) (BuildId: 82e9a6a46629fa6af7ccc2450f1549285a759ff0)
    #3 __invoke_impl<void, main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:61 (zedone_tsan+0x66a4)
    #4 __invoke<main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:96 (zedone_tsan+0x66a4)
    #5 _M_invoke<0, 1> /usr/include/c++/13/bits/std_thread.h:292 (zedone_tsan+0x66a4)
    #6 operator() /usr/include/c++/13/bits/std_thread.h:299 (zedone_tsan+0x66a4)
    #7 _M_run /usr/include/c++/13/bits/std_thread.h:244 (zedone_tsan+0x66a4)
    #8 <null> <null> (libstdc++.so.6+0xe1adc) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)

  Thread T18 (tid=39284, running) created by thread T11 at:
    #0 pthread_create ../../../../src/libsanitizer/tsan/tsan_interceptors_posix.cpp:1022 (libtsan.so.2+0x5dd98) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 std::thread::_M_start_thread(std::unique_ptr<std::thread::_State, std::default_delete<std::thread::_State> >, void (*)()) <null> (libstdc++.so.6+0xe1c64) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)
    #2 operator()<std::stop_token> <stripped>/zedone_tsan.cpp:56 (zedone_tsan+0x66a4) (BuildId: 82e9a6a46629fa6af7ccc2450f1549285a759ff0)
    #3 __invoke_impl<void, main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:61 (zedone_tsan+0x66a4)
    #4 __invoke<main(int, char**)::<lambda(auto:56&&)>::<lambda(auto:57)>, std::stop_token> /usr/include/c++/13/bits/invoke.h:96 (zedone_tsan+0x66a4)
    #5 _M_invoke<0, 1> /usr/include/c++/13/bits/std_thread.h:292 (zedone_tsan+0x66a4)
    #6 operator() /usr/include/c++/13/bits/std_thread.h:299 (zedone_tsan+0x66a4)
    #7 _M_run /usr/include/c++/13/bits/std_thread.h:244 (zedone_tsan+0x66a4)
    #8 <null> <null> (libstdc++.so.6+0xe1adc) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)

  Thread T11 (tid=38934, running) created by main thread at:
    #0 pthread_create ../../../../src/libsanitizer/tsan/tsan_interceptors_posix.cpp:1022 (libtsan.so.2+0x5dd98) (BuildId: dc0d657f42587fea53114ce058dbdfe5834e0205)
    #1 std::thread::_M_start_thread(std::unique_ptr<std::thread::_State, std::default_delete<std::thread::_State> >, void (*)()) <null> (libstdc++.so.6+0xe1c64) (BuildId: 7c239d1743727054caa3df1ab866bfa72cd4dd93)
    #2 __libc_start_call_main ../sysdeps/nptl/libc_start_call_main.h:58 (libc.so.6+0x284c0) (BuildId: d5ef86dde36cbd3289566cf5098226035d76f2e1)

SUMMARY: ThreadSanitizer: data race ../../../../src/libsanitizer/sanitizer_common/sanitizer_common_interceptors_memintrinsics.inc:115 in memcpy

Fwiw, while undesirable synchronising around `open` eliminates the first report. Doing the same for `grab` isn’t really possible.

Hi, 

Thank your for your patience.

We are looking into it with our internal engineering teams, I'll come back to you shortly with more insights. 

Best, 

Tristan 

StereoLabs Support

Hello,

The open and grab races you reported are fixed in ZED SDK 5.6, which is now public: https://www.stereolabs.com/en-fr/developers/release/5.6. Your team received the release and the updated ZED Link Duo driver by email on 17 November.

I am closing this thread on that basis. If ThreadSanitizer still reports a race on open or grab with SDK 5.6 and the latest driver, please reply here with the new report and your SDK and driver versions, and we will reopen it.

Best regards,


Tristan Leduc