Hi again, i have try to use the “zed-UE5-1.7_UE5.2” project but when I play it, i have this error:
I test the “L_BodyTrackingSingle” and “L_ObjectDetection_3D” but always i get the same error.
What is the problem ?
PD: Im try testing this project why the “zed-livelink-4.0.7” not work when y build project.
Thanks.
Hi, I leave an answer for each question:
Are you able to run other UE5 projects (not ZED related)?
a: Yes, Many
Are you able to run other scenes in the project? (like camera tracking)
a: No, i try to play other maps but nothing work.
Are you using ZED SDK v4.0.7? And Unreal 5.2?
a: Yes, the same configuration.
Do you have errors when building the solution in Visual Studio?
a: No, VS dont give me errors.
Have you modified the project in any way?
a: No, i use the fresh install of project.
What is your configuration? (GPU, OS)
a: Windows 11, VS 2022, GPU: Nvidia RTX 3070 TI.
Have you optimized the AI models after installing the SDK?
a: Yes, i have optimized all models from ZED Diagnostic.
Thanks for advance.
JPlou
October 18, 2023, 8:57am
4
I ran some tests and I forgot to ask you one thing.
Can you try using DirectX 11 instead of Dx12?
This is a known issue on our side, we’re working on fixing it, but for now that’s what causes this error.
Sorry for the inconvenience.
Hello, sorry for the delay in replying and yes, I have used dx12. Today I will try changing to dx11.
Thanks for your guidance.
El mié, 18 oct 2023 a la(s) 05:58, Jean-Loup Macarit (Stereolabs) (support@stereolabs.com ) escribió: